<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックIFC CONNECTION TO 16BIT NOR FLASH IN LS1043ARDB</title>
    <link>https://community.nxp.com/t5/Layerscape/IFC-CONNECTION-TO-16BIT-NOR-FLASH-IN-LS1043ARDB/m-p/1730696#M13403</link>
    <description>&lt;P&gt;We &amp;nbsp;are using &amp;nbsp;LS1043ARDB and as per schematic &amp;nbsp;diagram IFC connection to 16 bit NOR FLASH is in ADM-SHFT-MODE=0(as per LS1043A Reference manual figure 25.9). As per this mode, IFC_AD0 should be MSB and it should get connected to NOR FLASH &amp;nbsp;ADDRESS line A25. But IFC_AD1 is connected to A25 address pin of FLASH. Please clarify.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;IFC_A26 is the LSB bit and &amp;nbsp;it should be left un connected( for 16 bit operation). but it is connected to A0 &amp;nbsp;Address pin of NOR FLASH.Please clarify.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 27 Sep 2023 17:06:49 GMT</pubDate>
    <dc:creator>Pamid</dc:creator>
    <dc:date>2023-09-27T17:06:49Z</dc:date>
    <item>
      <title>IFC CONNECTION TO 16BIT NOR FLASH IN LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/IFC-CONNECTION-TO-16BIT-NOR-FLASH-IN-LS1043ARDB/m-p/1730696#M13403</link>
      <description>&lt;P&gt;We &amp;nbsp;are using &amp;nbsp;LS1043ARDB and as per schematic &amp;nbsp;diagram IFC connection to 16 bit NOR FLASH is in ADM-SHFT-MODE=0(as per LS1043A Reference manual figure 25.9). As per this mode, IFC_AD0 should be MSB and it should get connected to NOR FLASH &amp;nbsp;ADDRESS line A25. But IFC_AD1 is connected to A25 address pin of FLASH. Please clarify.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;IFC_A26 is the LSB bit and &amp;nbsp;it should be left un connected( for 16 bit operation). but it is connected to A0 &amp;nbsp;Address pin of NOR FLASH.Please clarify.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 17:06:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IFC-CONNECTION-TO-16BIT-NOR-FLASH-IN-LS1043ARDB/m-p/1730696#M13403</guid>
      <dc:creator>Pamid</dc:creator>
      <dc:date>2023-09-27T17:06:49Z</dc:date>
    </item>
    <item>
      <title>Re: IFC CONNECTION TO 16BIT NOR FLASH IN LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/IFC-CONNECTION-TO-16BIT-NOR-FLASH-IN-LS1043ARDB/m-p/1731064#M13408</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/47848"&gt;@Pamid&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;Please refer to figure 25-9 available in LS1043ARM which is the connection of x16 NOR for ADM MODE0. Please follow the connection details for your design.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 06:49:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IFC-CONNECTION-TO-16BIT-NOR-FLASH-IN-LS1043ARDB/m-p/1731064#M13408</guid>
      <dc:creator>mrudangshelat-13</dc:creator>
      <dc:date>2023-09-28T06:49:28Z</dc:date>
    </item>
    <item>
      <title>Re: IFC CONNECTION TO 16BIT NOR FLASH IN LS1043ARDB</title>
      <link>https://community.nxp.com/t5/Layerscape/IFC-CONNECTION-TO-16BIT-NOR-FLASH-IN-LS1043ARDB/m-p/1731137#M13414</link>
      <description>&lt;P&gt;&lt;EM&gt;In&amp;nbsp; LS1043A RDB-PD , 16 Bit NOR FLASH is connected to IFC interface of LS1043A.&amp;nbsp; &amp;nbsp;As per this&amp;nbsp;&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;IFC_ADDR[1:15] is connected to A[25:11].&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;IFC_ADDR[16:26] is connected to A[10: 0].&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;But as per LS1043ARM&amp;nbsp; Fig:25-9, IFC_AD0&amp;nbsp; after address decoding should get connect to A25 address line of NOR FLASH. I&lt;/EM&gt;&lt;EM&gt;&amp;nbsp;am confusing while co-relating&amp;nbsp;LS1043ARM&amp;nbsp; Fig:25-9 with 16 Bit NOR FLASH&amp;nbsp; connectivity in&amp;nbsp;LS1043A RDB-PD. Please clarify.&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 08:27:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/IFC-CONNECTION-TO-16BIT-NOR-FLASH-IN-LS1043ARDB/m-p/1731137#M13414</guid>
      <dc:creator>Pamid</dc:creator>
      <dc:date>2023-09-28T08:27:29Z</dc:date>
    </item>
  </channel>
</rss>