<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1012A Ethernet throughput issue!!</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1729300#M13380</link>
    <description>yes, the LSDK 21.08 will be replaced for the LLDP.&lt;BR /&gt;please check the full duplex behavior in the PHY you are using.&lt;BR /&gt;you could try with the LLDP</description>
    <pubDate>Tue, 26 Sep 2023 02:58:04 GMT</pubDate>
    <dc:creator>LFGP</dc:creator>
    <dc:date>2023-09-26T02:58:04Z</dc:date>
    <item>
      <title>LS1012A Ethernet throughput issue!!</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1726055#M13344</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using it by porting 18.12 to the LS1012A custom board.&lt;/P&gt;&lt;P&gt;We are conducting throughput tests by linking our equipment with a test instrument (MTS-8000).&lt;/P&gt;&lt;P&gt;We are doing a 150Mbps bi-directional test, and when normal, Tx/Rx operates at 150Mbps/150Mbps each without a problem.&lt;/P&gt;&lt;P&gt;However, when you unplug the Ethernet cable and reconnect it, the speed decreases by half, like 75Mbps/150Mbps. If you unplug and reconnect, it may return to normal.&lt;/P&gt;&lt;P&gt;There seems to be a problem when reconnecting the link. Please give me some advice.&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Gyosun.&lt;/P&gt;</description>
      <pubDate>Wed, 20 Sep 2023 07:50:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1726055#M13344</guid>
      <dc:creator>Gyosun</dc:creator>
      <dc:date>2023-09-20T07:50:12Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Ethernet throughput issue!!</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1727381#M13364</link>
      <description>&lt;P&gt;How do you have the ethernet port configured?&lt;/P&gt;
&lt;P&gt;What do you mean "There seems to be a problem when reconnecting the link"?&amp;nbsp; What happens? Do you get error messages?&amp;nbsp; Do you know noticed lights blinking on the port?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 21 Sep 2023 18:13:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1727381#M13364</guid>
      <dc:creator>Irene</dc:creator>
      <dc:date>2023-09-21T18:13:05Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Ethernet throughput issue!!</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1727495#M13367</link>
      <description>&lt;P&gt;Hi&amp;nbsp;Irene,&lt;/P&gt;&lt;P&gt;Thank you for answering.&lt;/P&gt;&lt;P&gt;I also want to know why this happens.&lt;BR /&gt;&lt;SPAN&gt;The LED is blinking normally, and packets are being received well.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;However, the problem is that the speed is reduced by half when reconnected.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;As of now, it appears that autoneg fails upon reconnection and operates in half duplex.&lt;BR /&gt;The ethernet phy chip is AR8033-AL1B.&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Is this a pfe driver bug?&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;I'm looking for a solution.&lt;/SPAN&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;BR /&gt;&lt;SPAN&gt;Best Regards,&lt;BR /&gt;&lt;/SPAN&gt;&lt;SPAN&gt;Gyosun.&lt;/SPAN&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 06:32:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1727495#M13367</guid>
      <dc:creator>Gyosun</dc:creator>
      <dc:date>2023-09-22T06:32:33Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Ethernet throughput issue!!</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1728154#M13372</link>
      <description>&lt;P&gt;&lt;SPAN&gt;you could try the command&lt;EM&gt; ifconfig eno1 down ; sleep 2 ; ifconfig eno1 up&amp;nbsp;&amp;nbsp;&lt;/EM&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;in order to restart the adapter.&lt;/P&gt;
&lt;P&gt;And as I suggested you in my last message "try to use the LSDK 21.08 instead the version 18"&lt;/P&gt;</description>
      <pubDate>Fri, 22 Sep 2023 16:17:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1728154#M13372</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2023-09-22T16:17:27Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Ethernet throughput issue!!</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1728458#M13374</link>
      <description>&lt;P&gt;Hi LFGP,&lt;/P&gt;&lt;P&gt;Even if I try setting it to "&lt;EM&gt;ifconfig eth1 down ; sleep 2 ; ifconfig eth1 up&amp;nbsp;&lt;/EM&gt;", the same symptoms still appear.&lt;BR /&gt;&lt;SPAN&gt;I also tested it by copying and porting the fsl_ppfe folder from LSDK 21.08 to 18.12.&lt;BR /&gt;&lt;/SPAN&gt;However, the symptoms did not resolve.&lt;/P&gt;&lt;P&gt;Among the latest SDKs, there is LLDP. Will it be replaced by LLDP in the future instead of LSDK 21.08?&lt;BR /&gt;Would it be better to try porting LLDP?&lt;/P&gt;&lt;P&gt;Thank you,&amp;nbsp;&lt;BR /&gt;Best Regards.&lt;BR /&gt;Gyosun.&lt;/P&gt;</description>
      <pubDate>Mon, 25 Sep 2023 02:34:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1728458#M13374</guid>
      <dc:creator>Gyosun</dc:creator>
      <dc:date>2023-09-25T02:34:37Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Ethernet throughput issue!!</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1729300#M13380</link>
      <description>yes, the LSDK 21.08 will be replaced for the LLDP.&lt;BR /&gt;please check the full duplex behavior in the PHY you are using.&lt;BR /&gt;you could try with the LLDP</description>
      <pubDate>Tue, 26 Sep 2023 02:58:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1729300#M13380</guid>
      <dc:creator>LFGP</dc:creator>
      <dc:date>2023-09-26T02:58:04Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Ethernet throughput issue!!</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1730618#M13401</link>
      <description>&lt;P&gt;Please provide more details as below.&lt;BR /&gt;output of "ethtool &amp;lt;eth&amp;gt;" and "ethtool -S &amp;lt;eth&amp;gt;", included before and after unplug the cable.&lt;BR /&gt;I want to get the port speed and duplex info.&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 14:48:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1730618#M13401</guid>
      <dc:creator>Irene</dc:creator>
      <dc:date>2023-09-27T14:48:58Z</dc:date>
    </item>
    <item>
      <title>Re: LS1012A Ethernet throughput issue!!</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1733441#M13429</link>
      <description>&lt;P&gt;Hi LFGP,&lt;/P&gt;&lt;P&gt;We ported LSDK version 21.08 and confirmed that Ethernet was operating normally.&lt;BR /&gt;It took a lot of trial and error, but eventually the problem was solved.&lt;/P&gt;&lt;P&gt;Thank you.&lt;BR /&gt;Best Regards,&lt;BR /&gt;Gyosun.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Oct 2023 02:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1012A-Ethernet-throughput-issue/m-p/1733441#M13429</guid>
      <dc:creator>Gyosun</dc:creator>
      <dc:date>2023-10-04T02:25:19Z</dc:date>
    </item>
  </channel>
</rss>