<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to confirm that ls1046ardb u-boot drivers are using device tree?. in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/How-to-confirm-that-ls1046ardb-u-boot-drivers-are-using-device/m-p/1710091#M13153</link>
    <description>&lt;P&gt;What do you mean that the probe is not being called?&amp;nbsp;&amp;nbsp;&amp;nbsp; Are you getting error messages?&amp;nbsp; Once uboot is up you can execute printenv and it will print out all U-Boot environment variables?&amp;nbsp;&amp;nbsp;&amp;nbsp; The Device Tree Blob is produced by the compiler, and is&lt;BR /&gt;the binary that gets loaded by the bootloader and parsed by the kernel at boot time.&lt;/P&gt;
&lt;P&gt;Compiled kernel images are in arch/${ARCH}/boot/ folder.&lt;BR /&gt;Compiled device trees (dtb files) are in arch/${ARCH}/boot/dts folder&lt;/P&gt;</description>
    <pubDate>Wed, 23 Aug 2023 19:32:36 GMT</pubDate>
    <dc:creator>Irene</dc:creator>
    <dc:date>2023-08-23T19:32:36Z</dc:date>
    <item>
      <title>How to confirm that ls1046ardb u-boot drivers are using device tree?.</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-confirm-that-ls1046ardb-u-boot-drivers-are-using-device/m-p/1707863#M13122</link>
      <description>&lt;P&gt;Though device node in ls1046a.dtsi and uboot driver compatible matching is found, but probe is not getting called. how to confirm that uboot is using device tree?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 20 Aug 2023 14:56:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-confirm-that-ls1046ardb-u-boot-drivers-are-using-device/m-p/1707863#M13122</guid>
      <dc:creator>srinivasa</dc:creator>
      <dc:date>2023-08-20T14:56:14Z</dc:date>
    </item>
    <item>
      <title>Re: How to confirm that ls1046ardb u-boot drivers are using device tree?.</title>
      <link>https://community.nxp.com/t5/Layerscape/How-to-confirm-that-ls1046ardb-u-boot-drivers-are-using-device/m-p/1710091#M13153</link>
      <description>&lt;P&gt;What do you mean that the probe is not being called?&amp;nbsp;&amp;nbsp;&amp;nbsp; Are you getting error messages?&amp;nbsp; Once uboot is up you can execute printenv and it will print out all U-Boot environment variables?&amp;nbsp;&amp;nbsp;&amp;nbsp; The Device Tree Blob is produced by the compiler, and is&lt;BR /&gt;the binary that gets loaded by the bootloader and parsed by the kernel at boot time.&lt;/P&gt;
&lt;P&gt;Compiled kernel images are in arch/${ARCH}/boot/ folder.&lt;BR /&gt;Compiled device trees (dtb files) are in arch/${ARCH}/boot/dts folder&lt;/P&gt;</description>
      <pubDate>Wed, 23 Aug 2023 19:32:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-to-confirm-that-ls1046ardb-u-boot-drivers-are-using-device/m-p/1710091#M13153</guid>
      <dc:creator>Irene</dc:creator>
      <dc:date>2023-08-23T19:32:36Z</dc:date>
    </item>
  </channel>
</rss>