<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ls1028 TSN 802.1QBV queueMaxSDU and guard band question in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/ls1028-TSN-802-1QBV-queueMaxSDU-and-guard-band-question/m-p/1701462#M13038</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;&amp;nbsp;and community&lt;/P&gt;&lt;P&gt;I wanna discuss with you guys regarding the definition of&amp;nbsp;queueMaxSDU and&amp;nbsp; guard band in NXP 802.1BV.&lt;/P&gt;&lt;P&gt;According to the reference menu the guardband is set by"--maxSDU"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xinliwang_0-1691548649359.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/235643i524578B1CD73EC8B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xinliwang_0-1691548649359.png" alt="xinliwang_0-1691548649359.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and the maxSDU definition is "queueMaxSDU" which also set by "--maxSDU"&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xinliwang_1-1691548687287.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/235644iFD738E08C535114A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xinliwang_1-1691548687287.png" alt="xinliwang_1-1691548687287.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But according to the IEEE802.1qbv. The queueMaxSDU and guardband has no absolut connection. W&lt;SPAN&gt;e can determine the size we need for the&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;guard bands&lt;/EM&gt;&lt;SPAN&gt;, depending on the&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;queueMaxSDU&lt;/EM&gt; which means we can set&amp;nbsp;queueMaxSDU and&amp;nbsp;guardband independently. On the other hand, these two parameters no need to be equal.&lt;/P&gt;&lt;P&gt;But on NXP board ls1028ardb, we can not set both parameters independently. I wonder is this a unique NXP qbv feature or it could be imprved based on IEEE802.1QBV standard?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Wed, 09 Aug 2023 02:44:49 GMT</pubDate>
    <dc:creator>xinliwang</dc:creator>
    <dc:date>2023-08-09T02:44:49Z</dc:date>
    <item>
      <title>ls1028 TSN 802.1QBV queueMaxSDU and guard band question</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1028-TSN-802-1QBV-queueMaxSDU-and-guard-band-question/m-p/1701462#M13038</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;&amp;nbsp;and community&lt;/P&gt;&lt;P&gt;I wanna discuss with you guys regarding the definition of&amp;nbsp;queueMaxSDU and&amp;nbsp; guard band in NXP 802.1BV.&lt;/P&gt;&lt;P&gt;According to the reference menu the guardband is set by"--maxSDU"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xinliwang_0-1691548649359.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/235643i524578B1CD73EC8B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xinliwang_0-1691548649359.png" alt="xinliwang_0-1691548649359.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and the maxSDU definition is "queueMaxSDU" which also set by "--maxSDU"&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xinliwang_1-1691548687287.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/235644iFD738E08C535114A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xinliwang_1-1691548687287.png" alt="xinliwang_1-1691548687287.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;But according to the IEEE802.1qbv. The queueMaxSDU and guardband has no absolut connection. W&lt;SPAN&gt;e can determine the size we need for the&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;guard bands&lt;/EM&gt;&lt;SPAN&gt;, depending on the&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;queueMaxSDU&lt;/EM&gt; which means we can set&amp;nbsp;queueMaxSDU and&amp;nbsp;guardband independently. On the other hand, these two parameters no need to be equal.&lt;/P&gt;&lt;P&gt;But on NXP board ls1028ardb, we can not set both parameters independently. I wonder is this a unique NXP qbv feature or it could be imprved based on IEEE802.1QBV standard?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Wed, 09 Aug 2023 02:44:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1028-TSN-802-1QBV-queueMaxSDU-and-guard-band-question/m-p/1701462#M13038</guid>
      <dc:creator>xinliwang</dc:creator>
      <dc:date>2023-08-09T02:44:49Z</dc:date>
    </item>
    <item>
      <title>Re: ls1028 TSN 802.1QBV queueMaxSDU and guard band question</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1028-TSN-802-1QBV-queueMaxSDU-and-guard-band-question/m-p/1704091#M13066</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Currently in linux driver, guard band is calculated according to "QSYS_QMAXSDU_CFG_x", it's MAX SDU for traffic class x(0~7).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Customer can also set "PORT_MAX_SDU", this value is used for guard band calculation for a traffic class if the QMAXSDU_CFG_* is set to '0'.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;for LS1028 switch IP, guard band is calculated according to the MAX SDU of the related traffic class or port.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Aug 2023 06:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1028-TSN-802-1QBV-queueMaxSDU-and-guard-band-question/m-p/1704091#M13066</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-08-14T06:53:15Z</dc:date>
    </item>
    <item>
      <title>Re: ls1028 TSN 802.1QBV queueMaxSDU and guard band question</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1028-TSN-802-1QBV-queueMaxSDU-and-guard-band-question/m-p/1704302#M13070</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52411"&gt;@yipingwang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your reply;&lt;/P&gt;&lt;P&gt;It seems like we could not set guardband independently.&lt;/P&gt;&lt;P&gt;But I wonder does eno0 port has guardband too? I could not find any description on ENETC chapter.&lt;/P&gt;&lt;P&gt;Thank you&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 14 Aug 2023 10:14:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1028-TSN-802-1QBV-queueMaxSDU-and-guard-band-question/m-p/1704302#M13070</guid>
      <dc:creator>xinliwang</dc:creator>
      <dc:date>2023-08-14T10:14:22Z</dc:date>
    </item>
  </channel>
</rss>