<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LX2160A FlexSPI NAND Boot in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LX2160A-FlexSPI-NAND-Boot/m-p/1679477#M12762</link>
    <description>&lt;P&gt;I'm working on booting from 2K SPI NAND on the LX2160a SoC.&lt;/P&gt;&lt;P&gt;With some bug fixes to the create_pbl tool, I have managed to boot to BL2. Unfortunately ATF BL2 re-programs the FlexSPI LUTs for NOR flash operation and there is no corresponding NAND flash driver code within ATF.&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/nxp-qoriq/atf/tree/lf_v2.8/drivers/nxp/flexspi/nor" target="_blank" rel="noopener"&gt;https://github.com/nxp-qoriq/atf/tree/lf_v2.8/drivers/nxp/flexspi/nor&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Are reference / SDK software or bare metal drivers for using FlexSPI with NAND flash available somewhere or do NXP intend to add NAND support to ATF?&lt;/P&gt;&lt;P&gt;The FlexSPI Driver Design document (&lt;A href="https://community.nxp.com/t5/Layerscape-Knowledge-Base/FlexSPI-Driver-Design/ta-p/1354159" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Layerscape-Knowledge-Base/FlexSPI-Driver-Design/ta-p/1354159&lt;/A&gt;) mentions some driver files -&amp;nbsp;&lt;SPAN class=""&gt;&lt;SPAN&gt;flexspi_n&lt;/SPAN&gt;&lt;SPAN&gt;and&lt;/SPAN&gt;&lt;SPAN&gt;.c etc. Where can I get these from?&lt;BR /&gt;&lt;BR /&gt;Many thanks&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 30 Jun 2023 09:12:53 GMT</pubDate>
    <dc:creator>womble</dc:creator>
    <dc:date>2023-06-30T09:12:53Z</dc:date>
    <item>
      <title>LX2160A FlexSPI NAND Boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-FlexSPI-NAND-Boot/m-p/1679477#M12762</link>
      <description>&lt;P&gt;I'm working on booting from 2K SPI NAND on the LX2160a SoC.&lt;/P&gt;&lt;P&gt;With some bug fixes to the create_pbl tool, I have managed to boot to BL2. Unfortunately ATF BL2 re-programs the FlexSPI LUTs for NOR flash operation and there is no corresponding NAND flash driver code within ATF.&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/nxp-qoriq/atf/tree/lf_v2.8/drivers/nxp/flexspi/nor" target="_blank" rel="noopener"&gt;https://github.com/nxp-qoriq/atf/tree/lf_v2.8/drivers/nxp/flexspi/nor&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Are reference / SDK software or bare metal drivers for using FlexSPI with NAND flash available somewhere or do NXP intend to add NAND support to ATF?&lt;/P&gt;&lt;P&gt;The FlexSPI Driver Design document (&lt;A href="https://community.nxp.com/t5/Layerscape-Knowledge-Base/FlexSPI-Driver-Design/ta-p/1354159" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Layerscape-Knowledge-Base/FlexSPI-Driver-Design/ta-p/1354159&lt;/A&gt;) mentions some driver files -&amp;nbsp;&lt;SPAN class=""&gt;&lt;SPAN&gt;flexspi_n&lt;/SPAN&gt;&lt;SPAN&gt;and&lt;/SPAN&gt;&lt;SPAN&gt;.c etc. Where can I get these from?&lt;BR /&gt;&lt;BR /&gt;Many thanks&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jun 2023 09:12:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-FlexSPI-NAND-Boot/m-p/1679477#M12762</guid>
      <dc:creator>womble</dc:creator>
      <dc:date>2023-06-30T09:12:53Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160A FlexSPI NAND Boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-FlexSPI-NAND-Boot/m-p/1684590#M12825</link>
      <description>&lt;P&gt;You could refer to u-boot source code&amp;nbsp;drivers/spi/fsl_fspi_nand.c.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jul 2023 07:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-FlexSPI-NAND-Boot/m-p/1684590#M12825</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-07-10T07:31:22Z</dc:date>
    </item>
  </channel>
</rss>