<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB 3.0 micro AB acting as USB 2.0 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/USB-3-0-micro-AB-acting-as-USB-2-0/m-p/1676400#M12719</link>
    <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using LS 1046ARDB board. When I am trying to connect a USB 3.0 device using USB 3.0 micro AB port on the board, it says its USB 2.0. However, it should be USB 3.0.&lt;/P&gt;&lt;P&gt;I want to use USB 3.0 but I am unable to do so. I tried changing the wire and also tried connecting different device compatible with USB 3.0 but USB 3.0 micro AB port says it 2.0.&lt;/P&gt;&lt;P&gt;I have checked the reference sheet, it says 3.0 but when I connect something its say its USB 2.0. I am using all the wires provided in the kit.&lt;/P&gt;&lt;P&gt;Can someone please guide me how I can change the behavior of USB 3.0 micro AB to USB 3.0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Tue, 27 Jun 2023 00:09:08 GMT</pubDate>
    <dc:creator>Sarthak</dc:creator>
    <dc:date>2023-06-27T00:09:08Z</dc:date>
    <item>
      <title>USB 3.0 micro AB acting as USB 2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/USB-3-0-micro-AB-acting-as-USB-2-0/m-p/1676400#M12719</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am using LS 1046ARDB board. When I am trying to connect a USB 3.0 device using USB 3.0 micro AB port on the board, it says its USB 2.0. However, it should be USB 3.0.&lt;/P&gt;&lt;P&gt;I want to use USB 3.0 but I am unable to do so. I tried changing the wire and also tried connecting different device compatible with USB 3.0 but USB 3.0 micro AB port says it 2.0.&lt;/P&gt;&lt;P&gt;I have checked the reference sheet, it says 3.0 but when I connect something its say its USB 2.0. I am using all the wires provided in the kit.&lt;/P&gt;&lt;P&gt;Can someone please guide me how I can change the behavior of USB 3.0 micro AB to USB 3.0.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 27 Jun 2023 00:09:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/USB-3-0-micro-AB-acting-as-USB-2-0/m-p/1676400#M12719</guid>
      <dc:creator>Sarthak</dc:creator>
      <dc:date>2023-06-27T00:09:08Z</dc:date>
    </item>
    <item>
      <title>Re: USB 3.0 micro AB acting as USB 2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/USB-3-0-micro-AB-acting-as-USB-2-0/m-p/1677644#M12738</link>
      <description>&lt;P&gt;Please refer to my u-boot console log, USB 3.0 device was detected successfully without any problem.&lt;/P&gt;
&lt;P&gt;Which version LSDK are you using? Would you please provide your u-boot console log?&lt;/P&gt;
&lt;P&gt;U-Boot 2020.04-gf46a944f71 (Dec 11 2020 - 04:34:39 +0800)&lt;/P&gt;
&lt;P&gt;SoC: LS1046AE Rev1.0 (0x87070010)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;CPU0(A72):1800 MHz CPU1(A72):1800 MHz CPU2(A72):1800 MHz&lt;BR /&gt;CPU3(A72):1800 MHz&lt;BR /&gt;Bus: 700 MHz DDR: 2100 MT/s FMAN: 800 MHz&lt;BR /&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 0e150012 10000000 00000000 00000000&lt;BR /&gt;00000010: 11335559 40005012 40025000 c1000000&lt;BR /&gt;00000020: 00000000 00000000 00000000 00238800&lt;BR /&gt;00000030: 20124000 00003101 00000096 00000001&lt;BR /&gt;Model: LS1046A RDB Board&lt;BR /&gt;Board: LS1046ARDB, boot from QSPI vBank 0&lt;BR /&gt;CPLD: V2.3&lt;BR /&gt;PCBA: V2.0&lt;BR /&gt;SERDES Reference Clocks:&lt;BR /&gt;SD1_CLK1 = 156.25MHZ, SD1_CLK2 = 100.00MHZ&lt;BR /&gt;DRAM: 7.9 GiB (DDR4, 64-bit, CL=15, ECC on)&lt;BR /&gt;DDR Chip-Select Interleaving Mode: CS0+CS1&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;Using SERDES1 Protocol: 4403 (0x1133)&lt;BR /&gt;Using SERDES2 Protocol: 21849 (0x5559)&lt;BR /&gt;NAND: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0&lt;BR /&gt;Loading Environment from SPI Flash... SF: Detected s25fs512s with page size 256 Bytes, erase size 256 KiB, total 64 MiB&lt;BR /&gt;OK&lt;BR /&gt;EEPROM: NXID v1&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: SF: Detected s25fs512s with page size 256 Bytes, erase size 256 KiB, total 64 MiB&lt;BR /&gt;Fman1: Uploading microcode version 106.4.18&lt;BR /&gt;PCIe1: pcie@3400000 Root Complex: no link&lt;BR /&gt;PCIe2: pcie@3500000 Root Complex: no link&lt;BR /&gt;PCIe3: pcie@3600000 Root Complex: x1 gen1&lt;BR /&gt;e1000: 68:05:ca:35:6d:ec&lt;BR /&gt;FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5, FM1@DTSEC6, FM1@TGEC1, FM1@TGEC2, e1000#0 [PRIME]&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;=&amp;gt; usb info&lt;BR /&gt;USB is stopped. Please issue 'usb start' first.&lt;BR /&gt;=&amp;gt; usb start&lt;BR /&gt;starting USB...&lt;BR /&gt;Bus usb@2f00000: Register 200017f NbrPorts 2&lt;BR /&gt;Starting the controller&lt;BR /&gt;USB XHCI 1.00&lt;BR /&gt;Bus usb@3000000: Register 200017f NbrPorts 2&lt;BR /&gt;Starting the controller&lt;BR /&gt;USB XHCI 1.00&lt;BR /&gt;Bus usb@3100000: Register 200017f NbrPorts 2&lt;BR /&gt;Starting the controller&lt;BR /&gt;USB XHCI 1.00&lt;BR /&gt;scanning bus usb@2f00000 for devices... 2 USB Device(s) found&lt;BR /&gt;scanning bus usb@3000000 for devices... 2 USB Device(s) found&lt;BR /&gt;scanning bus usb@3100000 for devices... 1 USB Device(s) found&lt;BR /&gt;scanning usb for storage devices... 2 Storage Device(s) found&lt;BR /&gt;=&amp;gt; usb info&lt;BR /&gt;1: Hub, USB Revision 3.0&lt;BR /&gt;- U-Boot XHCI Host Controller&lt;BR /&gt;- Class: Hub&lt;BR /&gt;- PacketSize: 512 Configurations: 1&lt;BR /&gt;- Vendor: 0x0000 Product 0x0000 Version 1.0&lt;BR /&gt;Configuration: 1&lt;BR /&gt;- Interfaces: 1 Self Powered 0mA&lt;BR /&gt;Interface: 0&lt;BR /&gt;- Alternate Setting 0, Endpoints: 1&lt;BR /&gt;- Class Hub&lt;BR /&gt;- Endpoint 1 In Interrupt MaxPacket 8 Interval 255ms&lt;/P&gt;
&lt;P&gt;2: Mass Storage, USB Revision 3.0&lt;BR /&gt;- SanDisk Ultra USB 3.0 4C531001530430115561&lt;BR /&gt;- Class: (from Interface) Mass Storage&lt;BR /&gt;- PacketSize: 512 Configurations: 1&lt;BR /&gt;- Vendor: 0x0781 Product 0x5591 Version 1.0&lt;BR /&gt;Configuration: 1&lt;BR /&gt;- Interfaces: 1 Bus Powered 224mA&lt;BR /&gt;Interface: 0&lt;BR /&gt;- Alternate Setting 0, Endpoints: 2&lt;BR /&gt;- Class Mass Storage, Transp. SCSI, Bulk only&lt;BR /&gt;- Endpoint 1 In Bulk MaxPacket 1024&lt;BR /&gt;- Endpoint 2 Out Bulk MaxPacket 1024&lt;/P&gt;
&lt;P&gt;1: Hub, USB Revision 3.0&lt;BR /&gt;- U-Boot XHCI Host Controller&lt;BR /&gt;- Class: Hub&lt;BR /&gt;- PacketSize: 512 Configurations: 1&lt;BR /&gt;- Vendor: 0x0000 Product 0x0000 Version 1.0&lt;BR /&gt;Configuration: 1&lt;BR /&gt;- Interfaces: 1 Self Powered 0mA&lt;BR /&gt;Interface: 0&lt;BR /&gt;- Alternate Setting 0, Endpoints: 1&lt;BR /&gt;- Class Hub&lt;BR /&gt;- Endpoint 1 In Interrupt MaxPacket 8 Interval 255ms&lt;/P&gt;
&lt;P&gt;2: Mass Storage, USB Revision 3.0&lt;BR /&gt;- Kingston DataTraveler 3.0 60A44CB1AB9DBFA084600214&lt;BR /&gt;- Class: (from Interface) Mass Storage&lt;BR /&gt;- PacketSize: 512 Configurations: 1&lt;BR /&gt;- Vendor: 0x0951 Product 0x1666 Version 1.0&lt;BR /&gt;Configuration: 1&lt;BR /&gt;- Interfaces: 1 Bus Powered 224mA&lt;BR /&gt;Interface: 0&lt;BR /&gt;- Alternate Setting 0, Endpoints: 2&lt;BR /&gt;- Class Mass Storage, Transp. SCSI, Bulk only&lt;BR /&gt;- Endpoint 1 In Bulk MaxPacket 1024&lt;BR /&gt;- Endpoint 2 Out Bulk MaxPacket 1024&lt;/P&gt;
&lt;P&gt;1: Hub, USB Revision 3.0&lt;BR /&gt;- U-Boot XHCI Host Controller&lt;BR /&gt;- Class: Hub&lt;BR /&gt;- PacketSize: 512 Configurations: 1&lt;BR /&gt;- Vendor: 0x0000 Product 0x0000 Version 1.0&lt;BR /&gt;Configuration: 1&lt;BR /&gt;- Interfaces: 1 Self Powered 0mA&lt;BR /&gt;Interface: 0&lt;BR /&gt;- Alternate Setting 0, Endpoints: 1&lt;BR /&gt;- Class Hub&lt;BR /&gt;- Endpoint 1 In Interrupt MaxPacket 8 Interval 255ms&lt;/P&gt;
&lt;P&gt;=&amp;gt;&lt;/P&gt;</description>
      <pubDate>Wed, 28 Jun 2023 07:54:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/USB-3-0-micro-AB-acting-as-USB-2-0/m-p/1677644#M12738</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-06-28T07:54:42Z</dc:date>
    </item>
    <item>
      <title>Re: USB 3.0 micro AB acting as USB 2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/USB-3-0-micro-AB-acting-as-USB-2-0/m-p/1678169#M12747</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thanks for quick reply&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;LSDK version = LSDK-21.08-0-g340b20bcb&lt;/P&gt;&lt;P&gt;OS = Ubuntu 20.04.5 LTS&lt;/P&gt;&lt;P&gt;Also I am attaching an image where it is recognizing as usb2.0&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;NOTICE: 16 GB DDR4, 64-bit, CL=15, ECC on, CS0+CS1&lt;BR /&gt;NOTICE: BL2: v2.4(release):LSDK-21.08-0-g340b20bcb&lt;BR /&gt;NOTICE: BL2: Built : 22:21:38, Aug 27 2021&lt;BR /&gt;NOTICE: BL2: Booting BL31&lt;BR /&gt;NOTICE: BL31: v2.4(release):LSDK-21.08-0-g340b20bcb&lt;BR /&gt;NOTICE: BL31: Built : 22:21:34, Aug 27 2021&lt;BR /&gt;NOTICE: Welcome to ls1046ardb BL31 Phase&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;U-Boot 2021.04-ge2eba0cd58 (Aug 27 2021 - 22:20:55 +0800)&lt;/P&gt;&lt;P&gt;SoC: LS1046AE Rev1.0 (0x87070010)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;CPU0(A72):1800 MHz CPU1(A72):1800 MHz CPU2(A72):1800 MHz&lt;BR /&gt;CPU3(A72):1800 MHz&lt;BR /&gt;Bus: 700 MHz DDR: 2100 MT/s FMAN: 800 MHz&lt;BR /&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 0e150012 10000000 00000000 00000000&lt;BR /&gt;00000010: 11335559 40005012 40025000 c1000000&lt;BR /&gt;00000020: 00000000 00000000 00000000 00238800&lt;BR /&gt;00000030: 20124000 00003101 00000096 00000001&lt;BR /&gt;Model: LS1046A RDB Board&lt;BR /&gt;Board: LS1046ARDB, boot from QSPI vBank 0&lt;BR /&gt;CPLD: V2.3&lt;BR /&gt;PCBA: V3.0&lt;BR /&gt;SERDES Reference Clocks:&lt;BR /&gt;SD1_CLK1 = 156.25MHZ, SD1_CLK2 = 100.00MHZ&lt;BR /&gt;DRAM: 15.9 GiB (DDR4, 64-bit, CL=15, ECC on)&lt;BR /&gt;DDR Chip-Select Interleaving Mode: CS0+CS1&lt;BR /&gt;Using SERDES1 Protocol: 4403 (0x1133)&lt;BR /&gt;Using SERDES2 Protocol: 21849 (0x5559)&lt;BR /&gt;NAND: 512 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0&lt;BR /&gt;Loading Environment from SPIFlash... SF: Detected s25fs512s with page size 256 B&lt;BR /&gt;OK&lt;BR /&gt;EEPROM: NXID v1&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;SEC0: RNG instantiated&lt;BR /&gt;Net: SF: Detected s25fs512s with page size 256 Bytes, erase size 256 KiB, totB&lt;BR /&gt;Fman1: Uploading microcode version 106.4.18&lt;BR /&gt;eth0: fm1-mac3, eth1: fm1-mac4, eth2: fm1-mac5, eth3: fm1-mac6, eth4: fm1-mac9,0&lt;BR /&gt;Hit any key to stop autoboot: 0&lt;BR /&gt;=&amp;gt; usb start&lt;BR /&gt;starting USB...&lt;BR /&gt;Bus usb@2f00000: Register 200017f NbrPorts 2&lt;BR /&gt;Starting the controller&lt;BR /&gt;USB XHCI 1.00&lt;BR /&gt;Bus usb@3000000: Register 200017f NbrPorts 2&lt;BR /&gt;Starting the controller&lt;BR /&gt;USB XHCI 1.00&lt;BR /&gt;Bus usb@3100000: Register 200017f NbrPorts 2&lt;BR /&gt;Starting the controller&lt;BR /&gt;USB XHCI 1.00&lt;BR /&gt;scanning bus usb@2f00000 for devices... 2 USB Device(s) found&lt;BR /&gt;scanning bus usb@3000000 for devices... 2 USB Device(s) found&lt;BR /&gt;scanning bus usb@3100000 for devices... 1 USB Device(s) found&lt;BR /&gt;scanning usb for storage devices... 2 Storage Device(s) found&lt;BR /&gt;=&amp;gt; usb info&lt;BR /&gt;1: Hub, USB Revision 3.0&lt;BR /&gt;- U-Boot XHCI Host Controller&lt;BR /&gt;- Class: Hub&lt;BR /&gt;- PacketSize: 512 Configurations: 1&lt;BR /&gt;- Vendor: 0x0000 Product 0x0000 Version 1.0&lt;BR /&gt;Configuration: 1&lt;BR /&gt;- Interfaces: 1 Self Powered 0mA&lt;BR /&gt;Interface: 0&lt;BR /&gt;- Alternate Setting 0, Endpoints: 1&lt;BR /&gt;- Class Hub&lt;BR /&gt;- Endpoint 1 In Interrupt MaxPacket 8 Interval 255ms&lt;BR /&gt;&lt;BR /&gt;2: Mass Storage, USB Revision 3.20&lt;BR /&gt;- USB SanDisk 3.2Gen1 0401ac76d4f76968c8cc0ae769694c6&lt;BR /&gt;- Class: (from Interface) Mass Storage&lt;BR /&gt;- PacketSize: 512 Configurations: 1&lt;BR /&gt;- Vendor: 0x0781 Product 0x5581 Version 1.0&lt;BR /&gt;Configuration: 1&lt;BR /&gt;- Interfaces: 1 Bus Powered 224mA&lt;BR /&gt;Interface: 0&lt;BR /&gt;- Alternate Setting 0, Endpoints: 2&lt;BR /&gt;- Class Mass Storage, Transp. SCSI, Bulk only&lt;BR /&gt;- Endpoint 1 In Bulk MaxPacket 1024&lt;BR /&gt;- Endpoint 2 Out Bulk MaxPacket 1024&lt;BR /&gt;&lt;BR /&gt;1: Hub, USB Revision 3.0&lt;BR /&gt;- U-Boot XHCI Host Controller&lt;BR /&gt;- Class: Hub&lt;BR /&gt;- PacketSize: 512 Configurations: 1&lt;BR /&gt;- Vendor: 0x0000 Product 0x0000 Version 1.0&lt;BR /&gt;Configuration: 1&lt;BR /&gt;- Interfaces: 1 Self Powered 0mA&lt;BR /&gt;Interface: 0&lt;BR /&gt;- Alternate Setting 0, Endpoints: 1&lt;BR /&gt;- Class Hub&lt;BR /&gt;- Endpoint 1 In Interrupt MaxPacket 8 Interval 255ms&lt;BR /&gt;&lt;BR /&gt;2: Mass Storage, USB Revision 3.0&lt;BR /&gt;- USB SanDisk 3.2Gen1 0901c7ea69703e26fd1a8446c2cdfd3&lt;BR /&gt;- Class: (from Interface) Mass Storage&lt;BR /&gt;- PacketSize: 512 Configurations: 1&lt;BR /&gt;- Vendor: 0x0781 Product 0x5581 Version 1.0&lt;BR /&gt;Configuration: 1&lt;BR /&gt;- Interfaces: 1 Bus Powered 224mA&lt;BR /&gt;Interface: 0&lt;BR /&gt;- Alternate Setting 0, Endpoints: 2&lt;BR /&gt;- Class Mass Storage, Transp. SCSI, Bulk only&lt;BR /&gt;- Endpoint 1 In Bulk MaxPacket 1024&lt;BR /&gt;- Endpoint 2 Out Bulk MaxPacket 1024&lt;BR /&gt;&lt;BR /&gt;1: Hub, USB Revision 3.0&lt;BR /&gt;- U-Boot XHCI Host Controller&lt;BR /&gt;- Class: Hub&lt;BR /&gt;- PacketSize: 512 Configurations: 1&lt;BR /&gt;- Vendor: 0x0000 Product 0x0000 Version 1.0&lt;BR /&gt;Configuration: 1&lt;BR /&gt;- Interfaces: 1 Self Powered 0mA&lt;BR /&gt;Interface: 0&lt;BR /&gt;- Alternate Setting 0, Endpoints: 1&lt;BR /&gt;- Class Hub&lt;BR /&gt;- Endpoint 1 In Interrupt MaxPacket 8 Interval 255ms&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jun 2023 00:59:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/USB-3-0-micro-AB-acting-as-USB-2-0/m-p/1678169#M12747</guid>
      <dc:creator>Sarthak</dc:creator>
      <dc:date>2023-06-29T00:59:31Z</dc:date>
    </item>
    <item>
      <title>Re: USB 3.0 micro AB acting as USB 2.0</title>
      <link>https://community.nxp.com/t5/Layerscape/USB-3-0-micro-AB-acting-as-USB-2-0/m-p/1684796#M12835</link>
      <description>&lt;P&gt;In your u-boot log,&amp;nbsp;&lt;SPAN&gt;Mass Storage devices are recognized as USB Revision 3.0, right?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jul 2023 10:23:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/USB-3-0-micro-AB-acting-as-USB-2-0/m-p/1684796#M12835</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-07-10T10:23:11Z</dc:date>
    </item>
  </channel>
</rss>