<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1028 switch dose not work in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028-switch-dose-not-work/m-p/1675479#M12715</link>
    <description>&lt;P&gt;Thanks yiping!&lt;/P&gt;&lt;P&gt;BTW，where can I see all methods of swtich settings?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;looking forward to your reply!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Sun, 25 Jun 2023 11:19:47 GMT</pubDate>
    <dc:creator>HingWong</dc:creator>
    <dc:date>2023-06-25T11:19:47Z</dc:date>
    <item>
      <title>LS1028 switch dose not work</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-switch-dose-not-work/m-p/1658061#M12560</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;How to configure the switch on LS1028 as a common switch, that is, self-learning type?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; I have now set eno2's IP address and plugged the network cable into swp0. eno2's IP cannot be pinged.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Does this configuration actually work at runtime, or does it have to be configured in the device tree?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 26 May 2023 04:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-switch-dose-not-work/m-p/1658061#M12560</guid>
      <dc:creator>HingWong</dc:creator>
      <dc:date>2023-05-26T04:09:37Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028 switch dose not work</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-switch-dose-not-work/m-p/1662488#M12596</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Run the following configure:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;# ip link add name br0 type bridge stp_state 0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;# ip link set swp0 master br0 &amp;amp;&amp;amp; ip link set swp0 up&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;# ip link set swp1 master br0 &amp;amp;&amp;amp; ip link set swp1 up&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;# ip link set swp2 master br0 &amp;amp;&amp;amp; ip link set swp2 up&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;# ip link set swp3 master br0 &amp;amp;&amp;amp; ip link set swp3 up&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;# ip link set br0 up&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Then ls1028a will work as an normal switch device. You can test it by connect two Ethernet devices with 2 of the swp ports and use ping to test.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 07:51:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-switch-dose-not-work/m-p/1662488#M12596</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-06-02T07:51:46Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028 switch dose not work</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-switch-dose-not-work/m-p/1675479#M12715</link>
      <description>&lt;P&gt;Thanks yiping!&lt;/P&gt;&lt;P&gt;BTW，where can I see all methods of swtich settings?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;looking forward to your reply!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 25 Jun 2023 11:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-switch-dose-not-work/m-p/1675479#M12715</guid>
      <dc:creator>HingWong</dc:creator>
      <dc:date>2023-06-25T11:19:47Z</dc:date>
    </item>
  </channel>
</rss>