<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックQuery on LX2160A SERDES Pin mapping</title>
    <link>https://community.nxp.com/t5/Layerscape/Query-on-LX2160A-SERDES-Pin-mapping/m-p/1672992#M12702</link>
    <description>&lt;P&gt;&lt;SPAN&gt;We are using LX210A Processor in our design, We have connected different interfaces in the same SERDES : For Example:If we connect the PCIe on Lane 4,5, SGMII on Lane6 and SGMII on Lane 7 ,Is necessary to provide GNDS/NC in between the pins. Please suggest us the solution in detail.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 20 Jun 2023 20:00:16 GMT</pubDate>
    <dc:creator>Aathi1122000</dc:creator>
    <dc:date>2023-06-20T20:00:16Z</dc:date>
    <item>
      <title>Query on LX2160A SERDES Pin mapping</title>
      <link>https://community.nxp.com/t5/Layerscape/Query-on-LX2160A-SERDES-Pin-mapping/m-p/1672992#M12702</link>
      <description>&lt;P&gt;&lt;SPAN&gt;We are using LX210A Processor in our design, We have connected different interfaces in the same SERDES : For Example:If we connect the PCIe on Lane 4,5, SGMII on Lane6 and SGMII on Lane 7 ,Is necessary to provide GNDS/NC in between the pins. Please suggest us the solution in detail.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Jun 2023 20:00:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Query-on-LX2160A-SERDES-Pin-mapping/m-p/1672992#M12702</guid>
      <dc:creator>Aathi1122000</dc:creator>
      <dc:date>2023-06-20T20:00:16Z</dc:date>
    </item>
    <item>
      <title>Re: Query on LX2160A SERDES Pin mapping</title>
      <link>https://community.nxp.com/t5/Layerscape/Query-on-LX2160A-SERDES-Pin-mapping/m-p/1681476#M12781</link>
      <description>&lt;P&gt;&lt;SPAN&gt;LX2160 has a fixed ball map and if there are GND or NC pins in between then use them. For not used interface, refer LX2160 design checklist for guidelines.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 05 Jul 2023 01:22:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Query-on-LX2160A-SERDES-Pin-mapping/m-p/1681476#M12781</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-07-05T01:22:31Z</dc:date>
    </item>
  </channel>
</rss>