<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1046ARDB accessories -RJ45-to-DB9F compatibility and pin configuration. in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-accessories-RJ45-to-DB9F-compatibility-and-pin/m-p/1664771#M12621</link>
    <description>&lt;P&gt;Please refer to the following link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.juniper.net/documentation/us/en/hardware/mx2020/srx4600/topics/concept/port-rj45-db9-adapter-pinout.html" target="_blank"&gt;https://www.juniper.net/documentation/us/en/hardware/mx2020/srx4600/topics/concept/port-rj45-db9-adapter-pinout.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.digi.com/support/knowledge-base/using-an-rj45-adapter-to-connect-to-a-db9-connecto" target="_blank"&gt;https://www.digi.com/support/knowledge-base/using-an-rj45-adapter-to-connect-to-a-db9-connecto&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jun 2023 03:42:38 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2023-06-07T03:42:38Z</dc:date>
    <item>
      <title>LS1046ARDB accessories -RJ45-to-DB9F compatibility and pin configuration.</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-accessories-RJ45-to-DB9F-compatibility-and-pin/m-p/1662239#M12594</link>
      <description>&lt;P&gt;We are developing a module with an LS1046A processor. We use a micro-D (D-Sub) 9-pin connector (instead of RJ45) to achieve 1GbE. We also have an LS1046ARDB which comes with a RJ45-to-DB9F cable. I was wondering if we could use the cable assembly (RJ45-to-DB9F) in our module to communicate with the PC through Ethernet protocol.&lt;/P&gt;&lt;P&gt;RJ45-to-DB9F cable setup:-The RJ45 UTP will be connected to the RJ45 Female jack on the PC and the DB9F will be connected to a micro-D connector in our module.&lt;/P&gt;&lt;P&gt;Would you please provide us with the pin configuration of the RJ45-to-DB9F cable? It helps us to configure the micro-D connector in our module.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your support.&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 01:05:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-accessories-RJ45-to-DB9F-compatibility-and-pin/m-p/1662239#M12594</guid>
      <dc:creator>Kavinravi</dc:creator>
      <dc:date>2023-06-02T01:05:21Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB accessories -RJ45-to-DB9F compatibility and pin configuration.</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-accessories-RJ45-to-DB9F-compatibility-and-pin/m-p/1664771#M12621</link>
      <description>&lt;P&gt;Please refer to the following link.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.juniper.net/documentation/us/en/hardware/mx2020/srx4600/topics/concept/port-rj45-db9-adapter-pinout.html" target="_blank"&gt;https://www.juniper.net/documentation/us/en/hardware/mx2020/srx4600/topics/concept/port-rj45-db9-adapter-pinout.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.digi.com/support/knowledge-base/using-an-rj45-adapter-to-connect-to-a-db9-connecto" target="_blank"&gt;https://www.digi.com/support/knowledge-base/using-an-rj45-adapter-to-connect-to-a-db9-connecto&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jun 2023 03:42:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-accessories-RJ45-to-DB9F-compatibility-and-pin/m-p/1664771#M12621</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-06-07T03:42:38Z</dc:date>
    </item>
  </channel>
</rss>