<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Secure Debug Controller for LS1046A in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1664702#M12618</link>
    <description>&lt;P&gt;&lt;SPAN&gt;All the fuse are blown once bit. Once you burn a fuse bit from b'0 to a b'1, you cannot turn a fuse b'1 back to a b'0. That is why the &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;OEM Security Policy Register 1 (SFP_OSPR1), bit 29–31 DBLEV&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; 000 Open: Debug portals are enabled unconditionally.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; 001 Conditionally closed via challenge response, without notification.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; 01x 01x: Conditionally closed via challenge response, with notification.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; 1xx 1xx: Closed. All debug portals are disabled.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;instead of use decimal value 1,2,3,4.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Back to Q1, you have to blown the fuse. Burning the debug response value register just prepare the prepare for secure boot. You need to program SFP_OSPR to activate it.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 07 Jun 2023 02:07:33 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2023-06-07T02:07:33Z</dc:date>
    <item>
      <title>Secure Debug Controller for LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1664150#M12608</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I need few clarifications on Secure debug controller for LS1046A RDB and have few questions :&lt;/P&gt;&lt;P&gt;1) Can Secure debug be enabled without blowing fuses by just writing debug response value to mirror registers?&lt;/P&gt;&lt;P&gt;2)If Secure Debug controller is enabled by blowing the&amp;nbsp; fuses permanently,&amp;nbsp; Is it possible to switch&amp;nbsp; between debug levels like level 1 to Level 0 and level 0 to level 3 and so on.?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any help/suggestions would be appreciated.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Faizan&lt;/P&gt;</description>
      <pubDate>Tue, 06 Jun 2023 08:53:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1664150#M12608</guid>
      <dc:creator>Faizanbaig</dc:creator>
      <dc:date>2023-06-06T08:53:36Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Debug Controller for LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1664702#M12618</link>
      <description>&lt;P&gt;&lt;SPAN&gt;All the fuse are blown once bit. Once you burn a fuse bit from b'0 to a b'1, you cannot turn a fuse b'1 back to a b'0. That is why the &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;OEM Security Policy Register 1 (SFP_OSPR1), bit 29–31 DBLEV&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; 000 Open: Debug portals are enabled unconditionally.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; 001 Conditionally closed via challenge response, without notification.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; 01x 01x: Conditionally closed via challenge response, with notification.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; 1xx 1xx: Closed. All debug portals are disabled.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;instead of use decimal value 1,2,3,4.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Back to Q1, you have to blown the fuse. Burning the debug response value register just prepare the prepare for secure boot. You need to program SFP_OSPR to activate it.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Jun 2023 02:07:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1664702#M12618</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-06-07T02:07:33Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Debug Controller for LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1678432#M12749</link>
      <description>Can we switch between these levels in lab environment?&lt;BR /&gt;Like if we enable level 3 , can we go back to level 0 again?</description>
      <pubDate>Thu, 29 Jun 2023 06:56:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1678432#M12749</guid>
      <dc:creator>Faizanbaig</dc:creator>
      <dc:date>2023-06-29T06:56:14Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Debug Controller for LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1684283#M12815</link>
      <description>&lt;P&gt;&lt;SPAN&gt;No, fuse burning is permanent. They cannot switch option back and forth.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jul 2023 00:29:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1684283#M12815</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-07-10T00:29:49Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Debug Controller for LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1684501#M12822</link>
      <description>Thanks for the response..&lt;BR /&gt;Any Mirror registers method or temporary writes?</description>
      <pubDate>Mon, 10 Jul 2023 05:43:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1684501#M12822</guid>
      <dc:creator>Faizanbaig</dc:creator>
      <dc:date>2023-07-10T05:43:23Z</dc:date>
    </item>
    <item>
      <title>Re: Secure Debug Controller for LS1046A</title>
      <link>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1685251#M12840</link>
      <description>&lt;P&gt;No method for temporary writing.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;You have to blown the fuse. Burning the debug response value register just prepare the prepare for secure boot. You need to program SFP_OSPR to activate it.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 11 Jul 2023 01:53:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Secure-Debug-Controller-for-LS1046A/m-p/1685251#M12840</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-07-11T01:53:33Z</dc:date>
    </item>
  </channel>
</rss>