<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: UART registar (UARTMISC) specifications for LX2160A</title>
    <link>https://community.nxp.com/t5/Layerscape/UART-registar-UARTMISC-specifications-for-LX2160A/m-p/1662492#M12597</link>
    <description>&lt;P&gt;&lt;SPAN&gt;When I checked the operation with the evaluation board, the reception interrupt occurs by setting 1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;--&amp;gt; According to the provided register dump, when you write to the UARTIMSC register (all interrupt mask set), no bit is set in UARTRIS. This means that you are not receiving any interrupts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please provide the steps to reproduce this issue on LX2160ARDB.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 02 Jun 2023 07:58:16 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2023-06-02T07:58:16Z</dc:date>
    <item>
      <title>UART registar (UARTMISC) specifications for LX2160A</title>
      <link>https://community.nxp.com/t5/Layerscape/UART-registar-UARTMISC-specifications-for-LX2160A/m-p/1653424#M12518</link>
      <description>&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;Regarding the behavior of the UARTMISC register, I think there is a difference between the document description and the implementation.By setting 1, is it correct that "Interrupts occur when the interrupt mask is released"?&lt;/P&gt;&lt;P&gt;According to Section 29.6.1.10 of the QorIQ LX 2160 A Reference Manual, Rev. 1, 10/2021, with the following statement,it has been determined that "Interrupt Mask Settings" is 1.&lt;/P&gt;&lt;P&gt;The UARTIMSC register is the interrupt mask set/clear register. It is a read/write register.&lt;BR /&gt;On a read this register returns the current value of the mask on the relevant interrupt. On a write of 1 to the particular bit, it sets the corresponding mask of that interrupt. A write of 0 clears the corresponding mask. All the bits are cleared to 0 when reset.&lt;/P&gt;&lt;P&gt;When I checked the operation with the evaluation board, the reception interrupt occurs by setting 1.&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best regards.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 19 May 2023 01:39:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/UART-registar-UARTMISC-specifications-for-LX2160A/m-p/1653424#M12518</guid>
      <dc:creator>shiota_kotaro</dc:creator>
      <dc:date>2023-05-19T01:39:13Z</dc:date>
    </item>
    <item>
      <title>Re: UART registar (UARTMISC) specifications for LX2160A</title>
      <link>https://community.nxp.com/t5/Layerscape/UART-registar-UARTMISC-specifications-for-LX2160A/m-p/1659387#M12570</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Can you please provide the UART register dump before and after writing to the UARTIMSC register.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 30 May 2023 02:14:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/UART-registar-UARTMISC-specifications-for-LX2160A/m-p/1659387#M12570</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-05-30T02:14:31Z</dc:date>
    </item>
    <item>
      <title>Re: UART registar (UARTMISC) specifications for LX2160A</title>
      <link>https://community.nxp.com/t5/Layerscape/UART-registar-UARTMISC-specifications-for-LX2160A/m-p/1661487#M12587</link>
      <description>&lt;P&gt;The collected information is attached. (collected on TRACE 32)&lt;/P&gt;</description>
      <pubDate>Thu, 01 Jun 2023 05:33:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/UART-registar-UARTMISC-specifications-for-LX2160A/m-p/1661487#M12587</guid>
      <dc:creator>shiota_kotaro</dc:creator>
      <dc:date>2023-06-01T05:33:53Z</dc:date>
    </item>
    <item>
      <title>Re: UART registar (UARTMISC) specifications for LX2160A</title>
      <link>https://community.nxp.com/t5/Layerscape/UART-registar-UARTMISC-specifications-for-LX2160A/m-p/1662492#M12597</link>
      <description>&lt;P&gt;&lt;SPAN&gt;When I checked the operation with the evaluation board, the reception interrupt occurs by setting 1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;--&amp;gt; According to the provided register dump, when you write to the UARTIMSC register (all interrupt mask set), no bit is set in UARTRIS. This means that you are not receiving any interrupts.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Please provide the steps to reproduce this issue on LX2160ARDB.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Jun 2023 07:58:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/UART-registar-UARTMISC-specifications-for-LX2160A/m-p/1662492#M12597</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-06-02T07:58:16Z</dc:date>
    </item>
  </channel>
</rss>