<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1046A not working now in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-not-working-now/m-p/1656399#M12541</link>
    <description>&lt;P&gt;Its working.&lt;/P&gt;&lt;P&gt;I followed &lt;A href="https://community.nxp.com/t5/Layerscape/LS1046A-RDB-not-booting-mbed-problem/m-p/723357/highlight/true" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Layerscape/LS1046A-RDB-not-booting-mbed-problem/m-p/723357/highlight/true&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 24 May 2023 07:40:12 GMT</pubDate>
    <dc:creator>Sarthak</dc:creator>
    <dc:date>2023-05-24T07:40:12Z</dc:date>
    <item>
      <title>LS1046A not working now</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-not-working-now/m-p/1656081#M12536</link>
      <description>&lt;DIV class=""&gt;&lt;DIV class=""&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Hello,&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;I am facing an issue with NXP LS1046A RDB. It was working well but suddenly its not connecting to the host. When I try to connect it to a linux host using minicom, it is not getting connected to ttyACM0. It throws "No such file or directory". It is connecting in bootloader mode and the led D8 is blinking .&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;After performing the usual process when I tap reset button, instead of connecting to tty serial port it is getting detected or connecting as a bootloader.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Minicom serial port setup:&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;| A - Serial Device : /dev/ttyACM0 |&lt;BR /&gt;| B - Lockfile Location : /var/lock |&lt;BR /&gt;| C - Callin Program : |&lt;BR /&gt;| D - Callout Program : |&lt;BR /&gt;| E - Bps/Par/Bits : 115200 8N1 |&lt;BR /&gt;| F - Hardware Flow Control : Yes |&lt;BR /&gt;| G - Software Flow Control : No &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Error:&lt;/P&gt;&lt;P&gt;minicom: cannot open /dev/ttyACM0: No such file or directory.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;SPAN class=""&gt;Please help me to solve this issue. &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Tue, 23 May 2023 23:47:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-not-working-now/m-p/1656081#M12536</guid>
      <dc:creator>Sarthak</dc:creator>
      <dc:date>2023-05-23T23:47:51Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A not working now</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-not-working-now/m-p/1656399#M12541</link>
      <description>&lt;P&gt;Its working.&lt;/P&gt;&lt;P&gt;I followed &lt;A href="https://community.nxp.com/t5/Layerscape/LS1046A-RDB-not-booting-mbed-problem/m-p/723357/highlight/true" target="_blank" rel="noopener"&gt;https://community.nxp.com/t5/Layerscape/LS1046A-RDB-not-booting-mbed-problem/m-p/723357/highlight/true&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 May 2023 07:40:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-not-working-now/m-p/1656399#M12541</guid>
      <dc:creator>Sarthak</dc:creator>
      <dc:date>2023-05-24T07:40:12Z</dc:date>
    </item>
  </channel>
</rss>