<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: [LS1046A]kernal panic issue when run iperf3 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-kernal-panic-issue-when-run-iperf3/m-p/1656142#M12537</link>
    <description>&lt;P&gt;Which version NXP LSDK are you using? Or where did you get Linux Kernel source code?&lt;/P&gt;
&lt;P&gt;Would you please send your Linux Kernel configuration file to me to do more investigation?&lt;/P&gt;</description>
    <pubDate>Wed, 24 May 2023 02:27:08 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2023-05-24T02:27:08Z</dc:date>
    <item>
      <title>[LS1046A]kernal panic issue when run iperf3</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-kernal-panic-issue-when-run-iperf3/m-p/1650646#M12473</link>
      <description>&lt;P&gt;Hi NXP,&lt;/P&gt;&lt;P&gt;I have some questions about kernal panic.&amp;nbsp;&amp;nbsp;I use LS1046A as the server side, and my PC as the client side.&lt;/P&gt;&lt;P&gt;PC through telnet and input commands: &lt;STRONG&gt;iperf3 -c 192.168.1.254 -t 600 -R&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;After about 10 seconds of testing, iperf is stopped, and an error log was seen. Also I have the same problem using both WAN and LAN ports, please refer to the attached file for detailed logs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Richard Guo&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 01:28:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-kernal-panic-issue-when-run-iperf3/m-p/1650646#M12473</guid>
      <dc:creator>richard_guo</dc:creator>
      <dc:date>2023-05-16T01:28:38Z</dc:date>
    </item>
    <item>
      <title>Re: [LS1046A]kernal panic issue when run iperf3</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-kernal-panic-issue-when-run-iperf3/m-p/1656142#M12537</link>
      <description>&lt;P&gt;Which version NXP LSDK are you using? Or where did you get Linux Kernel source code?&lt;/P&gt;
&lt;P&gt;Would you please send your Linux Kernel configuration file to me to do more investigation?&lt;/P&gt;</description>
      <pubDate>Wed, 24 May 2023 02:27:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-kernal-panic-issue-when-run-iperf3/m-p/1656142#M12537</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-05-24T02:27:08Z</dc:date>
    </item>
  </channel>
</rss>