<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1046 power sequencing</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046-power-sequencing/m-p/1650347#M12469</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm going to do the bring up of an LS1046 custom board.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The part 3.2 of the datasheet mention the following Power Sequencing :&lt;BR /&gt;1. OVDD, DVDD, LVDD, EVDD, TVDD, XVDD, AVDD_CGAn, AVDD_PLAT,&lt;BR /&gt;AVDD_D1, AVDD_SDn_PLL1, AVDD_SDn_PLL2, USB_HVDD. Drive&lt;BR /&gt;TA_PROG_SFP = GND.&lt;BR /&gt;• PORESET_B input must be driven asserted and held during this step.&lt;BR /&gt;2. VDD, SVDD, TA_BB_VDD, USB_SDVDD, USB_SVDD&lt;BR /&gt;• The 3.3 V (USB_HVDD) in Step 1 and 1.0 V (USB_SDVDD, USB_SVDD) in&lt;BR /&gt;Step 2 supplies can power up in any sequence provided all these USB supplies&lt;BR /&gt;ramp up within 95 ms with respect to each other.&lt;BR /&gt;3. G1VDD&lt;BR /&gt;&lt;BR /&gt;Is there an issue or a risk to damage the processor if I power only the first sequence to check the power supplies signal integrity, and if I do the same for the second and third stage ?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Wilfrid&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 15 May 2023 13:27:50 GMT</pubDate>
    <dc:creator>WilfridBertrand</dc:creator>
    <dc:date>2023-05-15T13:27:50Z</dc:date>
    <item>
      <title>LS1046 power sequencing</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-power-sequencing/m-p/1650347#M12469</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm going to do the bring up of an LS1046 custom board.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;The part 3.2 of the datasheet mention the following Power Sequencing :&lt;BR /&gt;1. OVDD, DVDD, LVDD, EVDD, TVDD, XVDD, AVDD_CGAn, AVDD_PLAT,&lt;BR /&gt;AVDD_D1, AVDD_SDn_PLL1, AVDD_SDn_PLL2, USB_HVDD. Drive&lt;BR /&gt;TA_PROG_SFP = GND.&lt;BR /&gt;• PORESET_B input must be driven asserted and held during this step.&lt;BR /&gt;2. VDD, SVDD, TA_BB_VDD, USB_SDVDD, USB_SVDD&lt;BR /&gt;• The 3.3 V (USB_HVDD) in Step 1 and 1.0 V (USB_SDVDD, USB_SVDD) in&lt;BR /&gt;Step 2 supplies can power up in any sequence provided all these USB supplies&lt;BR /&gt;ramp up within 95 ms with respect to each other.&lt;BR /&gt;3. G1VDD&lt;BR /&gt;&lt;BR /&gt;Is there an issue or a risk to damage the processor if I power only the first sequence to check the power supplies signal integrity, and if I do the same for the second and third stage ?&lt;/P&gt;&lt;P&gt;Best regards,&lt;BR /&gt;Wilfrid&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 13:27:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-power-sequencing/m-p/1650347#M12469</guid>
      <dc:creator>WilfridBertrand</dc:creator>
      <dc:date>2023-05-15T13:27:50Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 power sequencing</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-power-sequencing/m-p/1650401#M12471</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/217295"&gt;@WilfridBertrand&lt;/a&gt;!&lt;/P&gt;
&lt;P&gt;Thank you for contacting NXP Support!&lt;/P&gt;
&lt;P&gt;If you don't follow the power sequencing you can experiment with random failures or in the worst of cases damage the processor.&lt;/P&gt;
&lt;P&gt;If you want to check by steps but in the order, I think is not dangerous for the processor, but I can't be sure of that, we don't have documentation about that.&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Alejandro.&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 14:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-power-sequencing/m-p/1650401#M12471</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2023-05-15T14:38:57Z</dc:date>
    </item>
  </channel>
</rss>