<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is there any way to write RCW, u-Boot into QSPI without an external rom writer? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Is-there-any-way-to-write-RCW-u-Boot-into-QSPI-without-an/m-p/1649828#M12464</link>
    <description>&lt;P&gt;in case of LS1012A board,&lt;/P&gt;&lt;P&gt;Is there any way to write RCW, u-Boot into QSPI without an external rom writer?&lt;/P&gt;&lt;P&gt;is it possible to write them into empty QSPI using JTAG?&lt;/P&gt;&lt;P&gt;or do I have to use external rom writer to write them into empty QSPI?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 15 May 2023 02:37:58 GMT</pubDate>
    <dc:creator>Woon</dc:creator>
    <dc:date>2023-05-15T02:37:58Z</dc:date>
    <item>
      <title>Is there any way to write RCW, u-Boot into QSPI without an external rom writer?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-there-any-way-to-write-RCW-u-Boot-into-QSPI-without-an/m-p/1649828#M12464</link>
      <description>&lt;P&gt;in case of LS1012A board,&lt;/P&gt;&lt;P&gt;Is there any way to write RCW, u-Boot into QSPI without an external rom writer?&lt;/P&gt;&lt;P&gt;is it possible to write them into empty QSPI using JTAG?&lt;/P&gt;&lt;P&gt;or do I have to use external rom writer to write them into empty QSPI?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 02:37:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-there-any-way-to-write-RCW-u-Boot-into-QSPI-without-an/m-p/1649828#M12464</guid>
      <dc:creator>Woon</dc:creator>
      <dc:date>2023-05-15T02:37:58Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any way to write RCW, u-Boot into QSPI without an external rom writer?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-there-any-way-to-write-RCW-u-Boot-into-QSPI-without-an/m-p/1650358#M12470</link>
      <description>&lt;P&gt;Woon,&lt;/P&gt;&lt;P&gt;The board you have is not from a Dev Kit from NXP? It is empty. Blank correct? You are not able to boot at power on correct?&lt;/P&gt;</description>
      <pubDate>Mon, 15 May 2023 13:48:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-there-any-way-to-write-RCW-u-Boot-into-QSPI-without-an/m-p/1650358#M12470</guid>
      <dc:creator>williawh</dc:creator>
      <dc:date>2023-05-15T13:48:34Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any way to write RCW, u-Boot into QSPI without an external rom writer?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-there-any-way-to-write-RCW-u-Boot-into-QSPI-without-an/m-p/1650748#M12477</link>
      <description>&lt;P&gt;the board is working well.&lt;/P&gt;&lt;P&gt;I just ask it for my custom board to development &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 04:50:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-there-any-way-to-write-RCW-u-Boot-into-QSPI-without-an/m-p/1650748#M12477</guid>
      <dc:creator>Woon</dc:creator>
      <dc:date>2023-05-16T04:50:21Z</dc:date>
    </item>
    <item>
      <title>Re: Is there any way to write RCW, u-Boot into QSPI without an external rom writer?</title>
      <link>https://community.nxp.com/t5/Layerscape/Is-there-any-way-to-write-RCW-u-Boot-into-QSPI-without-an/m-p/1651358#M12487</link>
      <description>&lt;P&gt;I see. We are doing something similar. Our engineer developing the prototype is using a ls1046a chip and has procured CodeWarrior and CodeWarrior TAP to load/flash the blank chip if that helps or tells you anything.&lt;/P&gt;</description>
      <pubDate>Tue, 16 May 2023 16:28:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Is-there-any-way-to-write-RCW-u-Boot-into-QSPI-without-an/m-p/1651358#M12487</guid>
      <dc:creator>williawh</dc:creator>
      <dc:date>2023-05-16T16:28:49Z</dc:date>
    </item>
  </channel>
</rss>