<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 LS1046 Dual 10G XFI PHY MDIO problem</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046-Dual-10G-XFI-PHY-MDIO-problem/m-p/1645949#M12413</link>
    <description>&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;On my customized board, i have a Broadcom BCM89890 10g phy connected to XFI.9 and a Marvell AQR113C 10g phy connected to XFI.10.&amp;nbsp; They share the same EMI2 mdc/mdio interface.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now XFI.10 AQR113C phy works ok but XFI.9 BCM89890 does not.&lt;/P&gt;&lt;P&gt;In uboot, when i read the BCM phy mdio register, the return is 0xff which seems incorrect. When i use a oscilloscope to probe, the waveform seems to be a MDIO C22 protocol while BCM89890 requires C45.&lt;/P&gt;&lt;P&gt;dts and eth.c are attached. Could you help to check where is wrong in the system.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Sat, 06 May 2023 15:22:15 GMT</pubDate>
    <dc:creator>daoyuS</dc:creator>
    <dc:date>2023-05-06T15:22:15Z</dc:date>
    <item>
      <title>LS1046 Dual 10G XFI PHY MDIO problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-Dual-10G-XFI-PHY-MDIO-problem/m-p/1645949#M12413</link>
      <description>&lt;P&gt;Hi，&lt;/P&gt;&lt;P&gt;On my customized board, i have a Broadcom BCM89890 10g phy connected to XFI.9 and a Marvell AQR113C 10g phy connected to XFI.10.&amp;nbsp; They share the same EMI2 mdc/mdio interface.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Now XFI.10 AQR113C phy works ok but XFI.9 BCM89890 does not.&lt;/P&gt;&lt;P&gt;In uboot, when i read the BCM phy mdio register, the return is 0xff which seems incorrect. When i use a oscilloscope to probe, the waveform seems to be a MDIO C22 protocol while BCM89890 requires C45.&lt;/P&gt;&lt;P&gt;dts and eth.c are attached. Could you help to check where is wrong in the system.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Sat, 06 May 2023 15:22:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-Dual-10G-XFI-PHY-MDIO-problem/m-p/1645949#M12413</guid>
      <dc:creator>daoyuS</dc:creator>
      <dc:date>2023-05-06T15:22:15Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046 Dual 10G XFI PHY MDIO problem</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046-Dual-10G-XFI-PHY-MDIO-problem/m-p/1647518#M12436</link>
      <description>&lt;P&gt;Please refer to the following update from the AE team.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Can you please share the u-boot commands used to read registers from both PHYs?&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;Since they are on the same bus, they should show the same Clause implementation if they are both CL45 devices.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;In u-boot, if you give two arguments, it will try CL22. If you give three arguments, it will try CL45.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;At the HW level, you can double check MDIO_CCFG[ENC45]=1 from the MDIO offsets.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;the offsets-&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MAC1 @ e_0000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MDIO-1 @ e_1000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MAC2 @ e_2000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MDIO-2 @ e_3000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MAC3 @ e_4000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MDIO-3 @ e_5000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MAC4 @ e_6000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MDIO-4 @ e_7000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MAC5 @ e_8000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MDIO-5 @ e_9000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MAC6 @ e_a000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MDIO-6 @ e_b000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MAC7 @ e_c000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MDIO-7 @ e_d000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MAC8 @ e_e000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MDIO-8 @ e_f000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MAC9 @ f_0000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MDIO-9 @ f_1000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MAC10 @ f_2000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;MDIO-10 @ f_3000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;EMI1 @ f_c000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;;EMI2 @ f_d000&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I'm also attaching an example TeraTerm macro I shared with another CAS member to read MDIO registers. His case was Linux but you can see the steps and modify Linux memory commands with u-boot memory commands.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 10 May 2023 02:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046-Dual-10G-XFI-PHY-MDIO-problem/m-p/1647518#M12436</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-05-10T02:24:44Z</dc:date>
    </item>
  </channel>
</rss>