<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: PLL selection between PCI lanes</title>
    <link>https://community.nxp.com/t5/Layerscape/PLL-selection-between-PCI-lanes/m-p/1644216#M12386</link>
    <description>&lt;P&gt;&lt;SPAN&gt;This will not work. For protocol 0x1040&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;VSC8514 QSGMII Phy should be on Lane 2 - SerDes 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;AQR113 10G Phy should be on Lane-0 - Serdes-1&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 04 May 2023 03:47:14 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2023-05-04T03:47:14Z</dc:date>
    <item>
      <title>PLL selection between PCI lanes</title>
      <link>https://community.nxp.com/t5/Layerscape/PLL-selection-between-PCI-lanes/m-p/1633765#M12263</link>
      <description>&lt;P&gt;Hi,&lt;BR /&gt;I have a custom LS1046A board with the following configuration:&lt;BR /&gt;- VSC8514 QSGMII Phy on Serdes-1 Lane-2&lt;BR /&gt;- AQR113 10G Phy on Serdes-1 Lane-0&lt;BR /&gt;- Serdes-1 PLL-1 is clocked with 100MHz&lt;BR /&gt;- Serdes-1 PLL-2 is clocked with 156.25MHz&lt;/P&gt;&lt;P&gt;Below are the RCW configuration settings corresponding to Serdes-1:&lt;BR /&gt;SRDS_PRTCL_S1 - 0x1040 (XFI.9 on Lane-0 and QSGMII.6,5,10,1 on Lane-2)&lt;BR /&gt;SRDS_PLL_REF_CLK_SEL_S1 -0b01 (Serdes-1 PLL-1 = Lower Frequency (100MHz) and Serdes-1 PLL-2=Higher Frequency (156.25MHz))&lt;BR /&gt;SRDS_PLL_PD_S1 - 0b00 (Both Serdes-1 PLL-1 and Serdes-1 PLL-2 are not powered down)&lt;BR /&gt;SRDS_DIV_PEX_S1 - 0b01&lt;BR /&gt;SRDS_REFCLK_SEL_S1 - 0b0 (Separate reference clocks to both PLLs of Serdes-1)&lt;BR /&gt;&lt;BR /&gt;The QSGMII MAC is not getting detected when I boot into linux.&lt;BR /&gt;Where should I specify the following:&lt;BR /&gt;- Lane-2 (on which VSC8514 is mounted) should use 100MHz from Serdes-1 PLL-1&lt;BR /&gt;- Lane-0 (on which AQR113 is mounted) should use 156.25MHz from Serdes-1 PLL-2&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Regards&lt;BR /&gt;Balaji.V&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 04:06:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PLL-selection-between-PCI-lanes/m-p/1633765#M12263</guid>
      <dc:creator>balaji_1709</dc:creator>
      <dc:date>2023-05-04T04:06:52Z</dc:date>
    </item>
    <item>
      <title>Re: PLL selection between PCI lanes</title>
      <link>https://community.nxp.com/t5/Layerscape/PLL-selection-between-PCI-lanes/m-p/1644216#M12386</link>
      <description>&lt;P&gt;&lt;SPAN&gt;This will not work. For protocol 0x1040&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;VSC8514 QSGMII Phy should be on Lane 2 - SerDes 1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;AQR113 10G Phy should be on Lane-0 - Serdes-1&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 03:47:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PLL-selection-between-PCI-lanes/m-p/1644216#M12386</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-05-04T03:47:14Z</dc:date>
    </item>
    <item>
      <title>Re: PLL selection between PCI lanes</title>
      <link>https://community.nxp.com/t5/Layerscape/PLL-selection-between-PCI-lanes/m-p/1644232#M12387</link>
      <description>&lt;P&gt;Thank you for your reply.&lt;/P&gt;&lt;P&gt;To answer my query,&lt;/P&gt;&lt;P&gt;2212 in the RM specifies the PLL that will be assigned to each serdes lane (PLL&lt;U&gt;2&lt;/U&gt; for Lane-0, PLL&lt;U&gt;2&lt;/U&gt; for Lane-1, PLL&lt;U&gt;1&lt;/U&gt; for Lane-2, PLL&lt;U&gt;2&lt;/U&gt; for Lane-3)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Balaji&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 04:12:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/PLL-selection-between-PCI-lanes/m-p/1644232#M12387</guid>
      <dc:creator>balaji_1709</dc:creator>
      <dc:date>2023-05-04T04:12:01Z</dc:date>
    </item>
  </channel>
</rss>