<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックProblem with LS1046A XFI Mac</title>
    <link>https://community.nxp.com/t5/Layerscape/Problem-with-LS1046A-XFI-Mac/m-p/1642907#M12368</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; We have a clone of LS1046A Freeway board. However it uses a 10G Phy. The connections are as per LS1046A RDB RevC. It is connected through XFI interface and the RCW is modified accordingly (Serdes-1 PRTCL = 1040). We are able to communicate with the Phy (using mdio-proxy &amp;amp; mdio-app). However the MAC (XFI.9) is not getting detected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a few questions in this regard:&lt;/P&gt;&lt;P&gt;1. Should we modify the ucode that is loaded during the u-boot phase for the XFI.9 to get detected?&lt;/P&gt;&lt;P&gt;2. I am attaching the currently used DTS file. Can you check it and let us know if it is ok?&lt;/P&gt;&lt;P&gt;I am also attaching the bootlog.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Balaji&lt;/P&gt;</description>
    <pubDate>Tue, 02 May 2023 06:41:10 GMT</pubDate>
    <dc:creator>balaji_1709</dc:creator>
    <dc:date>2023-05-02T06:41:10Z</dc:date>
    <item>
      <title>Problem with LS1046A XFI Mac</title>
      <link>https://community.nxp.com/t5/Layerscape/Problem-with-LS1046A-XFI-Mac/m-p/1642907#M12368</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; We have a clone of LS1046A Freeway board. However it uses a 10G Phy. The connections are as per LS1046A RDB RevC. It is connected through XFI interface and the RCW is modified accordingly (Serdes-1 PRTCL = 1040). We are able to communicate with the Phy (using mdio-proxy &amp;amp; mdio-app). However the MAC (XFI.9) is not getting detected.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have a few questions in this regard:&lt;/P&gt;&lt;P&gt;1. Should we modify the ucode that is loaded during the u-boot phase for the XFI.9 to get detected?&lt;/P&gt;&lt;P&gt;2. I am attaching the currently used DTS file. Can you check it and let us know if it is ok?&lt;/P&gt;&lt;P&gt;I am also attaching the bootlog.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Balaji&lt;/P&gt;</description>
      <pubDate>Tue, 02 May 2023 06:41:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Problem-with-LS1046A-XFI-Mac/m-p/1642907#M12368</guid>
      <dc:creator>balaji_1709</dc:creator>
      <dc:date>2023-05-02T06:41:10Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with LS1046A XFI Mac</title>
      <link>https://community.nxp.com/t5/Layerscape/Problem-with-LS1046A-XFI-Mac/m-p/1644237#M12388</link>
      <description>&lt;P&gt;Problem fixed. In my case, in u-boot, board/freescale/ls1046afrwy/eth.c: fdt_update_ethernet_dt method, we are disabling ethernet6 (that corresponds to MAC.9). If we remove these lines, then fm1-mac9 will be enumerated.&lt;/P&gt;&lt;PRE&gt;if (!strcmp(name, "ethernet6"))&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; fdt_status_disabled(blob, nodeoff);&lt;/PRE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps someone.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Balaji&lt;/P&gt;</description>
      <pubDate>Thu, 04 May 2023 04:21:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Problem-with-LS1046A-XFI-Mac/m-p/1644237#M12388</guid>
      <dc:creator>balaji_1709</dc:creator>
      <dc:date>2023-05-04T04:21:52Z</dc:date>
    </item>
  </channel>
</rss>