<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1043 Hreset in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043-Hreset/m-p/1642015#M12359</link>
    <description>&lt;P&gt;Please refer to section "4.3 Power-on reset recommendations" in the attached application note.&lt;/P&gt;</description>
    <pubDate>Fri, 28 Apr 2023 06:22:49 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2023-04-28T06:22:49Z</dc:date>
    <item>
      <title>LS1043 Hreset</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043-Hreset/m-p/1631942#M12241</link>
      <description>&lt;P&gt;LS1043 reset circuit：&lt;/P&gt;&lt;P&gt;The connection relationship is shown in the figure：&lt;/P&gt;&lt;P&gt;one PMIC，&lt;SPAN&gt;model is MC34VR500VAES.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;one FPGA，&lt;SPAN&gt;model is xc7a15tcsg324.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;one LS1043，&lt;SPAN&gt;model is LS1043AXE7QQB.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;one power-on reset chip U3，model is ADM8611N293ACBZ-R7.&lt;/P&gt;&lt;P&gt;two input and gate U1, U2, model is 74LVC1G08.&lt;/P&gt;&lt;P&gt;one OCTAL BUFFERS/DRIVERS WITH 3-STATE OUTPUTS U4，model is SN74LVCH244APW.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="crazy210_0-1681288480514.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/218903i05AC46B657460A74/image-size/medium?v=v2&amp;amp;px=400" role="button" title="crazy210_0-1681288480514.png" alt="crazy210_0-1681288480514.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="crazy210_1-1681288480607.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/218904i2FB36C7353E35A2C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="crazy210_1-1681288480607.png" alt="crazy210_1-1681288480607.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The follow is a detailed description of the circuit:&lt;/P&gt;&lt;P&gt;The pin 1 of U1 is connected to the power-on status output of PMIC, it indicates that the PMIC is powered on. The pin 2 of U1 are disconnected during operation.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;U3 is a 200ms power-on reset, the output of U1 and the output&lt;/SPAN&gt;&lt;SPAN&gt; of &lt;/SPAN&gt;&lt;SPAN&gt;U3 output a reset through U2 AND gate, which is connected to pin 2 and pin 4 of U4 as inputs. Pin 18 and pin 16 of U4 are output pins, respectively are connected to FPGA, LS1043. HRRESET_B_18 and PORESET_B_18, which are all pulled up to 1.8v. &amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Why is HRESET_B_18 only 700Mv? See the yellow waveform below, the blue waveform is PORESET_B_18, and the waveform is 1.8V, What is the reason?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="crazy210_2-1681288482533.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/218905i377861C2F399E66A/image-size/medium?v=v2&amp;amp;px=400" role="button" title="crazy210_2-1681288482533.png" alt="crazy210_2-1681288482533.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 12 Apr 2023 08:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043-Hreset/m-p/1631942#M12241</guid>
      <dc:creator>crazy210</dc:creator>
      <dc:date>2023-04-12T08:34:54Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043 Hreset</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043-Hreset/m-p/1642015#M12359</link>
      <description>&lt;P&gt;Please refer to section "4.3 Power-on reset recommendations" in the attached application note.&lt;/P&gt;</description>
      <pubDate>Fri, 28 Apr 2023 06:22:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043-Hreset/m-p/1642015#M12359</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-04-28T06:22:49Z</dc:date>
    </item>
  </channel>
</rss>