<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Can the tiny Linux set the ssh or telnet startup service or not?</title>
    <link>https://community.nxp.com/t5/Layerscape/Can-the-tiny-Linux-set-the-ssh-or-telnet-startup-service-or-not/m-p/1636862#M12298</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Our project uses the LS1084 and the LS1046.&lt;BR /&gt;Our setting is to boot up from the NOR flash and load the system in eMMC.&lt;BR /&gt;We want to know that if the eMMC partition is corrupted, it boots to the tiny Linux system.&lt;BR /&gt;Does Tiny Linux have a way to set the ssh or telnet daemon can execute automatically after startup?&lt;BR /&gt;We want to connect to tiny Linux with ssh or telnet without going through the console.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Thu, 20 Apr 2023 03:25:16 GMT</pubDate>
    <dc:creator>tzongruey</dc:creator>
    <dc:date>2023-04-20T03:25:16Z</dc:date>
    <item>
      <title>Can the tiny Linux set the ssh or telnet startup service or not?</title>
      <link>https://community.nxp.com/t5/Layerscape/Can-the-tiny-Linux-set-the-ssh-or-telnet-startup-service-or-not/m-p/1636862#M12298</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Our project uses the LS1084 and the LS1046.&lt;BR /&gt;Our setting is to boot up from the NOR flash and load the system in eMMC.&lt;BR /&gt;We want to know that if the eMMC partition is corrupted, it boots to the tiny Linux system.&lt;BR /&gt;Does Tiny Linux have a way to set the ssh or telnet daemon can execute automatically after startup?&lt;BR /&gt;We want to connect to tiny Linux with ssh or telnet without going through the console.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 20 Apr 2023 03:25:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Can-the-tiny-Linux-set-the-ssh-or-telnet-startup-service-or-not/m-p/1636862#M12298</guid>
      <dc:creator>tzongruey</dc:creator>
      <dc:date>2023-04-20T03:25:16Z</dc:date>
    </item>
  </channel>
</rss>