<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: GPU on the LS1028A in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/GPU-on-the-LS1028A/m-p/1621832#M12087</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;There isn't a status flag in hardware but you can disable the GPU by the&lt;/P&gt;
&lt;P&gt;Device Disable Register 6 (DEVDISR6)&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It is a R/W register so you can read it to verify that it is disabled.&lt;/P&gt;</description>
    <pubDate>Fri, 24 Mar 2023 17:03:56 GMT</pubDate>
    <dc:creator>Oswalag</dc:creator>
    <dc:date>2023-03-24T17:03:56Z</dc:date>
    <item>
      <title>GPU on the LS1028A</title>
      <link>https://community.nxp.com/t5/Layerscape/GPU-on-the-LS1028A/m-p/1617056#M12052</link>
      <description>&lt;P&gt;I am using an LS1028A processor on an avoinics product. We do not need the GPU for the current project. I plan on turning off the GPU using a PBI command.&lt;/P&gt;&lt;P&gt;My question is about verifying if the GPU is actually off. Can you suggest a mechanism I can use to verify the GPU is actually off. This is needed for certification.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Mar 2023 18:29:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/GPU-on-the-LS1028A/m-p/1617056#M12052</guid>
      <dc:creator>rhaas</dc:creator>
      <dc:date>2023-03-16T18:29:49Z</dc:date>
    </item>
    <item>
      <title>Re: GPU on the LS1028A</title>
      <link>https://community.nxp.com/t5/Layerscape/GPU-on-the-LS1028A/m-p/1621832#M12087</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;There isn't a status flag in hardware but you can disable the GPU by the&lt;/P&gt;
&lt;P&gt;Device Disable Register 6 (DEVDISR6)&amp;nbsp;&lt;/P&gt;
&lt;P&gt;It is a R/W register so you can read it to verify that it is disabled.&lt;/P&gt;</description>
      <pubDate>Fri, 24 Mar 2023 17:03:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/GPU-on-the-LS1028A/m-p/1621832#M12087</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2023-03-24T17:03:56Z</dc:date>
    </item>
  </channel>
</rss>