<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Setting up multiple VLANs on a LX2160 in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Setting-up-multiple-VLANs-on-a-LX2160/m-p/1619901#M12070</link>
    <description>&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;Is it possible to configure multiple VLANs on a ethernet port of the LX2160 board ? I would like to be able to setup a switch that receives packets on a port and forwards them to two other ports based on the VLAN ID inside the packet.&lt;/P&gt;&lt;P&gt;I it is possible, could you explain to me how to set it up ?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Have a good day,&lt;/P&gt;&lt;P&gt;Nicolas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 22 Mar 2023 14:16:23 GMT</pubDate>
    <dc:creator>Ncaseau</dc:creator>
    <dc:date>2023-03-22T14:16:23Z</dc:date>
    <item>
      <title>Setting up multiple VLANs on a LX2160</title>
      <link>https://community.nxp.com/t5/Layerscape/Setting-up-multiple-VLANs-on-a-LX2160/m-p/1619901#M12070</link>
      <description>&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;Is it possible to configure multiple VLANs on a ethernet port of the LX2160 board ? I would like to be able to setup a switch that receives packets on a port and forwards them to two other ports based on the VLAN ID inside the packet.&lt;/P&gt;&lt;P&gt;I it is possible, could you explain to me how to set it up ?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;P&gt;Have a good day,&lt;/P&gt;&lt;P&gt;Nicolas&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 22 Mar 2023 14:16:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Setting-up-multiple-VLANs-on-a-LX2160/m-p/1619901#M12070</guid>
      <dc:creator>Ncaseau</dc:creator>
      <dc:date>2023-03-22T14:16:23Z</dc:date>
    </item>
    <item>
      <title>Re: Setting up multiple VLANs on a LX2160</title>
      <link>https://community.nxp.com/t5/Layerscape/Setting-up-multiple-VLANs-on-a-LX2160/m-p/1627063#M12143</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Yes it is possible, t&lt;SPAN&gt;he DPSW component provides VLAN filtering.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;take a look&amp;nbsp;in the DPAA2 user manual, DPSW_CREATE command takes a 16bit MAX_VLANS.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can also find examples of&amp;nbsp;Setting up Ethernet Switch Capability in the LSDK 21.08 USER GUIDE&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 03 Apr 2023 19:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Setting-up-multiple-VLANs-on-a-LX2160/m-p/1627063#M12143</guid>
      <dc:creator>Oswalag</dc:creator>
      <dc:date>2023-04-03T19:03:36Z</dc:date>
    </item>
  </channel>
</rss>