<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscapeのトピックflexbuilder ls1046afrwy build error</title>
    <link>https://community.nxp.com/t5/Layerscape/flexbuilder-ls1046afrwy-build-error/m-p/1616213#M12039</link>
    <description>&lt;P&gt;I am using flexbuilder that I downloaded from the "Get Started with the FRWY-LS1046A" page&amp;nbsp;2.4 Layerscape SDK for FRWY-LS1046A. I am running Ubuntu 18.04 (32bit) on Virtual Box Windows 10.&lt;/P&gt;&lt;P&gt;Entered following:&lt;/P&gt;&lt;P&gt;$ tar xvzf flexbuild_ls1046afrwy_bsp0.1.tgz&lt;BR /&gt;$ cd flexbuild&lt;BR /&gt;$ source setup.env&lt;BR /&gt;$ flex-builder -m ls1046afrwy -a arm64&lt;/P&gt;&lt;P&gt;The error I am getting is as follows:&lt;/P&gt;&lt;P&gt;Selecting previously unselected package iso-codes.&lt;BR /&gt;Preparing to unpack .../35-iso-codes_3.79-1_all.deb ...&lt;BR /&gt;Unpacking iso-codes (3.79-1) ...&lt;BR /&gt;Errors were encountered while processing:&lt;BR /&gt;/tmp/apt-dpkg-install-Uxij80/24-tzdata_2022g-0ubuntu0.18.04_all.deb&lt;BR /&gt;E: Sub-process /usr/bin/dpkg returned an error code (1)&lt;/P&gt;&lt;P&gt;When I look in /tmp the file is not there.&lt;/P&gt;&lt;P&gt;root@frwy1046a-VirtualBox:/tmp# ls&lt;BR /&gt;config-err-OLp4sk systemd-private-2ffa1dc8abe649f5be096dcbb3536e1d-ModemManager.service-k4Wh6k&lt;BR /&gt;config-err-plzppX systemd-private-2ffa1dc8abe649f5be096dcbb3536e1d-rtkit-daemon.service-1iw7Ca&lt;BR /&gt;snap-private-tmp systemd-private-2ffa1dc8abe649f5be096dcbb3536e1d-systemd-resolved.service-7FqkEC&lt;BR /&gt;ssh-xmSk2T2WyfS6&lt;/P&gt;&lt;P&gt;What do I need to do to correct this?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;William&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 15 Mar 2023 21:53:15 GMT</pubDate>
    <dc:creator>williawh</dc:creator>
    <dc:date>2023-03-15T21:53:15Z</dc:date>
    <item>
      <title>flexbuilder ls1046afrwy build error</title>
      <link>https://community.nxp.com/t5/Layerscape/flexbuilder-ls1046afrwy-build-error/m-p/1616213#M12039</link>
      <description>&lt;P&gt;I am using flexbuilder that I downloaded from the "Get Started with the FRWY-LS1046A" page&amp;nbsp;2.4 Layerscape SDK for FRWY-LS1046A. I am running Ubuntu 18.04 (32bit) on Virtual Box Windows 10.&lt;/P&gt;&lt;P&gt;Entered following:&lt;/P&gt;&lt;P&gt;$ tar xvzf flexbuild_ls1046afrwy_bsp0.1.tgz&lt;BR /&gt;$ cd flexbuild&lt;BR /&gt;$ source setup.env&lt;BR /&gt;$ flex-builder -m ls1046afrwy -a arm64&lt;/P&gt;&lt;P&gt;The error I am getting is as follows:&lt;/P&gt;&lt;P&gt;Selecting previously unselected package iso-codes.&lt;BR /&gt;Preparing to unpack .../35-iso-codes_3.79-1_all.deb ...&lt;BR /&gt;Unpacking iso-codes (3.79-1) ...&lt;BR /&gt;Errors were encountered while processing:&lt;BR /&gt;/tmp/apt-dpkg-install-Uxij80/24-tzdata_2022g-0ubuntu0.18.04_all.deb&lt;BR /&gt;E: Sub-process /usr/bin/dpkg returned an error code (1)&lt;/P&gt;&lt;P&gt;When I look in /tmp the file is not there.&lt;/P&gt;&lt;P&gt;root@frwy1046a-VirtualBox:/tmp# ls&lt;BR /&gt;config-err-OLp4sk systemd-private-2ffa1dc8abe649f5be096dcbb3536e1d-ModemManager.service-k4Wh6k&lt;BR /&gt;config-err-plzppX systemd-private-2ffa1dc8abe649f5be096dcbb3536e1d-rtkit-daemon.service-1iw7Ca&lt;BR /&gt;snap-private-tmp systemd-private-2ffa1dc8abe649f5be096dcbb3536e1d-systemd-resolved.service-7FqkEC&lt;BR /&gt;ssh-xmSk2T2WyfS6&lt;/P&gt;&lt;P&gt;What do I need to do to correct this?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;William&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 15 Mar 2023 21:53:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/flexbuilder-ls1046afrwy-build-error/m-p/1616213#M12039</guid>
      <dc:creator>williawh</dc:creator>
      <dc:date>2023-03-15T21:53:15Z</dc:date>
    </item>
    <item>
      <title>Re: flexbuilder ls1046afrwy build error</title>
      <link>https://community.nxp.com/t5/Layerscape/flexbuilder-ls1046afrwy-build-error/m-p/1616447#M12044</link>
      <description>&lt;P&gt;Processing triggers for systemd (237-3ubuntu10.57) ...&lt;BR /&gt;[sudo] password for frwy1046a:&lt;BR /&gt;&lt;FONT color="#FF0000"&gt;/home/frwy1046a/Downloads/flexbuild/build/rfs/rootfs_ubuntu_bionic_LS_arm64 [Done]&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF0000"&gt;Got it built finally!&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;My Virtual Box Unbuntu 18.04 32bit system was corrupted. I built a new Virtual Box Unbuntu 18.04 64bit system with unattended installation:&amp;nbsp;&lt;A href="https://ubuntu.com/tutorials/how-to-run-ubuntu-desktop-on-a-virtual-machine-using-virtualbox#1-overview" target="_blank"&gt;https://ubuntu.com/tutorials/how-to-run-ubuntu-desktop-on-a-virtual-machine-using-virtualbox#1-overview&lt;/A&gt;&lt;BR /&gt;I ran into a problem with rsyslog but this was solved by the solution in "ls1043a flexbuild_lsdk1806 build error" post with modifications since I am building ls1046a I guess.&lt;/P&gt;&lt;P&gt;vi flexbuild/tools/flex-mkdistrorfs&lt;/P&gt;&lt;P&gt;install_cfg_secondstage() {&lt;BR /&gt;.&lt;BR /&gt;.&lt;BR /&gt;.&lt;BR /&gt;apt -y install language-pack-en-base&lt;BR /&gt;fi&lt;BR /&gt;fi&lt;/P&gt;&lt;P&gt;test -f /proc/uptime || mount -t proc proc /proc&lt;/P&gt;&lt;P&gt;test -f /dev/pts/ptmx || mount -t devpts devpts /dev/pts&lt;/P&gt;&lt;P&gt;apt -y upgrade&lt;BR /&gt;.&lt;BR /&gt;.&lt;BR /&gt;.&lt;BR /&gt;}&lt;/P&gt;</description>
      <pubDate>Thu, 16 Mar 2023 06:21:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/flexbuilder-ls1046afrwy-build-error/m-p/1616447#M12044</guid>
      <dc:creator>williawh</dc:creator>
      <dc:date>2023-03-16T06:21:26Z</dc:date>
    </item>
  </channel>
</rss>