<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can LS1046 update the program without uboot? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Can-LS1046-update-the-program-without-uboot/m-p/1605345#M11928</link>
    <description>&lt;P&gt;Thank you for contacting NXP support!&lt;/P&gt;
&lt;P&gt;With the CodeWarrior TAP, you have to boot the board from RAM and then you can use the flash programmer tool in CodeWarrior.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/search?keyword=AN12081&amp;amp;start=0&amp;amp;_gl=1*jf9s68*_ga*ODk2ODQzMzUuMTY3NzI1MjM1OA..*_ga_WM5LE0KMSH*MTY3NzI1MjM1OC4xLjEuMTY3NzI1MjQ2My4wLjAuMA.." target="_blank"&gt;Search | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 24 Feb 2023 15:28:18 GMT</pubDate>
    <dc:creator>Chavira</dc:creator>
    <dc:date>2023-02-24T15:28:18Z</dc:date>
    <item>
      <title>Can LS1046 update the program without uboot?</title>
      <link>https://community.nxp.com/t5/Layerscape/Can-LS1046-update-the-program-without-uboot/m-p/1605187#M11923</link>
      <description>&lt;P&gt;I noticed that LS1046 supports two startup modes:TF CARD/ QSPI FLASH.&lt;/P&gt;&lt;P&gt;Can LS1046 update the program without uboot?&amp;nbsp;&lt;/P&gt;&lt;P&gt;For example, The QSPI Flash is erased. Is there any other way to program firmware image without using the TF card boot mode.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Fri, 24 Feb 2023 10:37:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Can-LS1046-update-the-program-without-uboot/m-p/1605187#M11923</guid>
      <dc:creator>Hmc510</dc:creator>
      <dc:date>2023-02-24T10:37:51Z</dc:date>
    </item>
    <item>
      <title>Re: Can LS1046 update the program without uboot?</title>
      <link>https://community.nxp.com/t5/Layerscape/Can-LS1046-update-the-program-without-uboot/m-p/1605345#M11928</link>
      <description>&lt;P&gt;Thank you for contacting NXP support!&lt;/P&gt;
&lt;P&gt;With the CodeWarrior TAP, you have to boot the board from RAM and then you can use the flash programmer tool in CodeWarrior.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/search?keyword=AN12081&amp;amp;start=0&amp;amp;_gl=1*jf9s68*_ga*ODk2ODQzMzUuMTY3NzI1MjM1OA..*_ga_WM5LE0KMSH*MTY3NzI1MjM1OC4xLjEuMTY3NzI1MjQ2My4wLjAuMA.." target="_blank"&gt;Search | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Feb 2023 15:28:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Can-LS1046-update-the-program-without-uboot/m-p/1605345#M11928</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2023-02-24T15:28:18Z</dc:date>
    </item>
    <item>
      <title>Re: Can LS1046 update the program without uboot?</title>
      <link>https://community.nxp.com/t5/Layerscape/Can-LS1046-update-the-program-without-uboot/m-p/1606416#M11946</link>
      <description>&lt;P&gt;You can try &lt;A href="https://u-boot.readthedocs.io/en/latest/board/nxp/ls1046ardb.html#jtag-boot" target="_blank"&gt;https://u-boot.readthedocs.io/en/latest/board/nxp/ls1046ardb.html#jtag-boot&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 27 Feb 2023 23:39:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Can-LS1046-update-the-program-without-uboot/m-p/1606416#M11946</guid>
      <dc:creator>stadium_aquino</dc:creator>
      <dc:date>2023-02-27T23:39:13Z</dc:date>
    </item>
  </channel>
</rss>