<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1021A-IOT QSPI boot</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601400#M11880</link>
    <description>&lt;P&gt;I tried to replace&amp;nbsp;&lt;SPAN&gt;u-boot-ls1021aiot.bin with one generated bonus my own.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I downloaded u-boot sources, used ls1021aiot_qspi_defconfig and then generated u-boot binary.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After this, I byteswapped the u-boot bin using your tcl byteswap script and flashed the so generated u-boot-byteswapped.bin in 0x10000 instead of&amp;nbsp;&lt;SPAN&gt;u-boot-ls1021aiot.bin. In u-boot TEXT_BASE is correctly set as 0x40010000.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Unfortunately this not works. I see nothing at console log. Reset led goes off so I suppose RCW load went good with reset cycle completed.&lt;/P&gt;&lt;P&gt;What could it be the problem? I used the most recent uboot version (2023.4-rc3) so could it be a compatibility issue?&lt;/P&gt;</description>
    <pubDate>Sat, 18 Feb 2023 07:47:49 GMT</pubDate>
    <dc:creator>Kensou</dc:creator>
    <dc:date>2023-02-18T07:47:49Z</dc:date>
    <item>
      <title>LS1021A-IOT QSPI boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601075#M11871</link>
      <description>&lt;P&gt;hello everybody,&lt;BR /&gt;I need urgently a way for generating LS1021A-IOT QSPI boot image.&lt;BR /&gt;&lt;BR /&gt;OpenIL, OpenWRT en Real-Time-Egde are only able to generate SD Card images.&lt;/P&gt;&lt;P&gt;LS1021A-IOT SDK 0.4 seems to be not available anywhere.&lt;BR /&gt;&lt;BR /&gt;I need urgently an SDK or similar for generating LS1021A-IOT QSPI, could anybody help me about?&lt;BR /&gt;&lt;BR /&gt;Thank you in advance.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 11:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601075#M11871</guid>
      <dc:creator>Kensou</dc:creator>
      <dc:date>2023-02-17T11:10:00Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A-IOT QSPI boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601107#M11872</link>
      <description>&lt;P&gt;Thank you for contacting NXP support!&lt;/P&gt;
&lt;P&gt;Note:I can't publish the files on the comunnity please open a case on&amp;nbsp;&lt;A href="https://www.nxp.com/support/support:SUPPORTHOME" target="_blank"&gt;Support | NXP Semiconductors&lt;/A&gt; to share the files with you.&lt;/P&gt;
&lt;P&gt;1. Files&lt;BR /&gt;u-boot-ls1021aiot.bin&lt;BR /&gt;rcw/ls1021aiot/RSR_PPS_70/rcw_1000_qspiboot_swap.bin&lt;/P&gt;
&lt;P&gt;2. Map&lt;BR /&gt;rcw: 0x0 - 0x100&lt;BR /&gt;u-boot: 0x10000 - 0x90000&lt;BR /&gt;u-boot env: 0x100000 - 0x120000&lt;/P&gt;
&lt;P&gt;3. Dip switch settings&lt;BR /&gt;For QSPI boot, SW2.1 = ON&lt;/P&gt;
&lt;P&gt;3.1 rcw/ls1021aiot/RSR_PPS_70/rcw_1000_qspiboot_swap.bin&lt;BR /&gt;Dip Switch: SW2.5 = OFF&lt;BR /&gt;Brief: ETH0 disabled&lt;BR /&gt;SATA enabled&lt;/P&gt;
&lt;P&gt;4. Assume qspi is empty, boot from SD card first, the run the following&lt;BR /&gt;commands to flash the images to QSPI.&lt;/P&gt;
&lt;P&gt;4.1 rcw/ls1021aiot/RSR_PPS_70/rcw_1000_qspiboot_swap.bin and u-boot&lt;BR /&gt;=&amp;gt; sf probe&lt;BR /&gt;=&amp;gt; sf erase 0x0 0x100000&lt;BR /&gt;=&amp;gt; tftp 0x82000000 rcw/ls1021aiot/RSR_PPS_70/rcw_1000_qspiboot_swap.bin&lt;BR /&gt;=&amp;gt; sf write 0x82000000 0x0 0x100&lt;BR /&gt;=&amp;gt; tftp 0x82000000 u-boot-ls1021aiot.bin&lt;BR /&gt;=&amp;gt; sf write 0x82000000 0x10000 0x80000&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 12:25:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601107#M11872</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2023-02-17T12:25:21Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A-IOT QSPI boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601145#M11873</link>
      <description>&lt;P&gt;How to generate rcw_1000_qspiboot_swap.bin and u-boot-ls1021aiot.bin? I need a procedure or a SDK.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 13:28:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601145#M11873</guid>
      <dc:creator>Kensou</dc:creator>
      <dc:date>2023-02-17T13:28:30Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A-IOT QSPI boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601207#M11874</link>
      <description>&lt;P&gt;Sorry, we do not have the components of that software because that board was made for an NXP partner, that information only can be provided by your distributor on a USB inside the package on the board, please contact your distributor.&lt;/P&gt;&lt;P&gt;We only have the first image for that board and we don't have the latest for that board.&lt;/P&gt;</description>
      <pubDate>Fri, 17 Feb 2023 15:10:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601207#M11874</guid>
      <dc:creator>Chavira</dc:creator>
      <dc:date>2023-02-17T15:10:44Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A-IOT QSPI boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601399#M11879</link>
      <description>&lt;P&gt;I tried to compile by myself ls1021aiot u-boot, by downloading u-boot sources, using ls1021aiot_qspi_defconfig, byteswapped u-boot.bin as per your tcl script, and then using the so generated u-boot-swapped.bin binary instead of your one.&lt;/P&gt;&lt;P&gt;TEXT_BASE is regularly set at 0x40010000&lt;/P&gt;&lt;P&gt;This seems not to work, I do not see anything at console log. Reset led is off so rcw was correctly loaded. I used the latest u-boot, 2023.4 version. Could it be a compatibility issue?&lt;/P&gt;</description>
      <pubDate>Sat, 18 Feb 2023 07:27:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601399#M11879</guid>
      <dc:creator>Kensou</dc:creator>
      <dc:date>2023-02-18T07:27:22Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A-IOT QSPI boot</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601400#M11880</link>
      <description>&lt;P&gt;I tried to replace&amp;nbsp;&lt;SPAN&gt;u-boot-ls1021aiot.bin with one generated bonus my own.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I downloaded u-boot sources, used ls1021aiot_qspi_defconfig and then generated u-boot binary.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After this, I byteswapped the u-boot bin using your tcl byteswap script and flashed the so generated u-boot-byteswapped.bin in 0x10000 instead of&amp;nbsp;&lt;SPAN&gt;u-boot-ls1021aiot.bin. In u-boot TEXT_BASE is correctly set as 0x40010000.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Unfortunately this not works. I see nothing at console log. Reset led goes off so I suppose RCW load went good with reset cycle completed.&lt;/P&gt;&lt;P&gt;What could it be the problem? I used the most recent uboot version (2023.4-rc3) so could it be a compatibility issue?&lt;/P&gt;</description>
      <pubDate>Sat, 18 Feb 2023 07:47:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-IOT-QSPI-boot/m-p/1601400#M11880</guid>
      <dc:creator>Kensou</dc:creator>
      <dc:date>2023-02-18T07:47:49Z</dc:date>
    </item>
  </channel>
</rss>