<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックM.2 SSD in LS1046 custom board</title>
    <link>https://community.nxp.com/t5/Layerscape/M-2-SSD-in-LS1046-custom-board/m-p/1598436#M11850</link>
    <description>&lt;P&gt;I am designing a hardware using LS1046. In our design, we are planning to use M.2 SSD PCIe3.0x4 instead of eMMC or SDcard. We are planning to connect M.2 SSD using USB -PCIe bridge. My questions are:&lt;/P&gt;&lt;P&gt;1) Can I use M.2 SSD&amp;nbsp;instead of eMMC or SDcard and will the processor support the same?&lt;/P&gt;&lt;P&gt;2) Is it compatible for the processor to use the&amp;nbsp;USB -PCIe bridge?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanking you in advance&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 13 Feb 2023 23:53:12 GMT</pubDate>
    <dc:creator>Ellu24</dc:creator>
    <dc:date>2023-02-13T23:53:12Z</dc:date>
    <item>
      <title>M.2 SSD in LS1046 custom board</title>
      <link>https://community.nxp.com/t5/Layerscape/M-2-SSD-in-LS1046-custom-board/m-p/1598436#M11850</link>
      <description>&lt;P&gt;I am designing a hardware using LS1046. In our design, we are planning to use M.2 SSD PCIe3.0x4 instead of eMMC or SDcard. We are planning to connect M.2 SSD using USB -PCIe bridge. My questions are:&lt;/P&gt;&lt;P&gt;1) Can I use M.2 SSD&amp;nbsp;instead of eMMC or SDcard and will the processor support the same?&lt;/P&gt;&lt;P&gt;2) Is it compatible for the processor to use the&amp;nbsp;USB -PCIe bridge?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanking you in advance&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Feb 2023 23:53:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/M-2-SSD-in-LS1046-custom-board/m-p/1598436#M11850</guid>
      <dc:creator>Ellu24</dc:creator>
      <dc:date>2023-02-13T23:53:12Z</dc:date>
    </item>
    <item>
      <title>Re: M.2 SSD in LS1046 custom board</title>
      <link>https://community.nxp.com/t5/Layerscape/M-2-SSD-in-LS1046-custom-board/m-p/1601622#M11881</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/199214"&gt;@Ellu24&lt;/a&gt;,&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;LS1046A can boot from SD/eMMC. It cannot boot from SSD. So if you use SSD, you need to use some other boot source.&lt;/P&gt;
&lt;P&gt;You are planning to use USB-PCIe bridge. I'm not sure why you do not plan to connect M.2 SSD directly to PCIe controller of LS1046A. This will give you very high throughput.&lt;/P&gt;
&lt;P&gt;The USB controller of LS1046A complies with USB specification rev 3.0. You can plug-in anything that complies to the specification.&lt;BR /&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Mrudang&lt;/P&gt;</description>
      <pubDate>Mon, 20 Feb 2023 03:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/M-2-SSD-in-LS1046-custom-board/m-p/1601622#M11881</guid>
      <dc:creator>mrudangshelat-13</dc:creator>
      <dc:date>2023-02-20T03:42:26Z</dc:date>
    </item>
    <item>
      <title>Re: M.2 SSD in LS1046 custom board</title>
      <link>https://community.nxp.com/t5/Layerscape/M-2-SSD-in-LS1046-custom-board/m-p/1603236#M11896</link>
      <description>&lt;P&gt;Thank you very much for your reply.&lt;/P&gt;</description>
      <pubDate>Tue, 21 Feb 2023 23:01:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/M-2-SSD-in-LS1046-custom-board/m-p/1603236#M11896</guid>
      <dc:creator>Ellu24</dc:creator>
      <dc:date>2023-02-21T23:01:59Z</dc:date>
    </item>
  </channel>
</rss>