<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックThe 1043 kernel sets the external interrupt IRQ 0 high-level problem</title>
    <link>https://community.nxp.com/t5/Layerscape/The-1043-kernel-sets-the-external-interrupt-IRQ-0-high-level/m-p/1594393#M11805</link>
    <description>&lt;P&gt;The 1043 kernel sets the external interrupt IRQ 0 high-level trigger interrupt mode. After registering the interrupt service routine. When the high level comes,if IRQ0 is not pulled down, tens of millions of interrupts will be generated within a few seconds, and the system will kernel panic after a while. Even if I pull down IRQ0 as soon as I enter the interrupt service routine,.there will be interrupts&amp;nbsp; but the problem of not entering the interrupt service routine from time to time.&lt;/P&gt;</description>
    <pubDate>Tue, 07 Feb 2023 05:53:11 GMT</pubDate>
    <dc:creator>ppbobo</dc:creator>
    <dc:date>2023-02-07T05:53:11Z</dc:date>
    <item>
      <title>The 1043 kernel sets the external interrupt IRQ 0 high-level problem</title>
      <link>https://community.nxp.com/t5/Layerscape/The-1043-kernel-sets-the-external-interrupt-IRQ-0-high-level/m-p/1594393#M11805</link>
      <description>&lt;P&gt;The 1043 kernel sets the external interrupt IRQ 0 high-level trigger interrupt mode. After registering the interrupt service routine. When the high level comes,if IRQ0 is not pulled down, tens of millions of interrupts will be generated within a few seconds, and the system will kernel panic after a while. Even if I pull down IRQ0 as soon as I enter the interrupt service routine,.there will be interrupts&amp;nbsp; but the problem of not entering the interrupt service routine from time to time.&lt;/P&gt;</description>
      <pubDate>Tue, 07 Feb 2023 05:53:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/The-1043-kernel-sets-the-external-interrupt-IRQ-0-high-level/m-p/1594393#M11805</guid>
      <dc:creator>ppbobo</dc:creator>
      <dc:date>2023-02-07T05:53:11Z</dc:date>
    </item>
    <item>
      <title>Re: The 1043 kernel sets the external interrupt IRQ 0 high-level problem</title>
      <link>https://community.nxp.com/t5/Layerscape/The-1043-kernel-sets-the-external-interrupt-IRQ-0-high-level/m-p/1598585#M11852</link>
      <description>&lt;P&gt;&lt;SPAN&gt;You can find a external IRQ reference code from LX2160ARDB. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;External IRQ3 is used for AQR107 PHY, high-level trigger mode. &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Following is the dts setting:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; aquantia_phy1: ethernet-phy@4 {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; /* AQR107 PHY */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; compatible = "ethernet-phy-ieee802.3-c45";&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; interrupts = &amp;lt;GIC_SPI 2 IRQ_TYPE_LEVEL_HIGH&amp;gt;;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; reg = &amp;lt;0x4&amp;gt;;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; };&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 14 Feb 2023 05:59:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/The-1043-kernel-sets-the-external-interrupt-IRQ-0-high-level/m-p/1598585#M11852</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-02-14T05:59:32Z</dc:date>
    </item>
  </channel>
</rss>