<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Programming LS1046ARDB Ethernet with 32bit RTOS in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Programming-LS1046ARDB-Ethernet-with-32bit-RTOS/m-p/1588336#M11764</link>
    <description>&lt;P&gt;I'm trying to program Ethernet port (independent mode) for an RTOS. The RTOS I use is 32-bit. U-boot is used to load the RTOS.&lt;/P&gt;&lt;P&gt;For Ethernet program, I understand that I need to load FMAN microcode.&amp;nbsp; I guess, FMAN microcode can work with 32-bit access. But, when I check the&amp;nbsp;LS1046A Reference manual, it says QMAN S/W Portal (05_0000_0000) is not supported for 32-bit access. Does FMAN microcode uses this QMAN S/W portal? Does this mean microcode/Ethernet port cannot be programmed with 32-bit RTOS?&lt;/P&gt;&lt;P&gt;Thanks in advance for any tips/information.&lt;/P&gt;</description>
    <pubDate>Thu, 26 Jan 2023 14:26:08 GMT</pubDate>
    <dc:creator>srak</dc:creator>
    <dc:date>2023-01-26T14:26:08Z</dc:date>
    <item>
      <title>Programming LS1046ARDB Ethernet with 32bit RTOS</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-LS1046ARDB-Ethernet-with-32bit-RTOS/m-p/1588336#M11764</link>
      <description>&lt;P&gt;I'm trying to program Ethernet port (independent mode) for an RTOS. The RTOS I use is 32-bit. U-boot is used to load the RTOS.&lt;/P&gt;&lt;P&gt;For Ethernet program, I understand that I need to load FMAN microcode.&amp;nbsp; I guess, FMAN microcode can work with 32-bit access. But, when I check the&amp;nbsp;LS1046A Reference manual, it says QMAN S/W Portal (05_0000_0000) is not supported for 32-bit access. Does FMAN microcode uses this QMAN S/W portal? Does this mean microcode/Ethernet port cannot be programmed with 32-bit RTOS?&lt;/P&gt;&lt;P&gt;Thanks in advance for any tips/information.&lt;/P&gt;</description>
      <pubDate>Thu, 26 Jan 2023 14:26:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-LS1046ARDB-Ethernet-with-32bit-RTOS/m-p/1588336#M11764</guid>
      <dc:creator>srak</dc:creator>
      <dc:date>2023-01-26T14:26:08Z</dc:date>
    </item>
    <item>
      <title>Re: Programming LS1046ARDB Ethernet with 32bit RTOS</title>
      <link>https://community.nxp.com/t5/Layerscape/Programming-LS1046ARDB-Ethernet-with-32bit-RTOS/m-p/1594388#M11804</link>
      <description>&lt;P&gt;&lt;SPAN&gt;FMan ucode and QMAN is independent to ARM operating system.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 07 Feb 2023 05:38:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Programming-LS1046ARDB-Ethernet-with-32bit-RTOS/m-p/1594388#M11804</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-02-07T05:38:11Z</dc:date>
    </item>
  </channel>
</rss>