<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: U-boot commands not working when running NOR and eMMC in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/U-boot-commands-not-working-when-running-NOR-and-eMMC/m-p/1586780#M11744</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Is this behavior happening with the provided NXP BSP? Or is this also a custom build?&lt;/P&gt;
&lt;P&gt;Have you followed the Linux User Guide for this build? Have you verified that the DDR PHY is under the required specifications?&lt;/P&gt;
&lt;P&gt;If we understand correctly, this is happening only in NOR and eMMC, running from SD is not causing this behavior?&lt;/P&gt;
&lt;P&gt;We have a platform booting from NOR Flash which can accept commands in u-boot.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
    <pubDate>Mon, 23 Jan 2023 19:01:06 GMT</pubDate>
    <dc:creator>Daniel-Aguirre</dc:creator>
    <dc:date>2023-01-23T19:01:06Z</dc:date>
    <item>
      <title>U-boot commands not working when running NOR and eMMC</title>
      <link>https://community.nxp.com/t5/Layerscape/U-boot-commands-not-working-when-running-NOR-and-eMMC/m-p/1585953#M11735</link>
      <description>&lt;P&gt;Hi Team,&lt;/P&gt;&lt;P&gt;I am working on a custom board based on RDB3, where we are using different DDR from Micron.&lt;/P&gt;&lt;P&gt;Generated code, with DDR&amp;nbsp; DQ swapping changes and include in BSP33 and BSP34 for our custom board.&lt;/P&gt;&lt;P&gt;In both case u-boot is running and stopping at command prompt it taking input, but not able to execute any command including "help".&lt;/P&gt;&lt;P&gt;Log:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;CPU:&amp;nbsp;&amp;nbsp; NXP S32G399A rev. 1.1&lt;/P&gt;&lt;P&gt;Model: NXP S32G399A-RDB3&lt;/P&gt;&lt;P&gt;DRAM:&amp;nbsp; 3.5 GiB&lt;/P&gt;&lt;P&gt;MMC:&amp;nbsp;&amp;nbsp; FSL_SDHC: 0&lt;/P&gt;&lt;P&gt;Loading Environment from MMC... OK&lt;/P&gt;&lt;P&gt;In:&amp;nbsp;&amp;nbsp;&amp;nbsp; serial@401c8000&lt;/P&gt;&lt;P&gt;Out:&amp;nbsp;&amp;nbsp; serial@401c8000&lt;/P&gt;&lt;P&gt;Err:&amp;nbsp;&amp;nbsp; serial@401c8000&lt;/P&gt;&lt;P&gt;##board specific logs##&lt;/P&gt;&lt;P&gt;Board revision: RDB&lt;/P&gt;&lt;P&gt;Net:&amp;nbsp;&amp;nbsp; Emac 0 not initialized&lt;/P&gt;&lt;P&gt;Invalid sgmii configuration for emac index 0&lt;/P&gt;&lt;P&gt;No ethernet found.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:&amp;nbsp; 0&lt;/P&gt;&lt;P&gt;=&amp;gt;&lt;/P&gt;&lt;P&gt;Unknown command '' - try 'help'&lt;/P&gt;&lt;P&gt;=&amp;gt; printenv&lt;/P&gt;&lt;P&gt;Unknown command 'printenv' - try 'help'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;from cli "commands" not working. working when executed from source code.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;#s32g3 #u-boot&lt;/P&gt;</description>
      <pubDate>Fri, 20 Jan 2023 13:24:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/U-boot-commands-not-working-when-running-NOR-and-eMMC/m-p/1585953#M11735</guid>
      <dc:creator>yellapu_anishkh</dc:creator>
      <dc:date>2023-01-20T13:24:26Z</dc:date>
    </item>
    <item>
      <title>Re: U-boot commands not working when running NOR and eMMC</title>
      <link>https://community.nxp.com/t5/Layerscape/U-boot-commands-not-working-when-running-NOR-and-eMMC/m-p/1586780#M11744</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Is this behavior happening with the provided NXP BSP? Or is this also a custom build?&lt;/P&gt;
&lt;P&gt;Have you followed the Linux User Guide for this build? Have you verified that the DDR PHY is under the required specifications?&lt;/P&gt;
&lt;P&gt;If we understand correctly, this is happening only in NOR and eMMC, running from SD is not causing this behavior?&lt;/P&gt;
&lt;P&gt;We have a platform booting from NOR Flash which can accept commands in u-boot.&lt;/P&gt;
&lt;P&gt;Please, let us know.&lt;/P&gt;</description>
      <pubDate>Mon, 23 Jan 2023 19:01:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/U-boot-commands-not-working-when-running-NOR-and-eMMC/m-p/1586780#M11744</guid>
      <dc:creator>Daniel-Aguirre</dc:creator>
      <dc:date>2023-01-23T19:01:06Z</dc:date>
    </item>
    <item>
      <title>Re: U-boot commands not working when running NOR and eMMC</title>
      <link>https://community.nxp.com/t5/Layerscape/U-boot-commands-not-working-when-running-NOR-and-eMMC/m-p/1587281#M11751</link>
      <description>&lt;P&gt;Make sure your terminal emulator or serial adapter is not inserting extra characters. Try modifying cmd_process in common/command.c to dump the hex code of what U-Boot thinks is the command. It's likely that a non-printable character has snuck in somewhere.&lt;/P&gt;</description>
      <pubDate>Tue, 24 Jan 2023 17:55:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/U-boot-commands-not-working-when-running-NOR-and-eMMC/m-p/1587281#M11751</guid>
      <dc:creator>stadium_aquino</dc:creator>
      <dc:date>2023-01-24T17:55:50Z</dc:date>
    </item>
    <item>
      <title>Re: U-boot commands not working when running NOR and eMMC</title>
      <link>https://community.nxp.com/t5/Layerscape/U-boot-commands-not-working-when-running-NOR-and-eMMC/m-p/1590675#M11773</link>
      <description>&lt;P&gt;Issue is resolved after upgrading the UART to USB chip driver, used for console.&lt;/P&gt;</description>
      <pubDate>Tue, 31 Jan 2023 15:26:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/U-boot-commands-not-working-when-running-NOR-and-eMMC/m-p/1590675#M11773</guid>
      <dc:creator>yellapu_anishkh</dc:creator>
      <dc:date>2023-01-31T15:26:05Z</dc:date>
    </item>
  </channel>
</rss>