<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 Re: LS1021A PCIe driver crashes</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021A-PCIe-driver-crashes/m-p/1575335#M11553</link>
    <description>&lt;P&gt;&lt;SPAN&gt;For the error case, are you using linux kernel from LSDK? Seems this linux kernel is not released by NXP:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.251637] layerscape-pcie 3400000.pcie: host bridge /soc/pcie@3400000 ranges:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.339741] layerscape-pcie 3400000.pcie: IO 0x4000010000..0x400001ffff -&amp;gt; 0x00000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.437213] layerscape-pcie 3400000.pcie: MEM 0x4040000000..0x407fffffff -&amp;gt; 0x40000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.534689] Unable to handle kernel NULL pointer dereference at virtual address 00000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.632140] pgd = (ptrval)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.664637] [00000000] *pgd=00000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.707615] Internal error: Oops: 5 [#1] SMP ARM&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In your log, seems non-prefetchable memory resource not configured. In NXP released linux, it should print 36-bits address, this code is from our linux kernel:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; dev_dbg(dev, "Parsing ranges property...\n");&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; for_each_of_pci_range(&amp;amp;parser, &amp;amp;range) {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; /* Read next ranges element */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; if ((range.flags &amp;amp; IORESOURCE_TYPE_BITS) == IORESOURCE_IO)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; range_type = "IO";&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; else if ((range.flags &amp;amp; IORESOURCE_TYPE_BITS) == IORESOURCE_MEM)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; range_type = "MEM";&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; else&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; range_type = "err";&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; dev_info(dev, " %6s %#012llx..%#012llx -&amp;gt; %#012llx\n",&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; range_type, range.cpu_addr,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; range.cpu_addr + range.size - 1, range.pci_addr);&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Dec 2022 01:31:18 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-12-29T01:31:18Z</dc:date>
    <item>
      <title>LS1021A PCIe driver crashes</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-PCIe-driver-crashes/m-p/1565349#M11480</link>
      <description>&lt;P&gt;We have a LS1021A based design. I am doing the board bring-up. We have our own boot laoder but also can run U-boot. When booting our Linux 5.17 kernel the system boots to the prompt but fails to get the correct vendor/device ID for a device connected to LANE 0. Though on the Ls1021A side everything seems good:&lt;/P&gt;&lt;P&gt;0.174370] layerscape-pcie 3400000.pcie: host bridge /soc/pcie@3400000 ranges:&lt;BR /&gt;[ 0.174444] layerscape-pcie 3400000.pcie: IO 0x4000010000..0x400001ffff -&amp;gt; 0x0000000000&lt;BR /&gt;[ 0.174483] layerscape-pcie 3400000.pcie: MEM 0x4040000000..0x407fffffff -&amp;gt; 0x0040000000&lt;BR /&gt;[ 0.174520] layerscape-pcie 3400000.pcie: non-prefetchable memory resource required&lt;BR /&gt;[ 0.174554] layerscape-pcie 3400000.pcie: iATU unroll: disabled&lt;BR /&gt;[ 0.174567] layerscape-pcie 3400000.pcie: Detected iATU regions: 6 outbound, 6 inbound&lt;BR /&gt;[ 0.174597] layerscape-pcie 3400000.pcie: Link up&lt;BR /&gt;[ 0.174722] layerscape-pcie 3400000.pcie: PCI host bridge to bus 0000:00&lt;BR /&gt;[ 0.174742] pci_bus 0000:00: root bus resource [bus 00-ff]&lt;BR /&gt;[ 0.174761] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]&lt;BR /&gt;[ 0.174809] pci 0000:00:00.0: [1957:0e09] type 01 class 0x060400 ==&amp;gt; NXP OK&lt;BR /&gt;[ 0.174840] pci 0000:00:00.0: reg 0x10: [mem 0x00000000-0x00ffffff]&lt;BR /&gt;[ 0.174861] pci 0000:00:00.0: reg 0x14: [mem 0x00000000-0x03ffffff]&lt;BR /&gt;[ 0.174880] pci 0000:00:00.0: reg 0x38: [mem 0x00000000-0x00ffffff pref]&lt;BR /&gt;[ 0.174941] pci 0000:00:00.0: supports D1 D2&lt;BR /&gt;[ 0.174954] pci 0000:00:00.0: PME# supported from D0 D1 D2 D3hot&lt;BR /&gt;[ 0.176805] PCI: bus0: Fast back to back transfers disabled&lt;BR /&gt;[ 0.176942] pci 0000:01:00.0: [f018:e59f] type 1f class 0xe59ff0&amp;nbsp; ==&amp;gt; DEVICE NOT OK&lt;BR /&gt;[ 0.176975] pci 0000:01:00.0: unknown header type 1f, ignoring device&lt;BR /&gt;[ 0.178508] PCI: bus1: Fast back to back transfers enabled&lt;BR /&gt;[ 0.178547] pci 0000:00:00.0: BAR 1: no space for [mem size 0x04000000]&lt;BR /&gt;[ 0.178566] pci 0000:00:00.0: BAR 1: failed to assign [mem size 0x04000000]&lt;BR /&gt;[ 0.178582] pci 0000:00:00.0: BAR 0: no space for [mem size 0x01000000]&lt;BR /&gt;[ 0.178597] pci 0000:00:00.0: BAR 0: failed to assign [mem size 0x01000000]&lt;BR /&gt;[ 0.178612] pci 0000:00:00.0: BAR 6: no space for [mem size 0x01000000 pref]&lt;BR /&gt;[ 0.178627] pci 0000:00:00.0: BAR 6: failed to assign [mem size 0x01000000 pref]&lt;BR /&gt;[ 0.178645] pci 0000:00:00.0: PCI bridge to [bus 01-ff]&lt;/P&gt;&lt;P&gt;When booting U-boot, I can see the correct ID:&lt;/P&gt;&lt;P&gt;=&amp;gt; pci heade 1.0.0&lt;BR /&gt;PCIe1: pcie@3400000 Root Complex: x1 gen1&lt;BR /&gt;vendor ID = 0x14e4&lt;BR /&gt;device ID = 0xb861&lt;/P&gt;&lt;P&gt;However, booting the NXP kernel 5.10:&lt;/P&gt;&lt;P&gt;[ 5.251637] layerscape-pcie 3400000.pcie: host bridge /soc/pcie@3400000 ranges:&lt;BR /&gt;[ 5.339741] layerscape-pcie 3400000.pcie: IO 0x4000010000..0x400001ffff -&amp;gt; 0x00000000&lt;BR /&gt;[ 5.437213] layerscape-pcie 3400000.pcie: MEM 0x4040000000..0x407fffffff -&amp;gt; 0x40000000&lt;BR /&gt;[ 5.534689] Unable to handle kernel NULL pointer dereference at virtual address 00000000&lt;BR /&gt;[ 5.632140] pgd = (ptrval)&lt;BR /&gt;[ 5.664637] [00000000] *pgd=00000000&lt;BR /&gt;[ 5.707615] Internal error: Oops: 5 [#1] SMP ARM&lt;BR /&gt;[ 5.763147] Modules linked in:&lt;BR /&gt;[ 5.799823] CPU: 0 PID: 1 Comm: swapper/0 Not tainted 4.19.68-00019-ga5c3ba83fc17-dirty #6&lt;BR /&gt;[ 5.899349] Hardware name: Freescale LS1021A&lt;BR /&gt;[ 5.950699] PC is at dw_pcie_host_init+0x20c/0x540&lt;BR /&gt;[ 6.008322] LR is at devm_pci_remap_iospace+0x58/0x78&lt;BR /&gt;[ 6.069083] pc : [&amp;lt;c04999c4&amp;gt;] lr : [&amp;lt;c047a12c&amp;gt;] psr: a0000053&lt;BR /&gt;[ 6.144514] sp : d708bde8 ip : 00000000 fp : d7fd710c&lt;BR /&gt;[ 6.207376] r10: d7216fb0 r9 : d710d010 r8 : d7216e00&lt;BR /&gt;[ 6.270238] r7 : d7216fb0 r6 : d7216fb0 r5 : 00000100 r4 : d7216c58&lt;BR /&gt;[ 6.348811] r3 : 00000000 r2 : 00000000 r1 : 00000000 r0 : 00000000&lt;BR /&gt;[ 6.427388] Flags: NzCv IRQs on FIQs off Mode SVC_32 ISA ARM Segment none&lt;BR /&gt;[ 6.514341] Control: 10c5387d Table: 8400406a DAC: 00000051&lt;BR /&gt;[ 6.583488] Process swapper/0 (pid: 1, stack limit = 0x(ptrval))&lt;BR /&gt;[ 6.655777] Stack: (0xd708bde8 to 0xd708c000)&lt;BR /&gt;[ 6.708167] bde0: d7216c80 dc910000 d710d010 c0c8d5d8 c0cab170 c0cc0cf8&lt;BR /&gt;[ 6.806652] be00: 00010000 d7270040 d710d010 d710d000 d710d010 00000000 c0f4f564 00000000&lt;BR /&gt;[ 6.905137] be20: c0e0049c c0e31524 00000000 d710d010 c0f4f564 c0fe9bbc 00000000 c05410b0&lt;BR /&gt;[ 7.003621] be40: d710d010 c0fe9bb8 00000000 c053f38c 00000000 d710d010 c0f4f564 d710d044&lt;BR /&gt;[ 7.102107] be60: c0f68e78 c0fac380 c0ea1aec c0e87854 c0e0049c c053f648 c053f750 c0f68e78&lt;BR /&gt;[ 7.200591] be80: d710d010 c0f4f564 d710d044 c0f68e78 c0fac380 c053f864 00000000 c0f4f564&lt;BR /&gt;[ 7.299076] bea0: c053f750 c053d20c d70e9058 d7100834 c0f4f564 d7265f80 00000000 c053e5f0&lt;BR /&gt;[ 7.397561] bec0: c0cc0dfc d7265f00 00000000 c0f4f564 00000000 c0f4f564 00000000 c05402c0&lt;BR /&gt;[ 7.496046] bee0: c0f4f550 c0e31428 c0f4f564 c054119c c0fa17c0 c0e31428 ffffe000 00000000&lt;BR /&gt;[ 7.594531] bf00: c0fac380 c0102c78 000005eb 00000000 d7fffd00 d7fffda3 d7fffd9d c0142020&lt;BR /&gt;[ 7.693016] bf20: d708bf20 c0d190f8 0000012f 00000000 00000006 00000006 d7fffdae d7fffdb4&lt;BR /&gt;[ 7.791501] bf40: 00000000 0000012f c0fac380 c0fa17c0 c0e87830 0000012f 00000007 c0fa17c0&lt;BR /&gt;[ 7.889986] bf60: c0e87834 c0e01000 00000006 00000006 00000000 c0e0049c d708a000 00000000&lt;BR /&gt;[ 7.988470] bf80: 00000000 00000000 c0a465d0 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 8.086955] bfa0: 00000000 c0a465d8 00000000 c01010e8 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 8.185439] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 8.283925] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000 00000000 00000000&lt;BR /&gt;[ 8.382426] [&amp;lt;c04999c4&amp;gt;] (dw_pcie_host_init) from [&amp;lt;c0e31524&amp;gt;] (ls_pcie_probe+0xe4/0x10c)&lt;BR /&gt;[ 8.480913] [&amp;lt;c0e31524&amp;gt;] (ls_pcie_probe) from [&amp;lt;c05410b0&amp;gt;] (platform_drv_probe+0x48/0x98)&lt;BR /&gt;[ 8.579396] [&amp;lt;c05410b0&amp;gt;] (platform_drv_probe) from [&amp;lt;c053f38c&amp;gt;] (really_probe+0x2b0/0x3c0)&lt;BR /&gt;[ 8.678927] [&amp;lt;c053f38c&amp;gt;] (really_probe) from [&amp;lt;c053f648&amp;gt;] (driver_probe_device+0x60/0x168)&lt;BR /&gt;[ 8.778459] [&amp;lt;c053f648&amp;gt;] (driver_probe_device) from [&amp;lt;c053f864&amp;gt;] (__driver_attach+0x114/0x134)&lt;BR /&gt;[ 8.882183] [&amp;lt;c053f864&amp;gt;] (__driver_attach) from [&amp;lt;c053d20c&amp;gt;] (bus_for_each_dev+0x64/0x90)&lt;BR /&gt;[ 8.980668] [&amp;lt;c053d20c&amp;gt;] (bus_for_each_dev) from [&amp;lt;c053e5f0&amp;gt;] (bus_add_driver+0x184/0x208)&lt;BR /&gt;[ 9.080198] [&amp;lt;c053e5f0&amp;gt;] (bus_add_driver) from [&amp;lt;c05402c0&amp;gt;] (driver_register+0x88/0x118)&lt;BR /&gt;[ 9.177637] [&amp;lt;c05402c0&amp;gt;] (driver_register) from [&amp;lt;c054119c&amp;gt;] (__platform_driver_probe+0x64/0x108)&lt;BR /&gt;[ 9.284505] [&amp;lt;c054119c&amp;gt;] (__platform_driver_probe) from [&amp;lt;c0102c78&amp;gt;] (do_one_initcall+0x44/0x1e4)&lt;BR /&gt;[ 9.391373] [&amp;lt;c0102c78&amp;gt;] (do_one_initcall) from [&amp;lt;c0e01000&amp;gt;] (kernel_init_freeable+0x26c/0x310)&lt;BR /&gt;[ 9.496150] [&amp;lt;c0e01000&amp;gt;] (kernel_init_freeable) from [&amp;lt;c0a465d8&amp;gt;] (kernel_init+0x8/0x10c)&lt;BR /&gt;[ 9.594637] [&amp;lt;c0a465d8&amp;gt;] (kernel_init) from [&amp;lt;c01010e8&amp;gt;] (ret_from_fork+0x14/0x2c)&lt;BR /&gt;[ 9.685781] Exception stack(0xd708bfb0 to 0xd708bff8)&lt;BR /&gt;[ 9.746549] bfa0: 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 9.845030] bfc0: 00000000 00000000 00000000 00000000 00000000 00000000 00000000 00000000&lt;BR /&gt;[ 9.943514] bfe0: 00000000 00000000 00000000 00000000 00000013 00000000&lt;BR /&gt;[ 10.023139] Code: e5143014 e3530000 0a00009f e5943050 (e5933000)&lt;BR /&gt;[ 10.096536] ---[ end trace 8a908bbfd8a662b3 ]---&lt;BR /&gt;[ 10.152112] Kernel panic - not syncing: Attempted to kill init! exitcode=0x0000000b&lt;BR /&gt;[ 10.152112]&lt;/P&gt;&lt;P&gt;So not sure if I have a hardware problem or software problem.&lt;/P&gt;&lt;P&gt;If you could point to things I may have not looked at or any suggestion, that could help.&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Renaud&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 06 Dec 2022 17:36:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-PCIe-driver-crashes/m-p/1565349#M11480</guid>
      <dc:creator>renaud</dc:creator>
      <dc:date>2022-12-06T17:36:24Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A PCIe driver crashes</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-PCIe-driver-crashes/m-p/1575335#M11553</link>
      <description>&lt;P&gt;&lt;SPAN&gt;For the error case, are you using linux kernel from LSDK? Seems this linux kernel is not released by NXP:&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.251637] layerscape-pcie 3400000.pcie: host bridge /soc/pcie@3400000 ranges:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.339741] layerscape-pcie 3400000.pcie: IO 0x4000010000..0x400001ffff -&amp;gt; 0x00000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.437213] layerscape-pcie 3400000.pcie: MEM 0x4040000000..0x407fffffff -&amp;gt; 0x40000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.534689] Unable to handle kernel NULL pointer dereference at virtual address 00000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.632140] pgd = (ptrval)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.664637] [00000000] *pgd=00000000&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[ 5.707615] Internal error: Oops: 5 [#1] SMP ARM&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;In your log, seems non-prefetchable memory resource not configured. In NXP released linux, it should print 36-bits address, this code is from our linux kernel:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; dev_dbg(dev, "Parsing ranges property...\n");&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; for_each_of_pci_range(&amp;amp;parser, &amp;amp;range) {&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; /* Read next ranges element */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; if ((range.flags &amp;amp; IORESOURCE_TYPE_BITS) == IORESOURCE_IO)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; range_type = "IO";&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; else if ((range.flags &amp;amp; IORESOURCE_TYPE_BITS) == IORESOURCE_MEM)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; range_type = "MEM";&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; else&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; range_type = "err";&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; dev_info(dev, " %6s %#012llx..%#012llx -&amp;gt; %#012llx\n",&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; range_type, range.cpu_addr,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; range.cpu_addr + range.size - 1, range.pci_addr);&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Dec 2022 01:31:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-PCIe-driver-crashes/m-p/1575335#M11553</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-12-29T01:31:18Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A PCIe driver crashes</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-PCIe-driver-crashes/m-p/2303791#M16433</link>
      <description>&lt;P&gt;Missing LPAE config in Linux if I remember correctly&lt;/P&gt;</description>
      <pubDate>Fri, 30 Jan 2026 12:54:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-PCIe-driver-crashes/m-p/2303791#M16433</guid>
      <dc:creator>renaud</dc:creator>
      <dc:date>2026-01-30T12:54:03Z</dc:date>
    </item>
  </channel>
</rss>