<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How does U-boot detect SATA drives? in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/How-does-U-boot-detect-SATA-drives/m-p/1566694#M11485</link>
    <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We boot from SD card on LS1028A-RDB, but U-boot doesn't detect SATA drive.&lt;BR /&gt;Already we have modified the LS1028A-RDB to use SATA interface, so the LS1028A-RDB is detected SATA drive on Linux OS.&lt;/P&gt;&lt;P&gt;How does U-boot detect SATA drives?&lt;/P&gt;&lt;P&gt;We have already modified the LS1028A-RDB and change RCW&amp;nbsp; to use SATA interface, so&amp;nbsp;the LS1028A-RDB&amp;nbsp;&amp;nbsp;detect SATA drive on Linux .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 08 Dec 2022 08:42:03 GMT</pubDate>
    <dc:creator>KZ</dc:creator>
    <dc:date>2022-12-08T08:42:03Z</dc:date>
    <item>
      <title>How does U-boot detect SATA drives?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-does-U-boot-detect-SATA-drives/m-p/1566694#M11485</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We boot from SD card on LS1028A-RDB, but U-boot doesn't detect SATA drive.&lt;BR /&gt;Already we have modified the LS1028A-RDB to use SATA interface, so the LS1028A-RDB is detected SATA drive on Linux OS.&lt;/P&gt;&lt;P&gt;How does U-boot detect SATA drives?&lt;/P&gt;&lt;P&gt;We have already modified the LS1028A-RDB and change RCW&amp;nbsp; to use SATA interface, so&amp;nbsp;the LS1028A-RDB&amp;nbsp;&amp;nbsp;detect SATA drive on Linux .&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Dec 2022 08:42:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-does-U-boot-detect-SATA-drives/m-p/1566694#M11485</guid>
      <dc:creator>KZ</dc:creator>
      <dc:date>2022-12-08T08:42:03Z</dc:date>
    </item>
    <item>
      <title>Re: How does U-boot detect SATA drives?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-does-U-boot-detect-SATA-drives/m-p/1566766#M11486</link>
      <description>&lt;P&gt;We use&amp;nbsp; &amp;nbsp;Layerscape(LSDK)&amp;nbsp; 21.08&lt;/P&gt;</description>
      <pubDate>Thu, 08 Dec 2022 10:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-does-U-boot-detect-SATA-drives/m-p/1566766#M11486</guid>
      <dc:creator>KZ</dc:creator>
      <dc:date>2022-12-08T10:06:42Z</dc:date>
    </item>
    <item>
      <title>Re: How does U-boot detect SATA drives?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-does-U-boot-detect-SATA-drives/m-p/1567419#M11490</link>
      <description>&lt;P&gt;The default u-boot source code provided in LSDK 21.08 for LS1028ARDB supports SATA.&lt;/P&gt;
&lt;PRE&gt;=&amp;gt; scsi reset

Reset SCSI
scanning bus for devices...
Target spinup took 0 ms.
AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst 
  Device 0: (0:0) Vendor: ATA Prod.: KINGSTON SA400M8 Rev: 0309
            Type: Hard Disk
            Capacity: 114473.4 MB = 111.7 GB (234441648 x 512)&lt;/PRE&gt;</description>
      <pubDate>Fri, 09 Dec 2022 09:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-does-U-boot-detect-SATA-drives/m-p/1567419#M11490</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-12-09T09:23:52Z</dc:date>
    </item>
    <item>
      <title>Re: How does U-boot detect SATA drives?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-does-U-boot-detect-SATA-drives/m-p/1567988#M11497</link>
      <description>We tried below in U-BOOT.&lt;BR /&gt;&lt;BR /&gt;--------------------------------------------------------------------------------&lt;BR /&gt;&lt;BR /&gt;=&amp;gt; scsi reset&lt;BR /&gt;&lt;BR /&gt;Reset SCSI&lt;BR /&gt;scanning bus for devices...&lt;BR /&gt;SATA link 0 timeout.&lt;BR /&gt;AHCI 0001.0301 32 slots 1 ports 6 Gbps 0x1 impl SATA mode&lt;BR /&gt;flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst&lt;BR /&gt;=&amp;gt;&lt;BR /&gt;&lt;BR /&gt;Reset SCSI&lt;BR /&gt;scanning bus for devices...&lt;BR /&gt;&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;&lt;BR /&gt;In Linux&amp;nbsp; log&lt;BR /&gt;[ 14.717390] ata1: SATA link down (SStatus 1 SControl 300)&lt;BR /&gt;[ 15.509285] ata1: limiting SATA link speed to 1.5 Gbps&lt;BR /&gt;[ 16.385402] ata1: SATA link up 1.5 Gbps (SStatus 113 SControl 310)&lt;BR /&gt;[ 16.394855] ata1.00: ATA-10: CFast 3IE4, L20420i, max UDMA/133&lt;BR /&gt;[ 16.400716] ata1.00: 31277232 sectors, multi 1: LBA48 NCQ (depth 32)&lt;BR /&gt;[ 16.415538] ata1.00: configured for UDMA/133&lt;BR /&gt;[ 16.420126] scsi 0:0:0:0: Direct-Access ATA CFast 3IE4 20i PQ: 0 ANSI: 5&lt;BR /&gt;[ 16.429191] sd 0:0:0:0: [sda] 31277232 512-byte logical blocks: (16.0 GB/14.9 GiB)&lt;BR /&gt;[ 16.436874] sd 0:0:0:0: [sda] Write Protect is off&lt;BR /&gt;[ 16.441739] sd 0:0:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA&lt;BR /&gt;[ 16.474405] sda: sda1 sda2 sda3 sda4&lt;BR /&gt;[ 16.480685] sd 0:0:0:0: [sda] Attached SCSI disk&lt;BR /&gt;[ 80.957385] ata1: SATA link down (SStatus 0 SControl 310)&lt;BR /&gt;[ 85.209384] ata1: SATA link up 1.5 Gbps (SStatus 113 SControl 310)&lt;BR /&gt;[ 85.227481] ata1.00: configured for UDMA/133&lt;BR /&gt;----------------------------------------------------------------------------------------------------&lt;BR /&gt;&lt;BR /&gt;In U-boot, Can we try to forced low speed link up ( SATA link up 1.5 Gbps)?&lt;BR /&gt;</description>
      <pubDate>Mon, 12 Dec 2022 06:43:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-does-U-boot-detect-SATA-drives/m-p/1567988#M11497</guid>
      <dc:creator>KZ</dc:creator>
      <dc:date>2022-12-12T06:43:10Z</dc:date>
    </item>
    <item>
      <title>Re: How does U-boot detect SATA drives?</title>
      <link>https://community.nxp.com/t5/Layerscape/How-does-U-boot-detect-SATA-drives/m-p/1576864#M11585</link>
      <description>&lt;P&gt;In u-boot, there is no command to implement this function, you need to modify u-boot source code to &lt;SPAN&gt;force low speed link up.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Jan 2023 06:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/How-does-U-boot-detect-SATA-drives/m-p/1576864#M11585</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2023-01-04T06:31:56Z</dc:date>
    </item>
  </channel>
</rss>