<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1021A-RWT PNOR</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1021A-RWT-PNOR/m-p/1559571#M11442</link>
    <description>&lt;P&gt;Hi, renaud&lt;/P&gt;
&lt;P&gt;No, it means that the bus connected to the NOR Flash is normal.&lt;/P&gt;
&lt;P&gt;Regarding this application note regarding the bid and little endianness. The LS1 IFC uses big endian format, reversing it would set to you write to the NOR Flash normally.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Joseph Linares&lt;/P&gt;</description>
    <pubDate>Thu, 24 Nov 2022 17:19:41 GMT</pubDate>
    <dc:creator>JosephAtNXP</dc:creator>
    <dc:date>2022-11-24T17:19:41Z</dc:date>
    <item>
      <title>LS1021A-RWT PNOR</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-RWT-PNOR/m-p/1558686#M11436</link>
      <description>&lt;P&gt;Looking at U-boot (LSDK-21.08) I see that for the ls1021a-twr configuration file, there is a flag&amp;nbsp;CONFIG_SYS_WRITE_SWAPPED_DATA which is used in the cfi_flash.c driver.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does that mean the data bus connection to the NOR is bit swapped on the ls1021a-twr?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;Renaud&lt;/P&gt;</description>
      <pubDate>Wed, 23 Nov 2022 15:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-RWT-PNOR/m-p/1558686#M11436</guid>
      <dc:creator>renaud</dc:creator>
      <dc:date>2022-11-23T15:35:19Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A-RWT PNOR</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-RWT-PNOR/m-p/1559571#M11442</link>
      <description>&lt;P&gt;Hi, renaud&lt;/P&gt;
&lt;P&gt;No, it means that the bus connected to the NOR Flash is normal.&lt;/P&gt;
&lt;P&gt;Regarding this application note regarding the bid and little endianness. The LS1 IFC uses big endian format, reversing it would set to you write to the NOR Flash normally.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Joseph Linares&lt;/P&gt;</description>
      <pubDate>Thu, 24 Nov 2022 17:19:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-RWT-PNOR/m-p/1559571#M11442</guid>
      <dc:creator>JosephAtNXP</dc:creator>
      <dc:date>2022-11-24T17:19:41Z</dc:date>
    </item>
    <item>
      <title>Re: LS1021A-RWT PNOR</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1021A-RWT-PNOR/m-p/1562722#M11456</link>
      <description>&lt;P&gt;Thanks for the documentation. Byte-swap in the driver allows me to write to the flash. Still have to do the write buffer support as programming is very slow otherwise&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 09:37:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1021A-RWT-PNOR/m-p/1562722#M11456</guid>
      <dc:creator>renaud</dc:creator>
      <dc:date>2022-12-01T09:37:22Z</dc:date>
    </item>
  </channel>
</rss>