<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscapeのトピック回复： Whether RPMsg and SRTM can be used for communicate between virtual partition in LS1028A</title>
    <link>https://community.nxp.com/t5/Layerscape/Whether-RPMsg-and-SRTM-can-be-used-for-communicate-between/m-p/1559194#M11439</link>
    <description>&lt;P&gt;&lt;SPAN&gt;1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In real-time-edge-v2.3, RPMSG and SRTM are only used for virtual uart case between A-core(linux) and M-core(RTOS),&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if want to use it in jailhouse, you should porting and modify the related code to Linux kernel or inmate system in jailhouse,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;you can refer to drivers/tty/rpmsg_tty.c in linux.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In jailhouse, there is inbuilt virtual NIC based on shared memory, you can refer to the keyword "JAILHOUSE_SHMEM_PROTO_VETH" in jailhouse code,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the virtual NIC can implement Interpartition communication.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 24 Nov 2022 07:40:56 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-11-24T07:40:56Z</dc:date>
    <item>
      <title>Whether RPMsg and SRTM can be used for communicate between virtual partition in LS1028A</title>
      <link>https://community.nxp.com/t5/Layerscape/Whether-RPMsg-and-SRTM-can-be-used-for-communicate-between/m-p/1545549#M11338</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I noticed the addition of RPMSG and SRTM capabilities for inter-core communication and device sharing in RT-Edge v2.3.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;However, the documentation I found for RPMSG and SRTM was for the i.MX8 product platform, and I didn't see more detailed instructions.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Where can I find more detailed instructions on how to use RPMSG and SRTM?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Whether RPMsg and SRTM can be used for &lt;SPAN&gt;inter-core communication and device sharing between virtualized partitions in LS1028A?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 28 Oct 2022 07:34:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Whether-RPMsg-and-SRTM-can-be-used-for-communicate-between/m-p/1545549#M11338</guid>
      <dc:creator>jiaweilin</dc:creator>
      <dc:date>2022-10-28T07:34:43Z</dc:date>
    </item>
    <item>
      <title>回复： Whether RPMsg and SRTM can be used for communicate between virtual partition in LS1028A</title>
      <link>https://community.nxp.com/t5/Layerscape/Whether-RPMsg-and-SRTM-can-be-used-for-communicate-between/m-p/1550733#M11379</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Could you give me some advice?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Nov 2022 05:48:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Whether-RPMsg-and-SRTM-can-be-used-for-communicate-between/m-p/1550733#M11379</guid>
      <dc:creator>jiaweilin</dc:creator>
      <dc:date>2022-11-09T05:48:13Z</dc:date>
    </item>
    <item>
      <title>回复： Whether RPMsg and SRTM can be used for communicate between virtual partition in LS1028A</title>
      <link>https://community.nxp.com/t5/Layerscape/Whether-RPMsg-and-SRTM-can-be-used-for-communicate-between/m-p/1551590#M11385</link>
      <description>&lt;P&gt;&lt;SPAN&gt;RPMsg and SRTM can't be used in LS1028A platform in RT-edge v2.3&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;about RPmsg, you can refer to the following link:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;A href="https://www.kernel.org/doc/html/latest/staging/rpmsg.html" target="_blank"&gt;https://www.kernel.org/doc/html/latest/staging/rpmsg.html&lt;/A&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;thanks&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Nov 2022 03:28:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Whether-RPMsg-and-SRTM-can-be-used-for-communicate-between/m-p/1551590#M11385</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-11-10T03:28:12Z</dc:date>
    </item>
    <item>
      <title>回复： Whether RPMsg and SRTM can be used for communicate between virtual partition in LS1028A</title>
      <link>https://community.nxp.com/t5/Layerscape/Whether-RPMsg-and-SRTM-can-be-used-for-communicate-between/m-p/1551883#M11390</link>
      <description>&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Thank you for the reply.&amp;nbsp;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;I have the following two questions.&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;1.&lt;/SPAN&gt;&lt;/SPAN&gt;Whether it can be done that&amp;nbsp;&lt;SPAN class=""&gt;&lt;SPAN&gt;implement inter-partition communication of jailhouse based on RPMsg on LS1028 by modifying DeviceTree or Linux driver? &lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;Can you provide relevant modification cases or explain what needs to be modified?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class=""&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;2. Does RT-Edge provide Jailhouse's original shared memory-based inter-partition communication API?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt; Or where can I find instructions for the Jailhouse Interpartition communication API?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;thanks!&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Nov 2022 09:56:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Whether-RPMsg-and-SRTM-can-be-used-for-communicate-between/m-p/1551883#M11390</guid>
      <dc:creator>jiaweilin</dc:creator>
      <dc:date>2022-11-10T09:56:33Z</dc:date>
    </item>
    <item>
      <title>回复： Whether RPMsg and SRTM can be used for communicate between virtual partition in LS1028A</title>
      <link>https://community.nxp.com/t5/Layerscape/Whether-RPMsg-and-SRTM-can-be-used-for-communicate-between/m-p/1559194#M11439</link>
      <description>&lt;P&gt;&lt;SPAN&gt;1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In real-time-edge-v2.3, RPMSG and SRTM are only used for virtual uart case between A-core(linux) and M-core(RTOS),&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if want to use it in jailhouse, you should porting and modify the related code to Linux kernel or inmate system in jailhouse,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;you can refer to drivers/tty/rpmsg_tty.c in linux.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;2.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;In jailhouse, there is inbuilt virtual NIC based on shared memory, you can refer to the keyword "JAILHOUSE_SHMEM_PROTO_VETH" in jailhouse code,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;the virtual NIC can implement Interpartition communication.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 24 Nov 2022 07:40:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Whether-RPMsg-and-SRTM-can-be-used-for-communicate-between/m-p/1559194#M11439</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-11-24T07:40:56Z</dc:date>
    </item>
  </channel>
</rss>