<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS1043A as network switch using OpenWRT</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1043A-as-network-switch-using-OpenWRT/m-p/1552063#M11392</link>
    <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/43353"&gt;@bpe&lt;/a&gt;&amp;nbsp;Platon,&lt;/P&gt;&lt;P&gt;Haven't really thanked you on this.&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 10 Nov 2022 15:15:57 GMT</pubDate>
    <dc:creator>carljones</dc:creator>
    <dc:date>2022-11-10T15:15:57Z</dc:date>
    <item>
      <title>LS1043A as network switch using OpenWRT</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-as-network-switch-using-OpenWRT/m-p/1317333#M8634</link>
      <description>&lt;P&gt;Hello NXP,&lt;/P&gt;&lt;P&gt;I connected VSC8531 and VSC8575 PHYs to an LS1043A chip to create a 6-port media server running on OpenWRT. I tried to configure one port as WAN and the rest of the ports as 5-port switch. Did you have a guide on how to achieve this? Currently, each port is configured independently, as if an individual network card on a PC.&lt;/P&gt;&lt;P&gt;Kind regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;</description>
      <pubDate>Tue, 03 Aug 2021 12:15:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-as-network-switch-using-OpenWRT/m-p/1317333#M8634</guid>
      <dc:creator>carljones</dc:creator>
      <dc:date>2021-08-03T12:15:40Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A as network switch using OpenWRT</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-as-network-switch-using-OpenWRT/m-p/1323298#M8708</link>
      <description>&lt;P&gt;There is no dedicated support in LSDK to L2 bridging for processors equipped &lt;BR /&gt;with DPAA1. You can use the kernel L2 bridge, which is a pure software&lt;BR /&gt;implementation and should work with any generic Ethernet interface driver.&lt;BR /&gt;Details on the kernel native Ethernet bridge can be found at &lt;A href="https://wiki.linuxfoundation.org/networking/bridge" target="_self"&gt;this link.&lt;/A&gt;&lt;BR /&gt;For hardware-accelerated bridging, consider moving to a DPAA2 processor,&lt;BR /&gt;LS1088, LS2088, LX2160 and their derivatives.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;BR /&gt;Platon&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 13 Aug 2021 14:58:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-as-network-switch-using-OpenWRT/m-p/1323298#M8708</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2021-08-13T14:58:06Z</dc:date>
    </item>
    <item>
      <title>Re: LS1043A as network switch using OpenWRT</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1043A-as-network-switch-using-OpenWRT/m-p/1552063#M11392</link>
      <description>&lt;P&gt;Hi &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/43353"&gt;@bpe&lt;/a&gt;&amp;nbsp;Platon,&lt;/P&gt;&lt;P&gt;Haven't really thanked you on this.&lt;/P&gt;&lt;P&gt;Thank you very much.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Nov 2022 15:15:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1043A-as-network-switch-using-OpenWRT/m-p/1552063#M11392</guid>
      <dc:creator>carljones</dc:creator>
      <dc:date>2022-11-10T15:15:57Z</dc:date>
    </item>
  </channel>
</rss>