<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1046A u-boot unstable in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1551018#M11382</link>
    <description>&lt;P&gt;Thank you, I can edit the timing parameters now.&lt;/P&gt;&lt;P&gt;Sorry but now I have another problem.&lt;/P&gt;&lt;P&gt;I have 4x2GB DDR4 chips on the board, sharing 1 chip select.&lt;/P&gt;&lt;P&gt;The bus width is 64bit, no ECC.&lt;/P&gt;&lt;P&gt;When I use this config as attached, u-boot can only detect 1.9GB memory.&lt;/P&gt;&lt;P&gt;Do you know where is the problem?&lt;/P&gt;</description>
    <pubDate>Wed, 09 Nov 2022 11:30:21 GMT</pubDate>
    <dc:creator>__OTL__</dc:creator>
    <dc:date>2022-11-09T11:30:21Z</dc:date>
    <item>
      <title>LS1046A u-boot unstable</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1547389#M11348</link>
      <description>&lt;P&gt;Hi I'm bringup our own board.&lt;/P&gt;&lt;P&gt;U-boot is unstable and stucks in different place every time.&lt;/P&gt;&lt;P&gt;Here are 3 stuck log&amp;nbsp;&lt;/P&gt;&lt;P&gt;1. stuck at DRAM INFO&lt;/P&gt;&lt;P&gt;U-Boot 2020.04-dirty (Nov 01 2022 - 18:09:02 +0900)&lt;/P&gt;&lt;PRE&gt;SoC: LS1046AE Rev1.0 (0x87070010)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;CPU0(A72):1600 MHz CPU1(A72):1600 MHz CPU2(A72):1600 MHz&lt;BR /&gt;CPU3(A72):1600 MHz&lt;BR /&gt;Bus: 600 MHz DDR: 1600 MT/s FMAN: 900 MHz&lt;BR /&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 0c100010 12000000 00000000 00000000&lt;BR /&gt;00000010: 10405577 40a00016 40000000 c1000000&lt;BR /&gt;00000020: 00200000 00000000 00000000 0003affc&lt;BR /&gt;00000030: 20004504 04201101 00000096 00000001&lt;BR /&gt;Model: LS1046A FRWY Board&lt;BR /&gt;Board: LS1046AFRWY, Rev: B, boot from QSPI&lt;BR /&gt;SD1_CLK1 = 100.00MHZ, SD1_CLK2 = 100.00MHZ&lt;BR /&gt;DRAM: 7.9 GiB (DDR4, 64-bit, CL=11, ECC off)&lt;/PRE&gt;&lt;P&gt;2.stuck with&amp;nbsp;"Synchronous Abort" handler&lt;/P&gt;&lt;PRE&gt;U-Boot 2020.04-dirty (Nov 01 2022 - 18:09:02 +0900)&lt;BR /&gt;&lt;BR /&gt;SoC: LS1046AE Rev1.0 (0x87070010)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt;CPU0(A72):1600 MHz CPU1(A72):1600 MHz CPU2(A72):1600 MHz&lt;BR /&gt;CPU3(A72):1600 MHz&lt;BR /&gt;Bus: 600 MHz DDR: 1600 MT/s FMAN: 900 MHz&lt;BR /&gt;Reset Configuration Word (RCW):&lt;BR /&gt;00000000: 0c100010 12000000 00000000 00000000&lt;BR /&gt;00000010: 10405577 40a00016 40000000 c1000000&lt;BR /&gt;00000020: 00200000 00000000 00000000 0003affc&lt;BR /&gt;00000030: 20004504 04201101 00000096 00000001&lt;BR /&gt;Model: LS1046A FRWY Board&lt;BR /&gt;Board: LS1046AFRWY, Rev: B, boot from QSPI&lt;BR /&gt;SD1_CLK1 = 100.00MHZ, SD1_CLK2 = 100.00MHZ&lt;BR /&gt;DRAM: 7.9 GiB (DDR4, 64-bit, CL=11, ECC off)&lt;BR /&gt;Using SERDES1 Protocol: 4160 (0x1040)&lt;BR /&gt;Using SERDES2 Protocol: 21879 (0x5577)&lt;BR /&gt;NAND: fsl_ifc_chip_init: address did not match any chip selects&lt;BR /&gt;0 MiB&lt;BR /&gt;MMC: FSL_SDHC: 0&lt;BR /&gt;EEPROM: Read failed.&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;BR /&gt;Net: Invalid SerDes protocol 0x1040 for LS1046AFRWY&lt;BR /&gt;unrecognized JEDEC id bytes: ef, 60, 18&lt;BR /&gt;"Synchronous Abort" handler, esr 0x96000004&lt;BR /&gt;elr: 000000008204a6a4 lr : 000000008204a68c (reloc)&lt;BR /&gt;elr: 00000000fbd786a4 lr : 00000000fbd7868c&lt;BR /&gt;x0 : f2a12001d2808001 x1 : 0000000000001070&lt;BR /&gt;x2 : 00000000fbdc8000 x3 : 0000000000001071&lt;BR /&gt;x4 : 00000000fbc2b880 x5 : 00000000fbc2bd60&lt;BR /&gt;x6 : 00000000fbdc83f0 x7 : 00000000fbdc8400&lt;BR /&gt;x8 : 00000000fbc43ad0 x9 : 0000000000000008&lt;BR /&gt;x10: 0000000000000010 x11: 00000000fbc26f8c&lt;BR /&gt;x12: 0000000000001238 x13: 0000000000001174&lt;BR /&gt;x14: 00000000fbc26fdc x15: 0000000000000002&lt;BR /&gt;x16: 0000000000000000 x17: 0000000000000000&lt;BR /&gt;x18: 00000000fbc29dc0 x19: 00000000fbc33ad0&lt;BR /&gt;x20: f2a12001d2808001 x21: 0000000001a00000&lt;BR /&gt;x22: 0000000000000000 x23: 0000000000000000&lt;BR /&gt;x24: 0000000000000000 x25: 0000000000000000&lt;BR /&gt;x26: 0000000000000000 x27: 0000000000000000&lt;BR /&gt;x28: 0000000000000000 x29: 00000000fbc27200&lt;BR /&gt;&lt;BR /&gt;Code: 90000200 91089c00 9400b6f5 17ffffd7 (f940c400)&lt;BR /&gt;Resetting CPU ...&lt;BR /&gt;&lt;BR /&gt;resetting ...&lt;/PRE&gt;&lt;P&gt;3. stuck at the same place with case 2, but with a different synchronous handler.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Should this be considered as a DDR setting issue?&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 04:58:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1547389#M11348</guid>
      <dc:creator>__OTL__</dc:creator>
      <dc:date>2022-11-02T04:58:29Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A u-boot unstable</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1547431#M11349</link>
      <description>&lt;P&gt;Probably this u-boot unstable problem is caused by the improper DDR controller configuration.&lt;/P&gt;
&lt;P&gt;It's better to use QCVS DDRv tool to connect to your custom board to do validation and optimization to get the optimized DDR controller configuration parameters.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 05:53:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1547431#M11349</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-11-02T05:53:16Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A u-boot unstable</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1547513#M11351</link>
      <description>&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;I'm using QorlQ&amp;nbsp;Version: 11.5.5 Build Id: 210930 to config DDR,&lt;/P&gt;&lt;P&gt;but for some parameters in Timing Configuration&amp;nbsp;&lt;/P&gt;&lt;P&gt;such like tRAS=29clocks in Timing Configuration 1 and 3&lt;/P&gt;&lt;P&gt;once I select a different value, it get back to default value by itself.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I can't change the value...&lt;/P&gt;&lt;P&gt;Do you have any idea to fix the problem?&lt;/P&gt;</description>
      <pubDate>Wed, 02 Nov 2022 07:30:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1547513#M11351</guid>
      <dc:creator>__OTL__</dc:creator>
      <dc:date>2022-11-02T07:30:08Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A u-boot unstable</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1548154#M11356</link>
      <description>&lt;P&gt;Please click "Advanced" on the right top of the panel, then configure "Enable timing editing" as "yes" under "SDRAM Timing Configurations".&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="yipingwang_0-1667463498534.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/199018i89BB54541F29A450/image-size/medium?v=v2&amp;amp;px=400" role="button" title="yipingwang_0-1667463498534.png" alt="yipingwang_0-1667463498534.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Nov 2022 08:18:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1548154#M11356</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-11-03T08:18:47Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A u-boot unstable</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1551018#M11382</link>
      <description>&lt;P&gt;Thank you, I can edit the timing parameters now.&lt;/P&gt;&lt;P&gt;Sorry but now I have another problem.&lt;/P&gt;&lt;P&gt;I have 4x2GB DDR4 chips on the board, sharing 1 chip select.&lt;/P&gt;&lt;P&gt;The bus width is 64bit, no ECC.&lt;/P&gt;&lt;P&gt;When I use this config as attached, u-boot can only detect 1.9GB memory.&lt;/P&gt;&lt;P&gt;Do you know where is the problem?&lt;/P&gt;</description>
      <pubDate>Wed, 09 Nov 2022 11:30:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1551018#M11382</guid>
      <dc:creator>__OTL__</dc:creator>
      <dc:date>2022-11-09T11:30:21Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A u-boot unstable</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1551773#M11388</link>
      <description>&lt;P&gt;In atf source code&amp;nbsp;flexbuild_lsdk2108/components/firmware/atf, please modify "DDR Compilation Configs" in&amp;nbsp;plat/nxp/soc-ls1046a/ls1046afrwy/platform.mk.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 10 Nov 2022 08:13:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-u-boot-unstable/m-p/1551773#M11388</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-11-10T08:13:06Z</dc:date>
    </item>
  </channel>
</rss>