<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: LS2080A capability</title>
    <link>https://community.nxp.com/t5/Layerscape/LS2080A-capability/m-p/508800#M1138</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One more question.&lt;/P&gt;&lt;P&gt;It has 4 PCIE controller.&lt;/P&gt;&lt;P&gt;Is it possible to use 2 lanes PCIE x 4 at single serdes block like below?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2x4.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58430i5058D07F3CBA3D24/image-size/large?v=v2&amp;amp;px=999" role="button" title="2x4.jpg" alt="2x4.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Mar 2016 08:43:43 GMT</pubDate>
    <dc:creator>JHY</dc:creator>
    <dc:date>2016-03-08T08:43:43Z</dc:date>
    <item>
      <title>LS2080A capability</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2080A-capability/m-p/508798#M1136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, experts.&lt;/P&gt;&lt;P&gt;LS2080A has total 16 serdes lanes for variable purpose.&lt;/P&gt;&lt;P&gt;So, please confirm below options are able to be implemented in LS2080A.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. simultaneously up to 5.8G input to LS2080A and up to 2.4G output from LS2080A by PCIE.&lt;/P&gt;&lt;P&gt;2. vice versa 5.8G output from LS2080A and up to 2.4G input to LS2080A by PCIE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Mar 2016 06:49:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2080A-capability/m-p/508798#M1136</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2016-03-07T06:49:24Z</dc:date>
    </item>
    <item>
      <title>Re: LS2080A capability</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2080A-capability/m-p/508799#M1137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LS2080 can support much higher than you specified data rates at the SecDes and on-chip interconnect&lt;/P&gt;&lt;P&gt;levels. I's ability to support a certain type of protocol or application&amp;nbsp; at some&amp;nbsp; data rate, however,&amp;nbsp; depends on&lt;/P&gt;&lt;P&gt;both the application/protocol type and the implementation. Contact a distributor in your region for&lt;/P&gt;&lt;P&gt;advanced performance information.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Mar 2016 08:33:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2080A-capability/m-p/508799#M1137</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2016-03-07T08:33:38Z</dc:date>
    </item>
    <item>
      <title>Re: LS2080A capability</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2080A-capability/m-p/508800#M1138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;One more question.&lt;/P&gt;&lt;P&gt;It has 4 PCIE controller.&lt;/P&gt;&lt;P&gt;Is it possible to use 2 lanes PCIE x 4 at single serdes block like below?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="2x4.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/58430i5058D07F3CBA3D24/image-size/large?v=v2&amp;amp;px=999" role="button" title="2x4.jpg" alt="2x4.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Mar 2016 08:43:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2080A-capability/m-p/508800#M1138</guid>
      <dc:creator>JHY</dc:creator>
      <dc:date>2016-03-08T08:43:43Z</dc:date>
    </item>
    <item>
      <title>Re: LS2080A capability</title>
      <link>https://community.nxp.com/t5/Layerscape/LS2080A-capability/m-p/508801#M1139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is too confused. Two lanes mean PCIe x2. PCIe x4 requires four lanes. The picture displays four PCIe controllers connected&lt;/P&gt;&lt;P&gt;to an 8-lane SerDes, which obviously can be done in several bus width combinations. Refer to the chip Manual, Section 25.1.2.1 for available SerDes protocol combinations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Mar 2016 11:13:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS2080A-capability/m-p/508801#M1139</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2016-03-09T11:13:30Z</dc:date>
    </item>
  </channel>
</rss>