<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックMultiple bootable SD cards on the SDHC1 controller</title>
    <link>https://community.nxp.com/t5/Layerscape/Multiple-bootable-SD-cards-on-the-SDHC1-controller/m-p/1549861#M11373</link>
    <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;Looks like it is possible to connect several SD cards to the same SD controller (SDHC1) on LX2160A SoC since it supports&amp;nbsp; ALL_SEND_CID broadcast command which allows to select SD card to operate with. Is it correct?&lt;/P&gt;&lt;P&gt;If yes, is it possible to do such a trick and to somehow select a proper boot source during boot process selecting one of SD cards connected to the same SDHC1 controller?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
    <pubDate>Mon, 07 Nov 2022 18:40:16 GMT</pubDate>
    <dc:creator>dstepanov</dc:creator>
    <dc:date>2022-11-07T18:40:16Z</dc:date>
    <item>
      <title>Multiple bootable SD cards on the SDHC1 controller</title>
      <link>https://community.nxp.com/t5/Layerscape/Multiple-bootable-SD-cards-on-the-SDHC1-controller/m-p/1549861#M11373</link>
      <description>&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;Looks like it is possible to connect several SD cards to the same SD controller (SDHC1) on LX2160A SoC since it supports&amp;nbsp; ALL_SEND_CID broadcast command which allows to select SD card to operate with. Is it correct?&lt;/P&gt;&lt;P&gt;If yes, is it possible to do such a trick and to somehow select a proper boot source during boot process selecting one of SD cards connected to the same SDHC1 controller?&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;</description>
      <pubDate>Mon, 07 Nov 2022 18:40:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Multiple-bootable-SD-cards-on-the-SDHC1-controller/m-p/1549861#M11373</guid>
      <dc:creator>dstepanov</dc:creator>
      <dc:date>2022-11-07T18:40:16Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple bootable SD cards on the SDHC1 controller</title>
      <link>https://community.nxp.com/t5/Layerscape/Multiple-bootable-SD-cards-on-the-SDHC1-controller/m-p/1553789#M11406</link>
      <description>&lt;P&gt;&lt;SPAN&gt;In theory, it is possible to do that. However, we have not done any validation on this. We do not have any board designed such way.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I would not mess around about the boot source as the BOOTROM is fixed in silicon. &lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 15 Nov 2022 07:29:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Multiple-bootable-SD-cards-on-the-SDHC1-controller/m-p/1553789#M11406</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-11-15T07:29:13Z</dc:date>
    </item>
  </channel>
</rss>