<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: restool create dpmac</title>
    <link>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1546258#M11344</link>
    <description>&lt;P&gt;Hmm. I have been provided with a validated pbi override that performs the above for SERDES, but it seems I need a new (different) behavior for the MC complex, as I understand from you that 31 is a fixed profile that does not match my needs. It's unfortunate that the MC does not read the serdes configuration directly, and instead operates off it's own table, making it the point of failure in this scenario.&lt;/P&gt;</description>
    <pubDate>Mon, 31 Oct 2022 10:09:37 GMT</pubDate>
    <dc:creator>dsouthwi</dc:creator>
    <dc:date>2022-10-31T10:09:37Z</dc:date>
    <item>
      <title>restool create dpmac</title>
      <link>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1535811#M11270</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm looking for info/help on how restool/MC-utils determines the number of dpmac devices that are available, and how I can modify this. Does it have it's own SERDES lookup table somewhere?&lt;/P&gt;&lt;P&gt;For example on the lx2160a:&lt;/P&gt;&lt;P&gt;If I boot with SD1=8, I see 8 dpmac devices corresponding the 8xUSXGMII lanes.&lt;/P&gt;&lt;P&gt;If I boot with SD1=17, I see 4 dpmac corresponding the the 4x25GE (and none for PCIe lanes).&lt;/P&gt;&lt;P&gt;If I boot with SD1=17 (modified to have 4x25G+4xUSGMII) I only get 4 dpmac.&lt;/P&gt;&lt;P&gt;Modifying the DPL file to declare more dpmac lanes is discarded/ignored by restool.&lt;/P&gt;&lt;P&gt;Modifying the SERDES definition in u-boot SERDES table is discarded/ignored by restool.&lt;/P&gt;&lt;P&gt;Trying to manually add more dpmac via restool results in :&lt;/P&gt;&lt;PRE&gt;&amp;gt; restool dpmac create --mac-id=7  #create dpmac.7&lt;BR /&gt;MC error: Invalid state (status 0xc)&lt;BR /&gt;&amp;gt; restool --mc-version&lt;BR /&gt;MC firmware version 10.28.1&lt;/PRE&gt;&lt;P&gt;My SFP modules are detected during kernel boot in the USXGMII lanes, but I cannot create dpni objects as I lack dpmac for them. I can use the 25G dpmac however.&lt;/P&gt;&lt;P&gt;I have modified my SERDES (following Application Note #&lt;SPAN&gt;AN13022) to have 4x25G+4xUSXGMII, but I cannot determine what in LSDK21.08 is blocking MC-utils from creating dpmac for these interfaces.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Is there any documentation / help on this?&lt;/P&gt;</description>
      <pubDate>Tue, 11 Oct 2022 19:15:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1535811#M11270</guid>
      <dc:creator>dsouthwi</dc:creator>
      <dc:date>2022-10-11T19:15:14Z</dc:date>
    </item>
    <item>
      <title>Re: restool create dpmac</title>
      <link>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1536128#M11274</link>
      <description>&lt;P&gt;Please refer to section "26.1.4 SerDes options" in&amp;nbsp;LX2160ARM.pdf, dpmac number is determined by&amp;nbsp;SerDes 1 protocol(RCW[SRDS_PRTCL_S1]), you cannot add more dpmac lanes.&lt;/P&gt;</description>
      <pubDate>Wed, 12 Oct 2022 08:42:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1536128#M11274</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-10-12T08:42:27Z</dc:date>
    </item>
    <item>
      <title>Re: restool create dpmac</title>
      <link>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1536349#M11278</link>
      <description>Right, I understand what the reference manual says, but I am referring to &lt;A href="https://www.nxp.com/docs/en/application-note/AN13022.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN13022.pdf&lt;/A&gt; where they state "MC firmware versions 10.24.1 and later add support for [serdes] protocol 31". Where is the information related to MC and protocol 31 limitation, etc?</description>
      <pubDate>Wed, 12 Oct 2022 15:12:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1536349#M11278</guid>
      <dc:creator>dsouthwi</dc:creator>
      <dc:date>2022-10-12T15:12:41Z</dc:date>
    </item>
    <item>
      <title>Re: restool create dpmac</title>
      <link>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1540964#M11293</link>
      <description>&lt;P&gt;If configuring SerDes 1 as protocol 31, you only can get 4xUSXGMII lanes, you only can get 4 DPMACs for these interfaces. It is still impossible to add more dpmacs manually.&lt;/P&gt;</description>
      <pubDate>Thu, 20 Oct 2022 08:09:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1540964#M11293</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-10-20T08:09:34Z</dc:date>
    </item>
    <item>
      <title>Re: restool create dpmac</title>
      <link>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1546258#M11344</link>
      <description>&lt;P&gt;Hmm. I have been provided with a validated pbi override that performs the above for SERDES, but it seems I need a new (different) behavior for the MC complex, as I understand from you that 31 is a fixed profile that does not match my needs. It's unfortunate that the MC does not read the serdes configuration directly, and instead operates off it's own table, making it the point of failure in this scenario.&lt;/P&gt;</description>
      <pubDate>Mon, 31 Oct 2022 10:09:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1546258#M11344</guid>
      <dc:creator>dsouthwi</dc:creator>
      <dc:date>2022-10-31T10:09:37Z</dc:date>
    </item>
    <item>
      <title>Re: restool create dpmac</title>
      <link>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1630083#M12207</link>
      <description>&lt;P&gt;Given that recent DPAA2 MC firmware support changing the DPMAC lane speeds (see DPAA2 user manual for 10.36.x, section &lt;SPAN&gt;15.2.21&lt;/SPAN&gt; &lt;SPAN&gt;DPMAC_SET_PROTOCOL&lt;/SPAN&gt; ) would it be possible to change the protocol from 25G to 10G?&lt;/P&gt;</description>
      <pubDate>Sat, 08 Apr 2023 12:08:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/restool-create-dpmac/m-p/1630083#M12207</guid>
      <dc:creator>dsouthwi</dc:creator>
      <dc:date>2023-04-08T12:08:17Z</dc:date>
    </item>
  </channel>
</rss>