<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1028 - ATF Logs using LPUART in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1028-ATF-Logs-using-LPUART/m-p/1534833#M11261</link>
    <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;It's already enabled. We do have the logs for U-Boot but not for ATF.&lt;BR /&gt;&lt;BR /&gt;When we enable DUART1, we have both U-Boot and ATF Logs.&lt;/P&gt;</description>
    <pubDate>Mon, 10 Oct 2022 11:53:27 GMT</pubDate>
    <dc:creator>cguer</dc:creator>
    <dc:date>2022-10-10T11:53:27Z</dc:date>
    <item>
      <title>LS1028 - ATF Logs using LPUART</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-ATF-Logs-using-LPUART/m-p/1530536#M11226</link>
      <description>&lt;P&gt;Hi NXP community !&lt;BR /&gt;&lt;BR /&gt;I wanted to know what to configure on ATF so that the ATF logs ( logs starting with NOTICE: ) could be prompted in the console using LPUART6?&lt;BR /&gt;&lt;BR /&gt;I know that in ATF to link the console to the right device, we should define NXP_CONSOLE_ADDR with the ADDR of the device, like that :&lt;/P&gt;&lt;LI-CODE lang="c"&gt;#define NXP_CONSOLE_ADDR NXP_UART_ADDR&lt;/LI-CODE&gt;&lt;P&gt;Than, I checked the file &lt;STRONG&gt;plat/nxp/soc-ls1028/include/soc.h&amp;nbsp;&lt;/STRONG&gt;to see which MACRO to use, and i see following ADDR related to UART:&lt;/P&gt;&lt;LI-CODE lang="c"&gt;#define NXP_UART_ADDR 0x021C0500
#define NXP_UART1_ADDR 0x021C0600&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;But nothing about LPUART.&lt;/P&gt;&lt;P&gt;So i tried to create my own define with the address of the LPUART but with no success.&lt;BR /&gt;&lt;BR /&gt;Any suggestions?&lt;BR /&gt;&lt;BR /&gt;Thanks in advance &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Sep 2022 14:40:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-ATF-Logs-using-LPUART/m-p/1530536#M11226</guid>
      <dc:creator>cguer</dc:creator>
      <dc:date>2022-09-29T14:40:54Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028 - ATF Logs using LPUART</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-ATF-Logs-using-LPUART/m-p/1534738#M11260</link>
      <description>&lt;P&gt;You need to configure RCW[UART1_SOUTSIN_PMUX] and RCW[UART2_SOUTSIN_PMUX] as 3 to enable LPUART6&lt;/P&gt;
&lt;P&gt;No need to modify ATF source code.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Oct 2022 09:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-ATF-Logs-using-LPUART/m-p/1534738#M11260</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-10-10T09:32:21Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028 - ATF Logs using LPUART</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-ATF-Logs-using-LPUART/m-p/1534833#M11261</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;It's already enabled. We do have the logs for U-Boot but not for ATF.&lt;BR /&gt;&lt;BR /&gt;When we enable DUART1, we have both U-Boot and ATF Logs.&lt;/P&gt;</description>
      <pubDate>Mon, 10 Oct 2022 11:53:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-ATF-Logs-using-LPUART/m-p/1534833#M11261</guid>
      <dc:creator>cguer</dc:creator>
      <dc:date>2022-10-10T11:53:27Z</dc:date>
    </item>
    <item>
      <title>Re: LS1028 - ATF Logs using LPUART</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1028-ATF-Logs-using-LPUART/m-p/1535457#M11267</link>
      <description>&lt;P&gt;ATF doesn't provide LPUART driver for ls1028a processor.&lt;/P&gt;</description>
      <pubDate>Tue, 11 Oct 2022 08:17:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1028-ATF-Logs-using-LPUART/m-p/1535457#M11267</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-10-11T08:17:26Z</dc:date>
    </item>
  </channel>
</rss>