<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1046A development board DPAA in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046A-development-board-DPAA/m-p/1526901#M11211</link>
    <description>Thank you.</description>
    <pubDate>Thu, 22 Sep 2022 18:35:29 GMT</pubDate>
    <dc:creator>bijan</dc:creator>
    <dc:date>2022-09-22T18:35:29Z</dc:date>
    <item>
      <title>LS1046A development board DPAA</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-development-board-DPAA/m-p/1520166#M11142</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are working with a Layerscape FRWY-LS1046A development board, using a Yocto build, and SDK version 2.0-1703.&lt;/P&gt;&lt;P&gt;Currently, we have IPSec set up and working but are seeing poor performance. We are investigating using DPAA and have seen some promising examples with ipsec-secgw in DPDK.&lt;/P&gt;&lt;P&gt;Are there any specific tools that allow for secure tunnels closer to wire speed and that support packet fragmentation? Is ipsec-secgw a path we should investigate?&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Sep 2022 23:10:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-development-board-DPAA/m-p/1520166#M11142</guid>
      <dc:creator>bijan</dc:creator>
      <dc:date>2022-09-09T23:10:58Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A development board DPAA</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-development-board-DPAA/m-p/1523466#M11173</link>
      <description>&lt;P&gt;&lt;SPAN&gt;ipsec-secgw doesn't have fragmentation feature.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;It can reach the line speed for 1442 large packets.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Sep 2022 07:36:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-development-board-DPAA/m-p/1523466#M11173</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-09-16T07:36:34Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A development board DPAA</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-development-board-DPAA/m-p/1526901#M11211</link>
      <description>Thank you.</description>
      <pubDate>Thu, 22 Sep 2022 18:35:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-development-board-DPAA/m-p/1526901#M11211</guid>
      <dc:creator>bijan</dc:creator>
      <dc:date>2022-09-22T18:35:29Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046A development board DPAA</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046A-development-board-DPAA/m-p/1618836#M12059</link>
      <description>&lt;P&gt;In the latest DPDK versions 22+ I see, an option&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;--reassemble NUM&lt;/PRE&gt;&lt;P&gt;Is it valid or not?&amp;nbsp;&lt;BR /&gt;I see the code also, present for the same. It uses, librte_ipsec does ip fragmentation and reassembly.&lt;/P&gt;&lt;P&gt;we see SEC error 0x20001b1a being received at times on [Tx or Rx path]. So when we try to run SSH from end-2-end it fails.&lt;/P&gt;&lt;P&gt;Normal ping passes.&lt;/P&gt;&lt;P&gt;even pings with higher packet -size like 1800/1900 also pass.&lt;BR /&gt;&lt;BR /&gt;we are stuck with this problem over SSH/SCP not working.&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;Any direction would be of great help to us in proceeding in the project.&lt;BR /&gt;&lt;BR /&gt;Thanks, Arun Ayachith&lt;/P&gt;</description>
      <pubDate>Tue, 21 Mar 2023 03:59:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046A-development-board-DPAA/m-p/1618836#M12059</guid>
      <dc:creator>arun_ayachith</dc:creator>
      <dc:date>2023-03-21T03:59:44Z</dc:date>
    </item>
  </channel>
</rss>