<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Proper RCW/PBI boot sequence in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Proper-RCW-PBI-boot-sequence/m-p/1519899#M11138</link>
    <description>&lt;P&gt;This command loads the 1024 bit Reset Configuration Word from the interface specified by Power-on Reset Configuration strapping pins (POR Config pins).&lt;BR /&gt;The RCW will generally always be present, though it is possible to specify through POR configuration pin strapping that a hardcoded RCW value is to be used by the hardware. In this case the service processor will not look for an RCW.&lt;/P&gt;</description>
    <pubDate>Fri, 09 Sep 2022 09:18:21 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-09-09T09:18:21Z</dc:date>
    <item>
      <title>Proper RCW/PBI boot sequence</title>
      <link>https://community.nxp.com/t5/Layerscape/Proper-RCW-PBI-boot-sequence/m-p/1509057#M11057</link>
      <description>&lt;P&gt;LX2160A Reference Manual (Rev. 0RH, 07/2020) in detailed Power-On reset description (4.9.5, table 11) states that initially Service processor loads RCW (stage 13) and only after that loads and executes PBI commands (stage 18).&lt;/P&gt;&lt;P&gt;But my XSPI flash image (generated using solidrun’s BSP&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://github.com/SolidRun/lx2160a_build" target="_blank" rel="noopener nofollow ugc"&gt;GitHub - SolidRun/lx2160a_build: Scripts to build basic images for LX2160A COM express type 7 modules&lt;/A&gt;) at 0 offset contains PBI Image Preamble (bytes 55 AA 55 AA) which defines that it is a PBI block (not RCW). And the first PBI command - loading RCW (bytes 00 00 10 80).&lt;BR /&gt;So actually after power-on reset Service Processor first executes PBI commands and the first PBI command is to load RCW. This contradicts with description in user’s manual. What is the proper RCW/PBI boot order?&lt;/P&gt;</description>
      <pubDate>Sun, 21 Aug 2022 12:51:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Proper-RCW-PBI-boot-sequence/m-p/1509057#M11057</guid>
      <dc:creator>dstepanov</dc:creator>
      <dc:date>2022-08-21T12:51:37Z</dc:date>
    </item>
    <item>
      <title>Re: Proper RCW/PBI boot sequence</title>
      <link>https://community.nxp.com/t5/Layerscape/Proper-RCW-PBI-boot-sequence/m-p/1519899#M11138</link>
      <description>&lt;P&gt;This command loads the 1024 bit Reset Configuration Word from the interface specified by Power-on Reset Configuration strapping pins (POR Config pins).&lt;BR /&gt;The RCW will generally always be present, though it is possible to specify through POR configuration pin strapping that a hardcoded RCW value is to be used by the hardware. In this case the service processor will not look for an RCW.&lt;/P&gt;</description>
      <pubDate>Fri, 09 Sep 2022 09:18:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Proper-RCW-PBI-boot-sequence/m-p/1519899#M11138</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-09-09T09:18:21Z</dc:date>
    </item>
  </channel>
</rss>