<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LX2160A second RCW source in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LX2160A-second-RCW-source/m-p/1509056#M11056</link>
    <description>&lt;P&gt;Hello! I’m using LX2160A clearfog development board and trying to implement reliable boot in case of failure of one of the boot sources (eMMC/SD/SPI).&lt;/P&gt;&lt;P&gt;LX2160A Reference Manual (Rev. 0RH, 07/2020) in detailed Power-On reset description (4.9.5, table 11, stage 13) points that it is possible to use second RCW source&lt;/P&gt;&lt;BLOCKQUOTE dir="ltr"&gt;&lt;P&gt;If the Service processor detects that the RCW loading failed, it initiates RCW loading from a second RCW source. If boot fails from the RCW loaded at offset 0 or 0x1000 (in case of SD), the boot ROM searches for RCW at 8 MB (8 MB + 0x1000 for SD) offset on the device.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I’m little bit confused with this description - what really happens if boot fails? where the second RCW source is selected? Does the boot process try to read RCW from first boot source (using 2 offsets) and if these 2 attempts fails it performs another 2 attempts (with 2 different offsets)?&lt;/P&gt;</description>
    <pubDate>Sun, 21 Aug 2022 12:48:32 GMT</pubDate>
    <dc:creator>dstepanov</dc:creator>
    <dc:date>2022-08-21T12:48:32Z</dc:date>
    <item>
      <title>LX2160A second RCW source</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-second-RCW-source/m-p/1509056#M11056</link>
      <description>&lt;P&gt;Hello! I’m using LX2160A clearfog development board and trying to implement reliable boot in case of failure of one of the boot sources (eMMC/SD/SPI).&lt;/P&gt;&lt;P&gt;LX2160A Reference Manual (Rev. 0RH, 07/2020) in detailed Power-On reset description (4.9.5, table 11, stage 13) points that it is possible to use second RCW source&lt;/P&gt;&lt;BLOCKQUOTE dir="ltr"&gt;&lt;P&gt;If the Service processor detects that the RCW loading failed, it initiates RCW loading from a second RCW source. If boot fails from the RCW loaded at offset 0 or 0x1000 (in case of SD), the boot ROM searches for RCW at 8 MB (8 MB + 0x1000 for SD) offset on the device.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I’m little bit confused with this description - what really happens if boot fails? where the second RCW source is selected? Does the boot process try to read RCW from first boot source (using 2 offsets) and if these 2 attempts fails it performs another 2 attempts (with 2 different offsets)?&lt;/P&gt;</description>
      <pubDate>Sun, 21 Aug 2022 12:48:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-second-RCW-source/m-p/1509056#M11056</guid>
      <dc:creator>dstepanov</dc:creator>
      <dc:date>2022-08-21T12:48:32Z</dc:date>
    </item>
    <item>
      <title>Re: LX2160A second RCW source</title>
      <link>https://community.nxp.com/t5/Layerscape/LX2160A-second-RCW-source/m-p/1519903#M11139</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The RM needs to be corrected. There is no&amp;nbsp;&lt;/SPAN&gt;&lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;second&lt;/STRONG&gt;&lt;/FONT&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;RCW&lt;/STRONG&gt;&lt;/FONT&gt;&lt;SPAN&gt;&amp;nbsp;source. This was initially planned but due to certain hardware issues, could not be implemented. &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;The statement should be removed:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I/O drivers for the backup&amp;nbsp;&lt;/SPAN&gt;&lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;RCW&lt;/STRONG&gt;&lt;/FONT&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;source&lt;/STRONG&gt;&lt;/FONT&gt;&lt;SPAN&gt;&amp;nbsp;are enabled, specifically those pins associated only with the secondary&amp;nbsp;&lt;/SPAN&gt;&lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;RCW&lt;/STRONG&gt;&lt;/FONT&gt;&lt;SPAN&gt;&amp;nbsp;interface.However in LX2160, we do have a provision of secondary&amp;nbsp;&lt;/SPAN&gt;&lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;RCW&lt;/STRONG&gt;&lt;/FONT&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;source&lt;/STRONG&gt;&lt;/FONT&gt;&lt;SPAN&gt;&amp;nbsp;on the same boot device. If boot fails from&amp;nbsp;&lt;/SPAN&gt;&lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;RCW&lt;/STRONG&gt;&lt;/FONT&gt;&lt;SPAN&gt;&amp;nbsp;loaded at offset 0 or 0x1000 ( in case of SD), ROM searches for&amp;nbsp;&lt;/SPAN&gt;&lt;FONT class="&amp;amp;quothighlight&amp;quot;"&gt;&lt;STRONG&gt;RCW&lt;/STRONG&gt;&lt;/FONT&gt;&lt;SPAN&gt;&amp;nbsp;at 8 MB (8 Mb + 0x1000 for SD) offset on the device.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 09 Sep 2022 09:26:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LX2160A-second-RCW-source/m-p/1519903#M11139</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-09-09T09:26:17Z</dc:date>
    </item>
  </channel>
</rss>