<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Code Warrior DDR4 Validation Not Working on Tool 11.5 Version in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/Code-Warrior-DDR4-Validation-Not-Working-on-Tool-11-5-Version/m-p/1505501#M11018</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are trying DDR4 validation testing in LS1046A - custom designed board using the Code Warrior Tap tool. The DDR4 validation testing is not able to successfully initialized if we are using Code warrior application version &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;11.5.&lt;/STRONG&gt;&lt;/FONT&gt; It throws the below error,&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;"D&lt;SPAN&gt;DR initialization failed: D_INIT was not cleared by hardware!"&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;But, if we try with &lt;FONT color="#008000"&gt;&lt;STRONG&gt;11.4&lt;/STRONG&gt; &lt;/FONT&gt;version the above error is not happening and also we are able to perform the DDR4 validation successfully (tested for 1KB and 100KB size).&lt;/P&gt;&lt;P&gt;Please share your comments what could be the reason for DDR4 validation is not working in the latest code warrior application version 11.5.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ganesh&lt;/P&gt;</description>
    <pubDate>Fri, 12 Aug 2022 09:12:50 GMT</pubDate>
    <dc:creator>CGganesh</dc:creator>
    <dc:date>2022-08-12T09:12:50Z</dc:date>
    <item>
      <title>Code Warrior DDR4 Validation Not Working on Tool 11.5 Version</title>
      <link>https://community.nxp.com/t5/Layerscape/Code-Warrior-DDR4-Validation-Not-Working-on-Tool-11-5-Version/m-p/1505501#M11018</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We are trying DDR4 validation testing in LS1046A - custom designed board using the Code Warrior Tap tool. The DDR4 validation testing is not able to successfully initialized if we are using Code warrior application version &lt;FONT color="#FF0000"&gt;&lt;STRONG&gt;11.5.&lt;/STRONG&gt;&lt;/FONT&gt; It throws the below error,&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;"D&lt;SPAN&gt;DR initialization failed: D_INIT was not cleared by hardware!"&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;But, if we try with &lt;FONT color="#008000"&gt;&lt;STRONG&gt;11.4&lt;/STRONG&gt; &lt;/FONT&gt;version the above error is not happening and also we are able to perform the DDR4 validation successfully (tested for 1KB and 100KB size).&lt;/P&gt;&lt;P&gt;Please share your comments what could be the reason for DDR4 validation is not working in the latest code warrior application version 11.5.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ganesh&lt;/P&gt;</description>
      <pubDate>Fri, 12 Aug 2022 09:12:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Code-Warrior-DDR4-Validation-Not-Working-on-Tool-11-5-Version/m-p/1505501#M11018</guid>
      <dc:creator>CGganesh</dc:creator>
      <dc:date>2022-08-12T09:12:50Z</dc:date>
    </item>
    <item>
      <title>Re: Code Warrior DDR4 Validation Not Working on Tool 11.5 Version</title>
      <link>https://community.nxp.com/t5/Layerscape/Code-Warrior-DDR4-Validation-Not-Working-on-Tool-11-5-Version/m-p/1506127#M11025</link>
      <description>&lt;P&gt;CodeWarrior initialization file provided in CodeWarrior is used for NXP demo board, you need to customize it for your custom board.&lt;/P&gt;
&lt;P&gt;In "Target Connections" panel, please click "LS1046A_RDB(1)" to open "Target Initialization File" panel, please modify "DDR Initialization" section according to your custom board.&lt;/P&gt;
&lt;P&gt;We often recommend customers use QCVS DDR tool to do DDR validation and optimization to get the optimized parameters, then use these parameter in CW initialization file.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Aug 2022 09:32:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Code-Warrior-DDR4-Validation-Not-Working-on-Tool-11-5-Version/m-p/1506127#M11025</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-08-15T09:32:20Z</dc:date>
    </item>
  </channel>
</rss>