<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1046ARDB (RJ45-to-DB9F) RJ45 UART port is not reposonse</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-to-DB9F-RJ45-UART-port-is-not-reposonse/m-p/1502820#M10999</link>
    <description>&lt;P class=""&gt;Hi all,&lt;/P&gt;&lt;P class=""&gt;I am trying to access theLS1046ARDB console connection from the UART to the COM by using the RJ45-to-DB9F cable.&lt;/P&gt;&lt;P class=""&gt;I have changed the SW4[4] on my LS1046ARDB board to 0 and configured the teraterm configure serial speed at 115200, but there is no connection that can be established.&lt;/P&gt;&lt;P class=""&gt;Could you please tell me:&lt;/P&gt;&lt;P class=""&gt;1. Is there any other setup I need to configure to make it work, etc., driver?&lt;/P&gt;&lt;P class=""&gt;If not, can you suggest another method to make the connection work besides connecting to the front port?&lt;/P&gt;&lt;P class=""&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 08 Aug 2022 21:52:06 GMT</pubDate>
    <dc:creator>Em31</dc:creator>
    <dc:date>2022-08-08T21:52:06Z</dc:date>
    <item>
      <title>LS1046ARDB (RJ45-to-DB9F) RJ45 UART port is not reposonse</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-to-DB9F-RJ45-UART-port-is-not-reposonse/m-p/1502820#M10999</link>
      <description>&lt;P class=""&gt;Hi all,&lt;/P&gt;&lt;P class=""&gt;I am trying to access theLS1046ARDB console connection from the UART to the COM by using the RJ45-to-DB9F cable.&lt;/P&gt;&lt;P class=""&gt;I have changed the SW4[4] on my LS1046ARDB board to 0 and configured the teraterm configure serial speed at 115200, but there is no connection that can be established.&lt;/P&gt;&lt;P class=""&gt;Could you please tell me:&lt;/P&gt;&lt;P class=""&gt;1. Is there any other setup I need to configure to make it work, etc., driver?&lt;/P&gt;&lt;P class=""&gt;If not, can you suggest another method to make the connection work besides connecting to the front port?&lt;/P&gt;&lt;P class=""&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 08 Aug 2022 21:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-to-DB9F-RJ45-UART-port-is-not-reposonse/m-p/1502820#M10999</guid>
      <dc:creator>Em31</dc:creator>
      <dc:date>2022-08-08T21:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: LS1046ARDB (RJ45-to-DB9F) RJ45 UART port is not reposonse</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-to-DB9F-RJ45-UART-port-is-not-reposonse/m-p/1504366#M11010</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;For the Teraterm, did you configure all the parameters as mentioned in the Getting Start Guide?&lt;/P&gt;&lt;P&gt;I use an RJ45-to-USB cable instead, and it works for me. I only need to install the USB driver on my Win10 pc.&lt;/P&gt;</description>
      <pubDate>Thu, 11 Aug 2022 00:56:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1046ARDB-RJ45-to-DB9F-RJ45-UART-port-is-not-reposonse/m-p/1504366#M11010</guid>
      <dc:creator>Chanh</dc:creator>
      <dc:date>2022-08-11T00:56:45Z</dc:date>
    </item>
  </channel>
</rss>