<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックLS1024A SPI inquiry</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1024A-SPI-inquiry/m-p/1502317#M10991</link>
    <description>&lt;P&gt;May I ask about the SPI interface on the LS1024A?&lt;/P&gt;&lt;P&gt;The SPI interface is similar to the LS1024ARDB Schematic.&lt;/P&gt;&lt;P&gt;Related URLs:&lt;BR /&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/layerscape-processors/layerscape-1024a-dual-core-processor:LS1024A" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/layerscape-processors/layerscape-1024a-dual-core-processor:LS1024A&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The SPI interface does not work.&lt;/P&gt;&lt;P&gt;SCLK and SPI_SS1 are output as HIGH on the SPI interface.&lt;/P&gt;&lt;P&gt;There is a symptom that the clock does not come out from the SCLK pin and the chip select does not work on the CS pin.&lt;/P&gt;&lt;P&gt;What can I do to resolve these symptoms?&lt;/P&gt;</description>
    <pubDate>Mon, 08 Aug 2022 06:17:48 GMT</pubDate>
    <dc:creator>h201668</dc:creator>
    <dc:date>2022-08-08T06:17:48Z</dc:date>
    <item>
      <title>LS1024A SPI inquiry</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1024A-SPI-inquiry/m-p/1502317#M10991</link>
      <description>&lt;P&gt;May I ask about the SPI interface on the LS1024A?&lt;/P&gt;&lt;P&gt;The SPI interface is similar to the LS1024ARDB Schematic.&lt;/P&gt;&lt;P&gt;Related URLs:&lt;BR /&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/layerscape-processors/layerscape-1024a-dual-core-processor:LS1024A" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/arm-processors/layerscape-processors/layerscape-1024a-dual-core-processor:LS1024A&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The SPI interface does not work.&lt;/P&gt;&lt;P&gt;SCLK and SPI_SS1 are output as HIGH on the SPI interface.&lt;/P&gt;&lt;P&gt;There is a symptom that the clock does not come out from the SCLK pin and the chip select does not work on the CS pin.&lt;/P&gt;&lt;P&gt;What can I do to resolve these symptoms?&lt;/P&gt;</description>
      <pubDate>Mon, 08 Aug 2022 06:17:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1024A-SPI-inquiry/m-p/1502317#M10991</guid>
      <dc:creator>h201668</dc:creator>
      <dc:date>2022-08-08T06:17:48Z</dc:date>
    </item>
  </channel>
</rss>