<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LayerscapeのトピックRe: Can Codewarrior tap for LS1028ardb be used to debug both the cores at the same time</title>
    <link>https://community.nxp.com/t5/Layerscape/Can-Codewarrior-tap-for-LS1028ardb-be-used-to-debug-both-the/m-p/1498965#M10970</link>
    <description>&lt;P&gt;On CodeWarrior, using the Debug Configurations-&amp;gt; ‘Trace and profile’, you can see which cores you can debug.&lt;BR /&gt;For further information we have a document called “Enabling DAP on QorIQ LS1028A Processor”, Please note that this document is only provided if there is an active NDA.&lt;BR /&gt;I highly recommend you to put a new ticket asking for an NDA to obtain that document.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Hector Villarruel&lt;/P&gt;</description>
    <pubDate>Mon, 01 Aug 2022 18:01:12 GMT</pubDate>
    <dc:creator>Hector_Villarruel</dc:creator>
    <dc:date>2022-08-01T18:01:12Z</dc:date>
    <item>
      <title>Can Codewarrior tap for LS1028ardb be used to debug both the cores at the same time</title>
      <link>https://community.nxp.com/t5/Layerscape/Can-Codewarrior-tap-for-LS1028ardb-be-used-to-debug-both-the/m-p/1494907#M10933</link>
      <description>&lt;P&gt;I am using the Codewarrior TAP on the LS1028ardb. I can successfully debug on core 0. Can I deploy same elf or two different elfs on both the cores 0 and 1 at the same time in bareboard style and debug them together? I debug configurations I seem to be able to choose either of the cores or both cores but nothing happens when this option is selected. Its only working on Core 0. I did notice in the gic.c file it sets it up for core 0 so I can why core 1 does not work. But just wanted to know if that even works?&lt;/P&gt;</description>
      <pubDate>Mon, 25 Jul 2022 14:58:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Can-Codewarrior-tap-for-LS1028ardb-be-used-to-debug-both-the/m-p/1494907#M10933</guid>
      <dc:creator>SoccerMom</dc:creator>
      <dc:date>2022-07-25T14:58:21Z</dc:date>
    </item>
    <item>
      <title>Re: Can Codewarrior tap for LS1028ardb be used to debug both the cores at the same time</title>
      <link>https://community.nxp.com/t5/Layerscape/Can-Codewarrior-tap-for-LS1028ardb-be-used-to-debug-both-the/m-p/1498965#M10970</link>
      <description>&lt;P&gt;On CodeWarrior, using the Debug Configurations-&amp;gt; ‘Trace and profile’, you can see which cores you can debug.&lt;BR /&gt;For further information we have a document called “Enabling DAP on QorIQ LS1028A Processor”, Please note that this document is only provided if there is an active NDA.&lt;BR /&gt;I highly recommend you to put a new ticket asking for an NDA to obtain that document.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Hector Villarruel&lt;/P&gt;</description>
      <pubDate>Mon, 01 Aug 2022 18:01:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Can-Codewarrior-tap-for-LS1028ardb-be-used-to-debug-both-the/m-p/1498965#M10970</guid>
      <dc:creator>Hector_Villarruel</dc:creator>
      <dc:date>2022-08-01T18:01:12Z</dc:date>
    </item>
    <item>
      <title>Re: Can Codewarrior tap for LS1028ardb be used to debug both the cores at the same time</title>
      <link>https://community.nxp.com/t5/Layerscape/Can-Codewarrior-tap-for-LS1028ardb-be-used-to-debug-both-the/m-p/1499017#M10971</link>
      <description>&lt;P&gt;Thanks Hector.&lt;/P&gt;</description>
      <pubDate>Mon, 01 Aug 2022 21:08:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/Can-Codewarrior-tap-for-LS1028ardb-be-used-to-debug-both-the/m-p/1499017#M10971</guid>
      <dc:creator>SoccerMom</dc:creator>
      <dc:date>2022-08-01T21:08:35Z</dc:date>
    </item>
  </channel>
</rss>