<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscapeのトピックdpkg error when I use LSDK 20.04 to build code</title>
    <link>https://community.nxp.com/t5/Layerscape/dpkg-error-when-I-use-LSDK-20-04-to-build-code/m-p/1488391#M10861</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use LSDK 20.04 update290520 to build code.&lt;BR /&gt;When I set the FETCH_PREBUILT_LSDK_RFS to n, it will occur the error as below.&lt;/P&gt;&lt;P&gt;The user `syslog' is already a member of `adm'.&lt;BR /&gt;dpkg: error processing package rsyslog (--configure):&lt;BR /&gt;installed rsyslog package post-installation script subprocess returned error exit status 1&lt;/P&gt;&lt;P&gt;...&lt;BR /&gt;...&lt;/P&gt;&lt;P&gt;Errors were encountered while processing:&lt;BR /&gt;rsyslog&lt;BR /&gt;E: Sub-process /usr/bin/dpkg returned an error code (1)&lt;/P&gt;&lt;P&gt;The attached log is my build log.&lt;BR /&gt;please help me to clarify it.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
    <pubDate>Wed, 13 Jul 2022 02:07:02 GMT</pubDate>
    <dc:creator>tzongruey</dc:creator>
    <dc:date>2022-07-13T02:07:02Z</dc:date>
    <item>
      <title>dpkg error when I use LSDK 20.04 to build code</title>
      <link>https://community.nxp.com/t5/Layerscape/dpkg-error-when-I-use-LSDK-20-04-to-build-code/m-p/1488391#M10861</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I use LSDK 20.04 update290520 to build code.&lt;BR /&gt;When I set the FETCH_PREBUILT_LSDK_RFS to n, it will occur the error as below.&lt;/P&gt;&lt;P&gt;The user `syslog' is already a member of `adm'.&lt;BR /&gt;dpkg: error processing package rsyslog (--configure):&lt;BR /&gt;installed rsyslog package post-installation script subprocess returned error exit status 1&lt;/P&gt;&lt;P&gt;...&lt;BR /&gt;...&lt;/P&gt;&lt;P&gt;Errors were encountered while processing:&lt;BR /&gt;rsyslog&lt;BR /&gt;E: Sub-process /usr/bin/dpkg returned an error code (1)&lt;/P&gt;&lt;P&gt;The attached log is my build log.&lt;BR /&gt;please help me to clarify it.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 02:07:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/dpkg-error-when-I-use-LSDK-20-04-to-build-code/m-p/1488391#M10861</guid>
      <dc:creator>tzongruey</dc:creator>
      <dc:date>2022-07-13T02:07:02Z</dc:date>
    </item>
    <item>
      <title>Re: dpkg error when I use LSDK 20.04 to build code</title>
      <link>https://community.nxp.com/t5/Layerscape/dpkg-error-when-I-use-LSDK-20-04-to-build-code/m-p/1488534#M10864</link>
      <description>&lt;P&gt;&lt;SPAN&gt;The following change can resolve the problem when upgrading the newer ubuntu-18.04:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;+++ b/tools/flex-mkdistrorfs&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;@@ -203,11 +203,12 @@ do_distrorfs_second_stage() {&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; apt -y install language-pack-en-base&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fi&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fi&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;-&amp;nbsp;&amp;nbsp;&amp;nbsp; apt -y upgrade&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; test -f /proc/uptime || mount -t proc proc /proc&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; test -f /dev/pts/ptmx || mount -t devpts devpts /dev/pts&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp; apt -y upgrade&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Then rebuild it as below:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;$ flex-builder -i clean-rfs&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;$ flex-builder -i mkrfs&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 13 Jul 2022 06:41:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/dpkg-error-when-I-use-LSDK-20-04-to-build-code/m-p/1488534#M10864</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-07-13T06:41:22Z</dc:date>
    </item>
  </channel>
</rss>