<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LS1020A  RTC questions in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/LS1020A-RTC-questions/m-p/503966#M1082</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have the following follow up questions.&amp;nbsp; Please help answer these. In advance, thank you.&lt;/P&gt;&lt;P&gt;1) &lt;SPAN style="font-size: 9.5pt;"&gt;App note AN5097 states:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;&lt;BR /&gt; • Bit-swap is only allowed within a nibble.&lt;BR /&gt; • Bit-swap across two nibbles is not allowed.&lt;BR /&gt; &lt;BR /&gt; Does this note refer to just x4 memory configurations (where there is one DQS pair per 4-bits)? Or does it also refer to x8 configurations (where there is one DQS pair per 8-bits)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;2) In app note AN5097 it states "17 For QorIQ products with DDR3L and DDR4 memory options, there is an external VREF pin available for DDR3L mode. When DDR4 mode is used the external VREF pin needs to be grounded."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;To which pin is it referring as I don't see an equivalent comment in the reference manual?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) In an earlier email it was suggested that the TA_BB_RTC be driven from a 1.8V device. However, &lt;SPAN style="font-size: 9.5pt;"&gt;I am using TA_BB_RTC as my clock input which is powered from TA_BB_VDD (which is a 1V supply), surely the I/O voltage to that pin should be a maximum of 1V? Or is the pin tolerant to a higher voltage? Where in the datasheet does it show the recommended maximum voltage driving pin R6?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;4) It looks to me like there is an inconsistency in the datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Page 20 says MDC/MDIO are related to L1VDD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Page 61 says that Ethernet Management Interface is powered by LVDD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Page 92 says that the MDC/MDIO pins are available on LVDD and L1VDD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Could you clarify which comment is correct, and perhaps get the datasheet corrected.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;5) It looks to me like there is another inconsistency in the datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Page 51 says DVDD is 1.8 V ± 90 mV&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;The schematics for LS1021A-IOT and TWR-LS1021A-PB both have DVDD connected to 3.3V I/O.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Pin J2 is a good example.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Could you tell me the real voltage range for DVDD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;6) Could you please confirm that the power draw highlighted in yellow in the attached is the total power drawn by both the AVDD_SD1_PLL1/2 pins, and not per PLL pin.&lt;span class="lia-inline-image-display-wrapper" image-alt="PLL_Power.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21497iF3608D4BEB228A62/image-size/large?v=v2&amp;amp;px=999" role="button" title="PLL_Power.PNG" alt="PLL_Power.PNG" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jan 2016 18:11:27 GMT</pubDate>
    <dc:creator>enriqueencarnac</dc:creator>
    <dc:date>2016-01-19T18:11:27Z</dc:date>
    <item>
      <title>LS1020A  RTC questions</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1020A-RTC-questions/m-p/503964#M1080</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just finding my way around the documentation for the LS1020A but cannot seem to find anything about the RTC (real-time clock) capability (or lack of it). Is there an RTC on chip that just requires an external battery, or what is the device type I need to connect to pin TA_BB_RTC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) On what pin should I provide my 32768Hz clock for the LS1020A, is it TA_BB_RTC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2) At what voltage levels?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) Which pin is the battery voltage supplied on, is it TA_BB_VDD?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4) What is the current draw from the battery pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not using the trust/SecMon feature if that question comes up.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Dec 2015 18:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1020A-RTC-questions/m-p/503964#M1080</guid>
      <dc:creator>enriqueencarnac</dc:creator>
      <dc:date>2015-12-23T18:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: LS1020A  RTC questions</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1020A-RTC-questions/m-p/503965#M1081</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt; color: black;"&gt;1) The &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;TA_BB_RTC or RTC pins can be used as clock source for the LS1021A RTC. See the Figure 4-8 of the LS1021A Reference Manual:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt; color: black;"&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=LS1021ARM&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf&amp;amp;Parent_nodeId=1378142598972722203474&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=LS1021ARM&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Reference%20Manuals&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf&amp;amp;Parent_nodeId=1378142598972722203474&amp;amp;Parent_pageType=product&lt;/A&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt; color: black;"&gt;2) Recommended value is 1.8V. See the Table 3 of the LS1021A Datasheet:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt; color: black;"&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=LS1021A&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf&amp;amp;Parent_nodeId=1378142598972722203474&amp;amp;Parent_pageType=product"&gt;https://www.nxp.com/webapp/Download?colCode=LS1021A&amp;amp;location=null&amp;amp;fpsp=1&amp;amp;WT_TYPE=Data%20Sheets&amp;amp;WT_VENDOR=FREESCALE&amp;amp;WT_FILE_FORMAT=pdf&amp;amp;WT_ASSET=Documentation&amp;amp;fileExt=.pdf&amp;amp;Parent_nodeId=1378142598972722203474&amp;amp;Parent_pageType=product&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt; color: black;"&gt;3) Yes, the &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;TA_BB_VDD pins is power supply pin for the TA_BB_RTC pin. See the Table 1 of the LS1021 Datasheet. Find the TA_BB_RTC pin and power supply for this pin.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt; color: black;"&gt;The &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;OVDD is power supply for the &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;RTC&lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;/GPIO1_14 pin. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt; color: black;"&gt;4) See the Table 6 of the LS1021A Datasheet. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Dec 2015 05:10:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1020A-RTC-questions/m-p/503965#M1081</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2015-12-24T05:10:08Z</dc:date>
    </item>
    <item>
      <title>Re: LS1020A  RTC questions</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1020A-RTC-questions/m-p/503966#M1082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I have the following follow up questions.&amp;nbsp; Please help answer these. In advance, thank you.&lt;/P&gt;&lt;P&gt;1) &lt;SPAN style="font-size: 9.5pt;"&gt;App note AN5097 states:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;&lt;BR /&gt; • Bit-swap is only allowed within a nibble.&lt;BR /&gt; • Bit-swap across two nibbles is not allowed.&lt;BR /&gt; &lt;BR /&gt; Does this note refer to just x4 memory configurations (where there is one DQS pair per 4-bits)? Or does it also refer to x8 configurations (where there is one DQS pair per 8-bits)?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;2) In app note AN5097 it states "17 For QorIQ products with DDR3L and DDR4 memory options, there is an external VREF pin available for DDR3L mode. When DDR4 mode is used the external VREF pin needs to be grounded."&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;To which pin is it referring as I don't see an equivalent comment in the reference manual?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3) In an earlier email it was suggested that the TA_BB_RTC be driven from a 1.8V device. However, &lt;SPAN style="font-size: 9.5pt;"&gt;I am using TA_BB_RTC as my clock input which is powered from TA_BB_VDD (which is a 1V supply), surely the I/O voltage to that pin should be a maximum of 1V? Or is the pin tolerant to a higher voltage? Where in the datasheet does it show the recommended maximum voltage driving pin R6?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;4) It looks to me like there is an inconsistency in the datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Page 20 says MDC/MDIO are related to L1VDD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Page 61 says that Ethernet Management Interface is powered by LVDD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Page 92 says that the MDC/MDIO pins are available on LVDD and L1VDD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Could you clarify which comment is correct, and perhaps get the datasheet corrected.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;5) It looks to me like there is another inconsistency in the datasheet.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Page 51 says DVDD is 1.8 V ± 90 mV&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;The schematics for LS1021A-IOT and TWR-LS1021A-PB both have DVDD connected to 3.3V I/O.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Pin J2 is a good example.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;Could you tell me the real voltage range for DVDD.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 9.5pt;"&gt;6) Could you please confirm that the power draw highlighted in yellow in the attached is the total power drawn by both the AVDD_SD1_PLL1/2 pins, and not per PLL pin.&lt;span class="lia-inline-image-display-wrapper" image-alt="PLL_Power.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21497iF3608D4BEB228A62/image-size/large?v=v2&amp;amp;px=999" role="button" title="PLL_Power.PNG" alt="PLL_Power.PNG" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jan 2016 18:11:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1020A-RTC-questions/m-p/503966#M1082</guid>
      <dc:creator>enriqueencarnac</dc:creator>
      <dc:date>2016-01-19T18:11:27Z</dc:date>
    </item>
    <item>
      <title>Re: LS1020A  RTC questions</title>
      <link>https://community.nxp.com/t5/Layerscape/LS1020A-RTC-questions/m-p/503967#M1083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;1. It is information from the JEDEC Standard No. 21C:&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;&lt;A class="jive-link-external-small" href="https://www.google.ru/url?sa=t&amp;amp;rct=j&amp;amp;q=&amp;amp;esrc=s&amp;amp;source=web&amp;amp;cd=2&amp;amp;cad=rja&amp;amp;uact=8&amp;amp;ved=0ahUKEwi86ruJzbfKAhXDox4KHfl4AJwQFggiMAE&amp;amp;url=http%3A%2F%2Fwww.jedec.org%2Fsites%2Fdefault%2Ffiles%2Fdocs%2F4_20_26R24.pdf&amp;amp;usg=AFQjCNE91eZMe4JUIrXkyRv0pT1AKGFhIQ&amp;amp;bvm=bv.112064104,d.dmo" rel="nofollow"&gt;https://www.google.ru/url?sa=t&amp;amp;rct=j&amp;amp;q=&amp;amp;esrc=s&amp;amp;source=web&amp;amp;cd=2&amp;amp;cad=rja&amp;amp;uact=8&amp;amp;ved=0ahUKEwi86ruJzbfKAhXDox4KHfl4AJwQFggiMAE&amp;amp;url=http%3A%2F%2Fwww.jedec.org%2Fsites%2Fdefault%2Ffiles%2Fdocs%2F4_20_26R24.pdf&amp;amp;usg=AFQjCNE91eZMe4JUIrXkyRv0pT1AKGFhIQ&amp;amp;bvm=bv.112064104,d.dmo&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;2. &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;In DDR4, VREF is only used for address/command bus of DDR4 DRAM. Memory controller VREF is generated internally. When DDR4 mode is used the external VREF pin needs to be grounded. It is &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;D1_MVREF pin of the LS1021A.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;3. The TA_BB_RTC pin recommended voltage level is 1V see the Table 3 of the LS1021A Datasheet.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;4. See Note 7 for the Table 3 of the LS1021A Datasheet:&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;LVDD and L1VDD must always be the same voltage.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;5. Find the &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;DVDD_VSEL (435-436&lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt; bits) of the LS1021A RCW. See the Table 4-14 of the LS1021A Reference Manual. These bits determinates internal switch for using external DVDD voltage. If &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;DVDD_VSEL is set to 0b10, external DVDD powers supply can be 3.3V.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;If &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;DVDD_VSEL is set to 0b00, external DVDD powers supply should be 1.8V.&lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt; Do not use 3.3V DVDD if &lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;DVDD_VSEL is set to 0b00. The LS1021a can be damaged.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL style="list-style-type: decimal;"&gt;&lt;LI&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;6. It is power consumption of PLL. It is not current from PLL pins.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Jan 2016 06:10:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/LS1020A-RTC-questions/m-p/503967#M1083</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-01-20T06:10:59Z</dc:date>
    </item>
  </channel>
</rss>