<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Layerscape中的主题 ls1046a RCW source</title>
    <link>https://community.nxp.com/t5/Layerscape/ls1046a-RCW-source/m-p/1481943#M10786</link>
    <description>&lt;P&gt;I'm confused about the valid location for the RCW in the LS1046A.&lt;/P&gt;&lt;P&gt;In LS1046A Reference Manual, Rev. 3, 08/2021, page 208, it states:&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial black,avant garde"&gt;"NOTE: LS1046A do not support NAND flash as RCW source."&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;but on page 209, step 10, it states:&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial black,avant garde"&gt;"If the IFC's NAND Flash interface is configured as the RCW source, the reset block&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde"&gt;instructs the IFC to load a boot block from Flash into the internal buffer RAM of the&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde"&gt;IFC."&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;I'm confused reading this, and could use some explanation.&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 29 Jun 2022 16:18:51 GMT</pubDate>
    <dc:creator>Daves_Garage</dc:creator>
    <dc:date>2022-06-29T16:18:51Z</dc:date>
    <item>
      <title>ls1046a RCW source</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1046a-RCW-source/m-p/1481943#M10786</link>
      <description>&lt;P&gt;I'm confused about the valid location for the RCW in the LS1046A.&lt;/P&gt;&lt;P&gt;In LS1046A Reference Manual, Rev. 3, 08/2021, page 208, it states:&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial black,avant garde"&gt;"NOTE: LS1046A do not support NAND flash as RCW source."&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;but on page 209, step 10, it states:&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial black,avant garde"&gt;"If the IFC's NAND Flash interface is configured as the RCW source, the reset block&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde"&gt;instructs the IFC to load a boot block from Flash into the internal buffer RAM of the&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT face="arial black,avant garde"&gt;IFC."&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="arial,helvetica,sans-serif"&gt;I'm confused reading this, and could use some explanation.&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 29 Jun 2022 16:18:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1046a-RCW-source/m-p/1481943#M10786</guid>
      <dc:creator>Daves_Garage</dc:creator>
      <dc:date>2022-06-29T16:18:51Z</dc:date>
    </item>
    <item>
      <title>Re: ls1046a RCW source</title>
      <link>https://community.nxp.com/t5/Layerscape/ls1046a-RCW-source/m-p/1485667#M10837</link>
      <description>&lt;P&gt;The LS1046A does not support NAND flash as an RCW source.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 19:24:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/ls1046a-RCW-source/m-p/1485667#M10837</guid>
      <dc:creator>Daves_Garage</dc:creator>
      <dc:date>2022-07-06T19:24:09Z</dc:date>
    </item>
  </channel>
</rss>