<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: FTDI Driver in Kernel in Layerscape</title>
    <link>https://community.nxp.com/t5/Layerscape/FTDI-Driver-in-Kernel/m-p/1480989#M10772</link>
    <description>&lt;P&gt;Please find folder&amp;nbsp;build/linux/linux/arm64/LS/lib whether&amp;nbsp;&lt;SPAN&gt;ftdi_sio.ko&amp;nbsp;exists, if yes, it will be integrated in&amp;nbsp;modules folder in&amp;nbsp;bootpartition tar ball.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Tue, 28 Jun 2022 07:05:57 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2022-06-28T07:05:57Z</dc:date>
    <item>
      <title>FTDI Driver in Kernel</title>
      <link>https://community.nxp.com/t5/Layerscape/FTDI-Driver-in-Kernel/m-p/1479984#M10759</link>
      <description>&lt;P&gt;I am running lsdk 1906 and ran the command "flex-builder -c linux:custom -a arm64" to pull up the GUI so i can select the ftdi driver. Running "flex-builder -c linux -a arm64" and then "flex-builder -i mkbootpartition -a arm64" to create&amp;nbsp;&lt;SPAN&gt;kernel tarball im build/image. I also went inside build/image/linux_xx folder to check if the ftdi_sio.ko is in there but could not find anything relate to that. How do i know if the kernel tarball has the ftdi_sio driver in it when i don't see it in the linux folder.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 24 Jun 2022 21:10:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/FTDI-Driver-in-Kernel/m-p/1479984#M10759</guid>
      <dc:creator>laplace12</dc:creator>
      <dc:date>2022-06-24T21:10:32Z</dc:date>
    </item>
    <item>
      <title>Re: FTDI Driver in Kernel</title>
      <link>https://community.nxp.com/t5/Layerscape/FTDI-Driver-in-Kernel/m-p/1480989#M10772</link>
      <description>&lt;P&gt;Please find folder&amp;nbsp;build/linux/linux/arm64/LS/lib whether&amp;nbsp;&lt;SPAN&gt;ftdi_sio.ko&amp;nbsp;exists, if yes, it will be integrated in&amp;nbsp;modules folder in&amp;nbsp;bootpartition tar ball.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jun 2022 07:05:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/FTDI-Driver-in-Kernel/m-p/1480989#M10772</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2022-06-28T07:05:57Z</dc:date>
    </item>
    <item>
      <title>Re: FTDI Driver in Kernel</title>
      <link>https://community.nxp.com/t5/Layerscape/FTDI-Driver-in-Kernel/m-p/1481233#M10778</link>
      <description>&lt;P&gt;i don't see the ftdi driver in the lib/modules/4.19.46/kernel/driver/usb. When i create the boot tarball and create the linux_4.19)LS_arm64_&amp;lt;timestamp&amp;gt;.tgz, and put that on the sd card, i see that ftdi driver exist but could not find it in the lib folder.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 28 Jun 2022 13:05:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Layerscape/FTDI-Driver-in-Kernel/m-p/1481233#M10778</guid>
      <dc:creator>laplace12</dc:creator>
      <dc:date>2022-06-28T13:05:37Z</dc:date>
    </item>
  </channel>
</rss>